#include <zb_zcl_price.h>
PublishCalorificValue command payload
- See also
- SE spec, subclause D.4.2.4.4.
§ calorific_value
| zb_uint32_t zb_zcl_price_publish_calorific_value_payload_s::calorific_value |
- See also
- sub-clause D.4.2.2.4.5
§ calorific_value_trailing_digit
| zb_uint8_t zb_zcl_price_publish_calorific_value_payload_s::calorific_value_trailing_digit |
- See also
- sub-clause D.4.2.2.4.7
§ calorific_value_unit
| zb_uint8_t zb_zcl_price_publish_calorific_value_payload_s::calorific_value_unit |
- See also
- sub-clause D.4.2.2.4.6
§ issuer_event_id
| zb_uint32_t zb_zcl_price_publish_calorific_value_payload_s::issuer_event_id |
Unique identifier generated by the commodity provider.
§ start_time
| zb_uint32_t zb_zcl_price_publish_calorific_value_payload_s::start_time |
A UTCTime field to denote the time at which the value becomes valid. The value remains valid until replaced by a newer one.
The documentation for this struct was generated from the following file:
- /conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_price.h