#include <zb_zcl_prepayment.h>
Top Up Payload Details
- See also
- SE spec, Figure D-132
§ top_up_amount
| zb_int32_t zb_zcl_prepayment_top_up_payload_details_s::top_up_amount |
This is the amount of credit that was added to the Metering Device during this Top Up.
§ top_up_amount_plus_1
| zb_int32_t zb_zcl_prepayment_top_up_payload_details_s::top_up_amount_plus_1 |
§ top_up_amount_plus_n
| zb_int32_t zb_zcl_prepayment_top_up_payload_details_s::top_up_amount_plus_n |
§ top_up_code
| zb_uint8_t zb_zcl_prepayment_top_up_payload_details_s::top_up_code[26] |
This is the value of the Top Up code stored in the log.
§ top_up_code_plus_1
| zb_uint8_t zb_zcl_prepayment_top_up_payload_details_s::top_up_code_plus_1[26] |
§ top_up_code_plus_n
| zb_uint8_t zb_zcl_prepayment_top_up_payload_details_s::top_up_code_plus_n[26] |
§ top_up_time
| zb_uint32_t zb_zcl_prepayment_top_up_payload_details_s::top_up_time |
This is the UTC Timestamp when the Top Up was applied to the Metering Device.
§ top_up_time_plus_1
| zb_uint32_t zb_zcl_prepayment_top_up_payload_details_s::top_up_time_plus_1 |
§ top_up_time_plus_n
| zb_uint32_t zb_zcl_prepayment_top_up_payload_details_s::top_up_time_plus_n |
The documentation for this struct was generated from the following file:
- /conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_prepayment.h