Logo
Developing with ZBOSS for Zigbee
zb_zcl_level_control_move_to_closest_frequency_req_s Struct Reference

Structured representation of MOVE_TO_CLOSEST_FREQUENCY command payload. More...

#include <zb_zcl_level_control.h>

Data Fields

zb_uint16_t frequency
 

Detailed Description

Structured representation of MOVE_TO_CLOSEST_FREQUENCY command payload.

See also
ZCL spec, subclause 3.10.2.3.5.1

Field Documentation

§ frequency

zb_uint16_t zb_zcl_level_control_move_to_closest_frequency_req_s::frequency

Frequency field


The documentation for this struct was generated from the following file: