#include <zb_zcl_events.h>
Publish Event Log Sub-Payload
- See also
- SE spec, Figure D-175
-
zb_zcl_events_publish_event_log_payload_t::log_payload
§ event_data
| zb_uint8_t zb_zcl_events_sub_log_payload_s::event_data[47] |
A variable length octet string array used to hold additional information captured when the event occurred. The first element (element 0) of the array indicates the length of the string, NOT including the first element.
§ event_id
§ event_time
| zb_uint32_t zb_zcl_events_sub_log_payload_s::event_time |
§ log_id
| zb_uint8_t zb_zcl_events_sub_log_payload_s::log_id |
The least significant nibble is an enumeration indicating the Log ID. The most significant nibble is reserved.
§ number_of_events_log_payload_control
| zb_uint8_t zb_zcl_events_sub_log_payload_s::number_of_events_log_payload_control |
The least significant nibble represents the Log Payload Control. It determines availability of events to cross payload frame boundary. The most significant nibble indicates the number of events contained within the log payload of this command.
The documentation for this struct was generated from the following file:
- /conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_events.h