Configure Interface Response parameters. More...
#include <zb_zcl_direct_configuration.h>
Data Fields | |
| zb_uint8_t | status |
| zb_uint8_t | interface_state |
Configure Interface Response parameters.
| zb_uint8_t zb_zcl_direct_configuration_configure_interface_resp_s::interface_state |
Current Interface State,
| zb_uint8_t zb_zcl_direct_configuration_configure_interface_resp_s::status |
Command processing status