Logo
Developing with ZBOSS for Zigbee
zb_zcl_calendar_special_day_entry_s Struct Reference

#include <zb_zcl_calendar.h>

Data Fields

zb_uint32_t special_day_date
 
zb_uint8_t day_id_ref
 

Detailed Description

Special Day Entry A SpecialDayEntry consists of the Special Day Date and a reference (Day ID Ref) to the related Day Profile entry. The dates of the Special Day Table must be arranged in ascending order.

See also
SE spec, Figure D-147 - SpecialDayEntry Sub-Payload
zb_zcl_calendar_publish_special_days_payload_t::special_day_entry

Field Documentation

§ day_id_ref

zb_uint8_t zb_zcl_calendar_special_day_entry_s::day_id_ref

§ special_day_date

zb_uint32_t zb_zcl_calendar_special_day_entry_s::special_day_date

The documentation for this struct was generated from the following file: