#include <zb_zcl_calendar.h>
Season Entry payload A Season Entry consists of a Season Start Date and the reference (Week ID Ref) to the related Week Profile entry. The Start Date of the Season Entries must be arranged in ascending order. The active season is valid until the Season Start Date of the next Season Entry.
- See also
- SE spec, Figure D-145 - Season Entry Sub-Payload
-
zb_zcl_calendar_publish_seasons_payload_t::season_entry
§ season_start_date
| zb_uint32_t zb_zcl_calendar_season_entry_payload_s::season_start_date |
§ week_id_ref
| zb_uint8_t zb_zcl_calendar_season_entry_payload_s::week_id_ref |
The documentation for this struct was generated from the following file:
- /conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_calendar.h