Logo
Developing with ZBOSS for Zigbee
zb_secur_ic_entry_s Struct Reference

IC entry type zb_secur_ic_get_list_req. More...

#include <zboss_api.h>

Data Fields

zb_ieee_addr_t device_address
 
zb_uint8_t options
 
zb_uint8_t align
 
zb_uint8_t installcode [16U+2U]
 

Detailed Description

IC entry type zb_secur_ic_get_list_req.

Field Documentation

§ align

zb_uint8_t zb_secur_ic_entry_s::align

§ device_address

zb_ieee_addr_t zb_secur_ic_entry_s::device_address

Partner address

§ installcode

zb_uint8_t zb_secur_ic_entry_s::installcode[16U+2U]

16b installcode +2b crc

§ options

zb_uint8_t zb_secur_ic_entry_s::options

The documentation for this struct was generated from the following file: