#include <zboss_api_nwk.h>
Data Fields | |
| zb_uint16_t | index |
| zb_uint32_t | update_count |
| zb_uint16_t zb_nwk_nbr_iterator_cb_params_s::index |
In the callback function: Index of the returned neighbour table entry. The value of ZB_NWK_NBR_ITERATOR_INDEX_EOT indicates that the entry was not returned and the buffer payload should be ignored. If the structure is passed as the API call parameters: Index, from which the next neighbour table entry should be searched.
| zb_uint32_t zb_nwk_nbr_iterator_cb_params_s::update_count |
In the callback function: The current value of the table update counter. This parameter is ignored in the API call parameters.