Logo
Developing with ZBOSS for Zigbee
zb_channel_change_parameters_s Struct Reference

Parameters for zb_prepare_network_for_channel_change() and zb_start_channel_change() More...

#include <zboss_api_nwk.h>

Data Fields

zb_uint32_t next_channel_change
 

Detailed Description

Field Documentation

§ next_channel_change

zb_uint32_t zb_channel_change_parameters_s::next_channel_change

This field indicates the next channel that will be used once a start channel change command is received. Only 1 channel page and channel bit shall be set


The documentation for this struct was generated from the following file: