Logo
Developing with ZBOSS for Zigbee
zb_aps_check_binding_resp_s Struct Reference

#include <zboss_api_aps.h>

Data Fields

zb_uint8_t src_endpoint
 
zb_uint16_t cluster_id
 
zb_bool_t exists
 

Detailed Description

This data structure passed to callback passed to zb_zdo_check_binding_request().

Field Documentation

§ cluster_id

zb_uint16_t zb_aps_check_binding_resp_s::cluster_id

§ exists

zb_bool_t zb_aps_check_binding_resp_s::exists

§ src_endpoint

zb_uint8_t zb_aps_check_binding_resp_s::src_endpoint

The documentation for this struct was generated from the following file: