Data Structures | |
| struct | zb_nvram_failure_report_s |
| Structure that contains report about any NVRAM failure. Pointer to this structure will be set as additional info in error_app_handler with error code ERROR_CODE(ERROR_CATEGORY_NVRAM, ZB_ERROR_NVRAM_WRITE_VALIDATION_FAILURE). Upon receiving of this error, user can decide what to do: More... | |
Macros | |
| #define | ZB_NVRAM_DATA_SET_TYPE_PAGE_HDR_R22 30u |
| #define | ZB_NVRAM_APP_DATASET_NUMBER 4U |
Typedefs | |
| typedef enum zb_nvram_dataset_types_e | zb_nvram_dataset_types_t |
| typedef struct zb_nvram_failure_report_s | zb_nvram_failure_report_t |
| Structure that contains report about any NVRAM failure. Pointer to this structure will be set as additional info in error_app_handler with error code ERROR_CODE(ERROR_CATEGORY_NVRAM, ZB_ERROR_NVRAM_WRITE_VALIDATION_FAILURE). Upon receiving of this error, user can decide what to do: More... | |
| typedef void(* | zb_nvram_read_app_data_t) (zb_uint8_t page, zb_uint32_t pos, zb_uint16_t payload_length) |
| typedef zb_ret_t(* | zb_nvram_write_app_data_t) (zb_uint8_t page, zb_uint32_t pos) |
| typedef zb_uint16_t(* | zb_nvram_get_app_data_size_t) (void) |
Enumerations | |
| enum | zb_nvram_dataset_types_e { ZB_NVRAM_RESERVED = 0, ZB_NVRAM_COMMON_DATA = 1, ZB_NVRAM_HA_DATA = 2, ZB_NVRAM_ZCL_REPORTING_DATA = 3, ZB_NVRAM_APS_SECURE_DATA_GAP = 4, ZB_NVRAM_APS_BINDING_DATA_GAP = 5, ZB_NVRAM_HA_POLL_CONTROL_DATA = 6, ZB_NVRAM_APS_SECURE_DATA = 7, ZB_NVRAM_DATASET_GRPW_DATA = 8, ZB_NVRAM_APP_DATA1 = 9, ZB_NVRAM_APP_DATA2 = 10, ZB_NVRAM_ADDR_MAP = 11, ZB_NVRAM_NEIGHBOUR_TBL = 12, ZB_NVRAM_INSTALLCODES = 13, ZB_NVRAM_IB_COUNTERS = 14, ZB_NVRAM_APS_BINDING_DATA = 15, ZB_NVRAM_DATASET_GP_PRPOXYT = 16, ZB_NVRAM_DATASET_GP_SINKT = 17, ZB_NVRAM_DATASET_GP_CLUSTER = 18, ZB_NVRAM_APS_GROUPS_DATA = 19, ZB_NVRAM_DATASET_SE_CERTDB = 20, ZB_NVRAM_ZCL_WWAH_DATA = 21, ZB_NVRAM_DATASET_GP_APP_TBL = 22, ZB_NVRAM_APP_DATA3 = 27, ZB_NVRAM_APP_DATA4 = 28, ZB_NVRAM_KE_WHITELIST = 29, ZB_NVRAM_DATASET_ZB_DIRECT = 30, ZB_NVRAM_ZDO_DIAGNOSTICS_DATA = 31, ZB_NVRAM_DATASET_NUMBER, ZB_NVRAM_DATA_SET_TYPE_PAGE_HDR = 0xFFFFU } |
After the zboss_start() call, the ZBOSS stack reads the whole flash page and looks for the valid version of each dataset. If the valid application dataset is found, the read/load callback is called. The callback should store the read value inside the RAM using its own static/global variable.
Afterwards, it is assumed that the application uses the static/global variable to perform changes or read dataset field values.
Whenever needed, the application may call the zb_nvram_write_dataset() in order to store the updated dataset inside the flash.
Every call to the zb_nvram_write_dataset() triggers the write/store callback. The callback should get the static/global variable and use the zb_osif_nvram_write() to store its current value.
If there is no user dataset stored inside the flash, the callback will not be called, so the static/global variable should be initialized with valid default values before calling zboss_start().
There are also four predefined dataset IDs for a user application: ZB_NVRAM_APP_DATA1 , ZB_NVRAM_APP_DATA2 , ZB_NVRAM_APP_DATA3 and ZB_NVRAM_APP_DATA4. It is up to the application to decide what data to store in the NVRAM in these datasets.
To use application specific datasets, the appropriate callbacks should be defined in the application and registered by zb_nvram_register_appx_read_cb() and zb_nvram_register_appx_write_cb().
One callback is to be passed to zb_nvram_register_appx_read_cb(). This callback should get the static/global variable and use zb_osif_nvram_read() to read its value from the flash memory. Two callbacks are to be passed to zb_nvram_register_appx_write_cb(). One of them should get the static/global variable and use zb_osif_nvram_write() to store its current value. It should return error code from zb_osif_nvram_write(). The second should return the size of the application dataset structure.
Example #1:
Example #2 (Using application callbacks):
Define user dataset type:
Callback prototypes:
Register application callbacks:
Callback implementation:
Application NVRAM usage:
See light_sample application
| #define ZB_NVRAM_APP_DATASET_NUMBER 4U |
| #define ZB_NVRAM_DATA_SET_TYPE_PAGE_HDR_R22 30u |
| typedef enum zb_nvram_dataset_types_e zb_nvram_dataset_types_t |
Enum All NVRAM dataset types
ZB_NVRAM_DATASET_NUMBER - count of dataset types. Not a real dataset type!
| typedef struct zb_nvram_failure_report_s zb_nvram_failure_report_t |
Structure that contains report about any NVRAM failure. Pointer to this structure will be set as additional info in error_app_handler with error code ERROR_CODE(ERROR_CATEGORY_NVRAM, ZB_ERROR_NVRAM_WRITE_VALIDATION_FAILURE). Upon receiving of this error, user can decide what to do:
| typedef zb_uint16_t(* zb_nvram_get_app_data_size_t) (void) |
Returns size of application datasets
| typedef void(* zb_nvram_read_app_data_t) (zb_uint8_t page, zb_uint32_t pos, zb_uint16_t payload_length) |
Declares application callback used for reading application datasets from NVRAM.
| page | - page in NVRAM from data will be read |
| pos | - offset in page |
| payload_length | - number of bytes to read (aligned to 4) |
| typedef zb_ret_t(* zb_nvram_write_app_data_t) (zb_uint8_t page, zb_uint32_t pos) |
Declares application callback used for writing application datasets into NVRAM.
| page | - page in NVRAM where data will be stored |
| pos | - offset in page |
Enum All NVRAM dataset types
ZB_NVRAM_DATASET_NUMBER - count of dataset types. Not a real dataset type!
| void zb_nvram_erase | ( | void | ) |
Erase Informational Bases to NVRAM or other persistent storage
| zb_ret_t zb_nvram_read_data | ( | zb_uint8_t | page, |
| zb_uint32_t | pos, | ||
| zb_uint8_t * | buf, | ||
| zb_uint16_t | len | ||
| ) |
Reads a portion of some dataset.
| page | - an NVRAM page to read from |
| pos | - a position on the NVRAM page |
| buf | - a buffer where read data will be saved |
| len | - a data length to read |
| void zb_nvram_register_app1_read_cb | ( | zb_nvram_read_app_data_t | cb | ) |
Register application callback for reading ZB_NVRAM_APP_DATA1 from NVRAM
| cb | - callback that will be called upon reading dataset |
| void zb_nvram_register_app1_write_cb | ( | zb_nvram_write_app_data_t | wcb, |
| zb_nvram_get_app_data_size_t | gcb | ||
| ) |
Register application callback for writing ZB_NVRAM_APP_DATA1 to NVRAM
| wcb | - callback that will be called upon writing |
| gcb | - this callback will be called upon writing to determine dataset size |
| void zb_nvram_register_app2_read_cb | ( | zb_nvram_read_app_data_t | cb | ) |
Register application callback for reading ZB_NVRAM_APP_DATA2 from NVRAM
| cb | - callback that will be called upon reading dataset |
| void zb_nvram_register_app2_write_cb | ( | zb_nvram_write_app_data_t | wcb, |
| zb_nvram_get_app_data_size_t | gcb | ||
| ) |
Register application callback for writing ZB_NVRAM_APP_DATA2 to NVRAM
| wcb | - callback that will be called upon writing |
| gcb | - this callback will be called upon writing to determine dataset size |
| void zb_nvram_register_app3_read_cb | ( | zb_nvram_read_app_data_t | cb | ) |
Register application callback for reading ZB_NVRAM_APP_DATA3 from NVRAM
| cb | - callback that will be called upon reading dataset |
| void zb_nvram_register_app3_write_cb | ( | zb_nvram_write_app_data_t | wcb, |
| zb_nvram_get_app_data_size_t | gcb | ||
| ) |
Register application callback for writing ZB_NVRAM_APP_DATA3 to NVRAM
| wcb | - callback that will be called upon writing |
| gcb | - this callback will be called upon writing to determine dataset size |
| void zb_nvram_register_app4_read_cb | ( | zb_nvram_read_app_data_t | cb | ) |
Register application callback for reading ZB_NVRAM_APP_DATA4 from NVRAM
| cb | - callback that will be called upon reading dataset |
| void zb_nvram_register_app4_write_cb | ( | zb_nvram_write_app_data_t | wcb, |
| zb_nvram_get_app_data_size_t | gcb | ||
| ) |
Register application callback for writing ZB_NVRAM_APP_DATA4 to NVRAM
| wcb | - callback that will be called upon writing |
| gcb | - this callback will be called upon writing to determine dataset size |
| void zb_nvram_transaction_commit | ( | void | ) |
Commit NVRAM transaction.
Finish writing multiple datasets at once. A transaction must started by calling zb_nvram_transaction_start().
| void zb_nvram_transaction_start | ( | void | ) |
Start NVRAM transaction.
Start writing multiple datasets at once. A transaction must finished by calling zb_nvram_transaction_commit().
| zb_ret_t zb_nvram_write_data | ( | zb_uint8_t | page, |
| zb_uint32_t | pos, | ||
| zb_uint8_t * | buf, | ||
| zb_uint16_t | len | ||
| ) |
Writes a portion of some dataset.
| page | - an NVRAM page to write |
| pos | - a position on the NVRAM page |
| buf | - a buffer with data to be written |
| len | - a buffer size |
| zb_ret_t zb_nvram_write_dataset | ( | zb_nvram_dataset_types_t | t | ) |
Write specified dataset into NVRAM
| t | - dataset index, see zb_nvram_dataset_types_e |
Example
| void zb_set_nvram_erase_at_start | ( | zb_bool_t | erase | ) |
Enable or disable NVRAM erasing on every application startup.
| erase | - 1 to enable erasing; 0 - disable. Erasing is disabled by default. |