Data Structures | |
| struct | zb_secur_ic_get_list_req_s |
| Request for zb_secur_ic_get_list_req. More... | |
| struct | zb_secur_ic_get_list_resp_s |
| Response for zb_secur_ic_get_list_req. More... | |
| struct | zb_secur_ic_entry_s |
| IC entry type zb_secur_ic_get_list_req. More... | |
| struct | zb_secur_ic_get_by_idx_req_s |
| Request for zb_secur_ic_get_by_idx_req. More... | |
| struct | zb_secur_ic_get_by_idx_resp_s |
| Response for zb_secur_ic_get_by_idx_req. More... | |
| struct | zb_secur_ic_remove_req_s |
| Request for zb_secur_ic_remove_req. More... | |
| struct | zb_secur_ic_remove_resp_s |
| Response for zb_secur_ic_remove_req. More... | |
| struct | zb_secur_ic_remove_all_req_s |
| Request for zb_secur_ic_remove_all_req. More... | |
| struct | zb_secur_ic_remove_all_resp_s |
| Response for zb_secur_ic_remove_all_req. More... | |
Functions | |
| void | zb_secur_ic_add (const zb_ieee_addr_t address, zb_uint8_t ic_type, zb_uint8_t const *ic, zb_secur_ic_add_cb_t cb) |
| Add install code for the device with specified long address. More... | |
| zb_ret_t | zb_secur_ic_set (zb_uint8_t ic_type, const zb_uint8_t *ic) |
| Set install code for the device. More... | |
| void | zb_secur_ic_get_list_req (zb_uint8_t param) |
| Get list of the install codes. It is valid only for the TC (ZC). More... | |
| void | zb_secur_ic_get_by_idx_req (zb_uint8_t param) |
| Get the install code by index. It is valid only for the TC (ZC). More... | |
| void | zb_secur_ic_remove_req (zb_uint8_t param) |
| Remove the install code for the device with specified long address. It is valid only for the TC (ZC). More... | |
| void | zb_secur_ic_remove_all_req (zb_uint8_t param) |
| zb_ret_t | zb_secur_ic_str_set (char *ic_str) |
| Set install code for the device from character string. More... | |
| void | zb_secur_ic_str_add (zb_ieee_addr_t address, char *ic_str, zb_secur_ic_add_cb_t cb) |
| Add install code for the device from character string. More... | |
| void | zb_set_installcode_policy (zb_bool_t allow_ic_only) |
IC types | |
/* Set passcode for joiner */ zb_secur_ic_set(ZB_IC_TYPE_PASSCODE, g_r23_zed_passcode); | |
| #define | ZB_IC_TYPE_48 0U |
| #define | ZB_IC_TYPE_64 1U |
| #define | ZB_IC_TYPE_96 2U |
| #define | ZB_IC_TYPE_128 3U |
| #define | ZB_IC_TYPE_PASSCODE 4U /*<! Not an Installcode indeed, but r23 passcode (4 bytes) - extends to 128bit */ |
| #define | ZB_IC_TYPE_128_HASHED |
| #define | ZB_IC_TYPE_MAX 6U |
The Key Negotiation Protocols Bitmask Table I.5.1-4-54 | |
The Key Negotiation Protocols Bitmask Table I.5.1-4-54 (merged with Zigbee Direct 6.5.2.1. Zigbee Direct Key Negotiation Method TLV) /* The application can also change key negotiation methods and PSK secrets. * For example, we disable ZB_TLV_KEY_ECDHE_KEY_REQUEST_ZB_30. * It means that ZC will not accept r23+ devices without DLK support */ /* That call is just for a demo here. That method is already enabled by * zboss_use_r23_behavior() call. */ Note: These values were members of zb_tlv_key_negotiation_methods_t | |
| typedef zb_uint8_t | zb_tlv_key_negotiation_methods_t |
| #define | ZB_TLV_KEY_ECDHE_KEY_REQUEST_ZB_30 0x00U /*<! Static Key Update Request */ |
| #define | ZB_TLV_DIRECT_KEY_ECDHE_RESERVED_MIN 0x00U /*<! 0 is reserved in zigbee direct */ |
| #define | ZB_TLV_KEY_ECDHE_CURVE_25519_HASH_AESMMO128 0x01U /*<! DLK with curve 25519 and hash AESMMO128 */ |
| #define | ZB_TLV_KEY_ECDHE_CURVE_25519_HASH_SHA256 0x02U /*<! DLK with curve 25519 and hash SHA256 */ |
| #define | ZB_TLV_KEY_ECDHE_RESERVED_MAX 0x03U /*<! 3-15 is reserved in r23 */ |
| #define | ZB_TLV_KEY_ECDHE_CURVE_P256_HASH_SHA256 0x03U /*<! ZB Direct only: curve P256, hash SHA256 */ |
| #define | ZB_TLV_DIRECT_KEY_ECDHE_RESERVED_MAX 0x04U /*<! reserved value for Direct */ |
bitmask for support_secrets, value for selected secret | |
/* Rewrite supported PSK secrets bit mask. Just to demonstrate the API */ { zb_uint8_t supported_secrets_mask = 0; ZB_TLV_PSK_SECRET_ENABLE(supported_secrets_mask, ZB_TLV_PSK_SECRET_AUTH_TOKEN); ZB_TLV_PSK_SECRET_ENABLE(supported_secrets_mask, ZB_TLV_PSK_SECRET_INSTALL_CODE); ZB_TLV_PSK_SECRET_ENABLE(supported_secrets_mask, ZB_TLV_PSK_SECRET_PAKE_PASSCODE); zb_set_supported_psk_secrets(supported_secrets_mask); } Note: These values were members of zb_tlv_psk_secrets_t | |
| typedef zb_uint8_t | zb_tlv_psk_secrets_t |
| #define | ZB_TLV_PSK_SECRET_AUTH_TOKEN 0x00U |
| #define | ZB_TLV_PSK_SECRET_INSTALL_CODE 0x01U |
| #define | ZB_TLV_PSK_SECRET_PAKE_PASSCODE 0x02U |
| #define | ZB_TLV_PSK_SECRET_BASIC_ACCESS_KEY 0x03U |
| #define | ZB_TLV_PSK_SECRET_ADMINISTRATIVE_ACCESS_KEY 0x04U |
| #define | ZB_TLV_PSK_SECRET_RESERVED_MAX 0x05U /* 6-7 is reserved */ |
| #define | ZB_TLV_PSK_SECRET_WELL_KNOWN_KEY 0xFFU |
| #define ZB_IC_TYPE_128 3U |
| #define ZB_IC_TYPE_128_HASHED |
| #define ZB_IC_TYPE_48 0U |
| #define ZB_IC_TYPE_64 1U |
| #define ZB_IC_TYPE_96 2U |
| #define ZB_IC_TYPE_MAX 6U |
| #define ZB_IC_TYPE_PASSCODE 4U /*<! Not an Installcode indeed, but r23 passcode (4 bytes) - extends to 128bit */ |
| #define ZB_TLV_DIRECT_KEY_ECDHE_RESERVED_MAX 0x04U /*<! reserved value for Direct */ |
| #define ZB_TLV_DIRECT_KEY_ECDHE_RESERVED_MIN 0x00U /*<! 0 is reserved in zigbee direct */ |
| #define ZB_TLV_KEY_ECDHE_CURVE_25519_HASH_AESMMO128 0x01U /*<! DLK with curve 25519 and hash AESMMO128 */ |
| #define ZB_TLV_KEY_ECDHE_CURVE_25519_HASH_SHA256 0x02U /*<! DLK with curve 25519 and hash SHA256 */ |
| #define ZB_TLV_KEY_ECDHE_CURVE_P256_HASH_SHA256 0x03U /*<! ZB Direct only: curve P256, hash SHA256 */ |
| #define ZB_TLV_KEY_ECDHE_KEY_REQUEST_ZB_30 0x00U /*<! Static Key Update Request */ |
| #define ZB_TLV_KEY_ECDHE_RESERVED_MAX 0x03U /*<! 3-15 is reserved in r23 */ |
| #define ZB_TLV_PSK_SECRET_ADMINISTRATIVE_ACCESS_KEY 0x04U |
| #define ZB_TLV_PSK_SECRET_AUTH_TOKEN 0x00U |
| #define ZB_TLV_PSK_SECRET_BASIC_ACCESS_KEY 0x03U |
| #define ZB_TLV_PSK_SECRET_INSTALL_CODE 0x01U |
| #define ZB_TLV_PSK_SECRET_PAKE_PASSCODE 0x02U |
| #define ZB_TLV_PSK_SECRET_RESERVED_MAX 0x05U /* 6-7 is reserved */ |
| #define ZB_TLV_PSK_SECRET_WELL_KNOWN_KEY 0xFFU |
| typedef zb_uint8_t zb_ic_types_t |
| typedef void(* zb_secur_ic_add_cb_t) (zb_ret_t status) |
Declares application callback that is called after installcode addition.
| status | - status of installcode addition |
| typedef struct zb_secur_ic_entry_s zb_secur_ic_entry_t |
IC entry type zb_secur_ic_get_list_req.
| typedef struct zb_secur_ic_get_by_idx_req_s zb_secur_ic_get_by_idx_req_t |
Request for zb_secur_ic_get_by_idx_req.
| typedef struct zb_secur_ic_get_by_idx_resp_s zb_secur_ic_get_by_idx_resp_t |
Response for zb_secur_ic_get_by_idx_req.
| typedef struct zb_secur_ic_get_list_req_s zb_secur_ic_get_list_req_t |
Request for zb_secur_ic_get_list_req.
| typedef struct zb_secur_ic_get_list_resp_s zb_secur_ic_get_list_resp_t |
Response for zb_secur_ic_get_list_req.
| typedef struct zb_secur_ic_remove_all_req_s zb_secur_ic_remove_all_req_t |
Request for zb_secur_ic_remove_all_req.
| typedef struct zb_secur_ic_remove_all_resp_s zb_secur_ic_remove_all_resp_t |
Response for zb_secur_ic_remove_all_req.
| typedef struct zb_secur_ic_remove_req_s zb_secur_ic_remove_req_t |
Request for zb_secur_ic_remove_req.
| typedef struct zb_secur_ic_remove_resp_s zb_secur_ic_remove_resp_t |
Response for zb_secur_ic_remove_req.
| typedef zb_uint8_t zb_tlv_psk_secrets_t |
| void zb_secur_ic_add | ( | const zb_ieee_addr_t | address, |
| zb_uint8_t | ic_type, | ||
| zb_uint8_t const * | ic, | ||
| zb_secur_ic_add_cb_t | cb | ||
| ) |
Add install code for the device with specified long address.
| [in] | address | - long address of the device to add the install code |
| [in] | ic_type | - install code type as enumerated in ic_types |
| [in] | cb | - callback that will be called after installcode addition |
| [in] | ic | - pointer to the install code buffer |
This call allows to add install codes for several devices into NVRAM. It makes sense for Trust Center/Coordinator devices only as usual device doesn't need to have someone's else install codes.
| void zb_secur_ic_get_by_idx_req | ( | zb_uint8_t | param | ) |
Get the install code by index. It is valid only for the TC (ZC).
| param | buffer with request parameters, will be also used to store response. |
| void zb_secur_ic_get_list_req | ( | zb_uint8_t | param | ) |
Get list of the install codes. It is valid only for the TC (ZC).
| param | buffer with request parameters, will be also used to store response. |
| void zb_secur_ic_remove_all_req | ( | zb_uint8_t | param | ) |
Remove the install code for all devices. It is valid only for the TC (ZC).
| param | buffer with request parameters, will be also used to store response. |
| void zb_secur_ic_remove_req | ( | zb_uint8_t | param | ) |
Remove the install code for the device with specified long address. It is valid only for the TC (ZC).
| param | buffer with request parameters, will be also used to store response. |
| zb_ret_t zb_secur_ic_set | ( | zb_uint8_t | ic_type, |
| const zb_uint8_t * | ic | ||
| ) |
Set install code for the device.
| [in] | ic_type | - install code type as enumerated in ic_types |
| [in] | ic | - pointer to the install code buffer |
This call allows to set the install code for the current device. It is assumed that device can have only one install code.
| void zb_secur_ic_str_add | ( | zb_ieee_addr_t | address, |
| char * | ic_str, | ||
| zb_secur_ic_add_cb_t | cb | ||
| ) |
Add install code for the device from character string.
| [in] | address | - long address of the device to add the install code for |
| [in] | ic_str | - install code text string |
| [in] | cb | - callback that will be called after installcode addition |
This call allows to add install codes for several devices into NVRAM. It makes sense for Trust Center/Coordinator devices only as usual device doesn't need to have someone's else install codes.
| zb_ret_t zb_secur_ic_str_set | ( | char * | ic_str | ) |
Set install code for the device from character string.
| [in] | ic_str | - install code text string |
This call allows to set the install code for the current device. It is assumed that device can have only one install code.
| void zb_set_installcode_policy | ( | zb_bool_t | allow_ic_only | ) |
Set installcode policy flag.
| allow_ic_only | - use ZB_TRUE value to check installcodes |