Logo
Developing with ZBOSS for Zigbee
Read reporting configuration command sending and parsing

Data Structures

struct  zb_zcl_read_reporting_cfg_req_s
 
struct  zb_zcl_read_reporting_cfg_rsp_s
 

Macros

#define ZB_ZCL_READ_REP_CFG_REQ_SIZE   sizeof(zb_zcl_read_reporting_cfg_req_t)
 Minimal size of Write attribute request, it will be more if attr_value size is more than 1 byte. More...
 
#define ZB_ZCL_GENERAL_GET_NEXT_READ_REP_CFG_REQ(data_buf, rep_cfg_req, rslt)
 Parses read reporting configuration request and returns next Read reporting configuration attribute record or NULL if there is no more data. More...
 
#define ZB_ZCL_GENERAL_INIT_READ_REPORTING_CONFIGURATION_SRV_REQ(buffer, ptr, def_resp)
 Initialize Read reporting configuration command (report send case) More...
 
#define ZB_ZCL_GENERAL_INIT_READ_REPORTING_CONFIGURATION_SRV_REQ_MANUF(buffer, ptr, def_resp, manuf_code)
 Initialize Read reporting configuration command (report send case) More...
 
#define ZB_ZCL_GENERAL_INIT_READ_REPORTING_CONFIGURATION_CLI_REQ(buffer, ptr, def_resp)
 Initialize Read reporting configuration command (report receive case) More...
 
#define ZB_ZCL_GENERAL_ADD_SEND_READ_REPORTING_CONFIGURATION_REQ(ptr, attr_id)
 Add Read reporting configuration record to command payload (report send case) More...
 
#define ZB_ZCL_GENERAL_ADD_RECV_READ_REPORTING_CONFIGURATION_REQ(ptr, attr_id)
 Add Read reporting configuration record to command payload (report receive case) More...
 
#define ZB_ZCL_GENERAL_SEND_READ_REPORTING_CONFIGURATION_REQ( buffer, ptr, addr, dst_addr_mode, dst_ep, ep, prfl_id, cluster_id, cb)
 Sends Read reporting configuration command. More...
 
#define ZB_ZCL_GENERAL_GET_READ_REPORTING_CONFIGURATION_RES(data_buf, read_rep_conf_res)
 Parses Read reporting configuration response and returns next read reporting configuration record or NULL if there is no more data. More...
 

Typedefs

typedef struct zb_zcl_read_reporting_cfg_req_s zb_zcl_read_reporting_cfg_req_t
 
typedef struct zb_zcl_read_reporting_cfg_rsp_s zb_zcl_read_reporting_cfg_rsp_t
 

Detailed Description

Most of actions related to the read attribute reporting configuration are implemented in ZCL internals. Read reporting configuration command is described in ZCL spec, subclause 2.4.9.

Macro Definition Documentation

§ ZB_ZCL_GENERAL_ADD_RECV_READ_REPORTING_CONFIGURATION_REQ

#define ZB_ZCL_GENERAL_ADD_RECV_READ_REPORTING_CONFIGURATION_REQ (   ptr,
  attr_id 
)

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_commands.h>

Value:
{ \
ZB_ZCL_PACKET_PUT_DATA8(ptr, ZB_ZCL_CONFIGURE_REPORTING_RECV_REPORT); \
ZB_ZCL_PACKET_PUT_DATA16_VAL(ptr, (attr_id)); \
}
Definition: zb_zcl_commands.h:1461

Add Read reporting configuration record to command payload (report receive case)

Parameters
ptr- command buffer pointer
attr_id- attribute identifier

§ ZB_ZCL_GENERAL_ADD_SEND_READ_REPORTING_CONFIGURATION_REQ

#define ZB_ZCL_GENERAL_ADD_SEND_READ_REPORTING_CONFIGURATION_REQ (   ptr,
  attr_id 
)

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_commands.h>

Value:
{ \
ZB_ZCL_PACKET_PUT_DATA8(ptr, ZB_ZCL_CONFIGURE_REPORTING_SEND_REPORT); \
ZB_ZCL_PACKET_PUT_DATA16_VAL(ptr, (attr_id)); \
}
Definition: zb_zcl_commands.h:1460

Add Read reporting configuration record to command payload (report send case)

Parameters
ptr- command buffer pointer
attr_id- attribute identifier

§ ZB_ZCL_GENERAL_GET_NEXT_READ_REP_CFG_REQ

#define ZB_ZCL_GENERAL_GET_NEXT_READ_REP_CFG_REQ (   data_buf,
  rep_cfg_req,
  rslt 
)

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_commands.h>

Value:
{ \
zb_zcl_read_reporting_cfg_req_t *cfg_req; \
(cfg_req) = zb_buf_len(data_buf) >= ZB_ZCL_READ_REP_CFG_REQ_SIZE ? \
if (cfg_req) \
{ \
rep_cfg_req.direction = cfg_req -> direction; \
rep_cfg_req.attr_id = cfg_req -> attr_id; \
ZB_ZCL_HTOLE16_INPLACE(&(read_rep_cfg_req).attr_id); \
rslt = ZB_TRUE; \
} \
else \
{ \
rslt = ZB_FALSE; \
} \
}
#define zb_buf_cut_left(buf, size)
Definition: zboss_api_buf.h:474
#define ZB_FALSE
Definition: zb_types.h:349
#define zb_buf_begin(buf)
Definition: zboss_api_buf.h:354
#define ZB_ZCL_READ_REP_CFG_REQ_SIZE
Minimal size of Write attribute request, it will be more if attr_value size is more than 1 byte...
Definition: zb_zcl_commands.h:1814
#define ZB_TRUE
Definition: zb_types.h:350
Definition: zb_zcl_commands.h:1798
#define zb_buf_len(buf)
Definition: zboss_api_buf.h:372

Parses read reporting configuration request and returns next Read reporting configuration attribute record or NULL if there is no more data.

If request contains invalid data, NULL is returned.

Parameters
data_buf- ID zb_bufid_t of a buffer containing read reporting configuration request data
rep_cfg_req- out pointer to zb_zcl_read_attr_req_t, containing read reporting configuration request
rslt- returns TRUE if record exist and FALSE if not
Note
data_buf buffer should contain read reporting configuration request payload, without ZCL header. Each parsed read reporting configuration request is extracted from initial data_buf buffer

§ ZB_ZCL_GENERAL_GET_READ_REPORTING_CONFIGURATION_RES

#define ZB_ZCL_GENERAL_GET_READ_REPORTING_CONFIGURATION_RES (   data_buf,
  read_rep_conf_res 
)

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_commands.h>

Parses Read reporting configuration response and returns next read reporting configuration record or NULL if there is no more data.

If response contains invalid data, NULL is returned.

Parameters
data_buf- ID zb_bufid_t of a buffer containing Configure reporting response data
read_rep_conf_res- out pointer to zb_zcl_read_reporting_cfg_rsp_t, containing read reporting configuration record
Note
data_buf buffer should contain Read reporting configuration, without ZCL header. Each parsed Read reporting configuration record is extracted from initial data_buf buffer

§ ZB_ZCL_GENERAL_INIT_READ_REPORTING_CONFIGURATION_CLI_REQ

#define ZB_ZCL_GENERAL_INIT_READ_REPORTING_CONFIGURATION_CLI_REQ (   buffer,
  ptr,
  def_resp 
)

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_commands.h>

Value:
{ \
ptr = ZB_ZCL_START_PACKET(buffer); \
ZB_ZCL_CONSTRUCT_GENERAL_COMMAND_REQ_FRAME_CONTROL_A( \
ZB_ZCL_CONSTRUCT_COMMAND_HEADER(ptr, ZB_ZCL_GET_SEQ_NUM(), ZB_ZCL_CMD_READ_REPORT_CFG); \
}
#define ZB_ZCL_GET_SEQ_NUM()
Return next sequence number for ZCL frame.
Definition: zb_zcl_common.h:1470
#define ZB_ZCL_START_PACKET(zbbuf)
Initializes zb_buf_t buffer and returns pointer to the beginning of array.
Definition: zb_zcl_common.h:1550
#define ZB_ZCL_FRAME_DIRECTION_TO_CLI
Definition: zb_zcl_common.h:1066
#define ZB_ZCL_CMD_READ_REPORT_CFG
Definition: zb_zcl_commands.h:69
#define ZB_ZCL_NOT_MANUFACTURER_SPECIFIC
Definition: zb_zcl_common.h:1017

Initialize Read reporting configuration command (report receive case)

Parameters
bufferto put packet to
ptr- command buffer pointer
def_resp- enable/disable default response

§ ZB_ZCL_GENERAL_INIT_READ_REPORTING_CONFIGURATION_SRV_REQ

#define ZB_ZCL_GENERAL_INIT_READ_REPORTING_CONFIGURATION_SRV_REQ (   buffer,
  ptr,
  def_resp 
)

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_commands.h>

Value:
{ \
ptr = ZB_ZCL_START_PACKET(buffer); \
ZB_ZCL_CONSTRUCT_GENERAL_COMMAND_REQ_FRAME_CONTROL_A( \
ZB_ZCL_CONSTRUCT_COMMAND_HEADER(ptr, ZB_ZCL_GET_SEQ_NUM(), ZB_ZCL_CMD_READ_REPORT_CFG); \
}
#define ZB_ZCL_GET_SEQ_NUM()
Return next sequence number for ZCL frame.
Definition: zb_zcl_common.h:1470
#define ZB_ZCL_START_PACKET(zbbuf)
Initializes zb_buf_t buffer and returns pointer to the beginning of array.
Definition: zb_zcl_common.h:1550
#define ZB_ZCL_FRAME_DIRECTION_TO_SRV
Definition: zb_zcl_common.h:1064
#define ZB_ZCL_CMD_READ_REPORT_CFG
Definition: zb_zcl_commands.h:69
#define ZB_ZCL_NOT_MANUFACTURER_SPECIFIC
Definition: zb_zcl_common.h:1017

Initialize Read reporting configuration command (report send case)

Parameters
bufferto put packet to
ptr- command buffer pointer
def_resp- enable/disable default response

§ ZB_ZCL_GENERAL_INIT_READ_REPORTING_CONFIGURATION_SRV_REQ_MANUF

#define ZB_ZCL_GENERAL_INIT_READ_REPORTING_CONFIGURATION_SRV_REQ_MANUF (   buffer,
  ptr,
  def_resp,
  manuf_code 
)

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_commands.h>

Value:
{ \
ptr = ZB_ZCL_START_PACKET(buffer); \
ZB_ZCL_CONSTRUCT_GENERAL_COMMAND_REQ_FRAME_CONTROL_A( \
ZB_ZCL_CONSTRUCT_COMMAND_HEADER_EXT(ptr, ZB_ZCL_GET_SEQ_NUM(), ZB_TRUE, \
}
#define ZB_ZCL_GET_SEQ_NUM()
Return next sequence number for ZCL frame.
Definition: zb_zcl_common.h:1470
#define ZB_ZCL_START_PACKET(zbbuf)
Initializes zb_buf_t buffer and returns pointer to the beginning of array.
Definition: zb_zcl_common.h:1550
#define ZB_ZCL_FRAME_DIRECTION_TO_SRV
Definition: zb_zcl_common.h:1064
#define ZB_ZCL_MANUFACTURER_SPECIFIC
Definition: zb_zcl_common.h:1020
#define ZB_ZCL_CMD_READ_REPORT_CFG
Definition: zb_zcl_commands.h:69
#define ZB_TRUE
Definition: zb_types.h:350

Initialize Read reporting configuration command (report send case)

Parameters
bufferto put packet to
ptr- command buffer pointer
def_resp- enable/disable default response
manuf_code- manufacturer specific code

§ ZB_ZCL_GENERAL_SEND_READ_REPORTING_CONFIGURATION_REQ

#define ZB_ZCL_GENERAL_SEND_READ_REPORTING_CONFIGURATION_REQ (   buffer,
  ptr,
  addr,
  dst_addr_mode,
  dst_ep,
  ep,
  prfl_id,
  cluster_id,
  cb 
)

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_commands.h>

Value:
{ \
ZB_ZCL_FINISH_PACKET(buffer, ptr) \
ZB_ZCL_SEND_COMMAND_SHORT(buffer, addr, dst_addr_mode, dst_ep, ep, prfl_id, cluster_id, cb); \
}

Sends Read reporting configuration command.

Parameters
bufferto put data to
ptr- pointer to the memory area to put data to
addr- address to send packet to
dst_addr_mode- addressing mode
dst_ep- destination endpoint
ep- sending endpoint
prfl_id- profile identifier
cluster_id- cluster identifier
cb- callback for getting command send status

§ ZB_ZCL_READ_REP_CFG_REQ_SIZE

#define ZB_ZCL_READ_REP_CFG_REQ_SIZE   sizeof(zb_zcl_read_reporting_cfg_req_t)

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_commands.h>

Minimal size of Write attribute request, it will be more if attr_value size is more than 1 byte.

Typedef Documentation

§ zb_zcl_read_reporting_cfg_req_t

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_commands.h>

Format of the Attribute Status Record Field Figure 2.20 in ZCL spec. NOTE: it can be various number of attribute status record fields in Read reporting configuration request

§ zb_zcl_read_reporting_cfg_rsp_t

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_commands.h>

Format of the Attribute Reporting Configuration Record Field Figure 2.22 in ZCL spec. NOTE: it can be various number of attribute recording configuration record fields in Read reporting configuration response