Functions | |
| void | zboss_use_r22_behavior (void) |
| void | zboss_use_r23_behavior (void) |
| void | zb_nwk_use_r22_joining (zb_bool_t value) |
| void zb_nwk_use_r22_joining | ( | zb_bool_t | value | ) |
Use r22 joining instead nwk commissioning request
| value | - if true, then mac association or rejoin_req will be used |
| void zboss_use_r22_behavior | ( | void | ) |
Setup required behavior for testing legacy R22 GU as specified by Zigbee Pro Compliant Test Specification - Section 7.5.1:
For Legacy Version= 22 The GU special build must be implemented which disables the following features of R23 and the device behaves as an R22 device:
Notes: If you’re unsure what the text above is, you probably do not need this call! This is not a full r22 compatibility mode.
| void zboss_use_r23_behavior | ( | void | ) |
Enable using of r23 joining featires: NWK Commissioning then DLK.