Logo
Developing with ZBOSS for Zigbee
Discover attributes request and response sending and parsing.

Data Structures

struct  zb_zcl_disc_attr_req_s
 ZCL Discover Attribute Command frame. More...
 
struct  zb_zcl_disc_attr_info_s
 ZCL Description for Discover Attribute Response frame. More...
 
struct  zb_zcl_disc_attr_res_s
 ZCL Discover Attribute Response frame. More...
 

Macros

#define ZB_ZCL_GENERAL_GET_COMPLETE_DISC_RES(data_buf, complete)
 Parses Discovery attribute response and returns next Read attribute status record or NULL if there is no more data. More...
 
#define ZB_ZCL_GENERAL_GET_NEXT_DISC_ATTR_RES(data_buf, disc_attr_info)
 Discovery attribute response and returns next Discovery attribute status record or NULL if there is no more data. More...
 
#define ZB_ZCL_GENERAL_DISC_READ_ATTR_REQ(buffer, def_resp, start_attr_id, max_len, addr, dst_addr_mode, dst_ep, ep, profile_id, cluster_id, cb)
 Discover attribute command. More...
 
#define ZB_ZCL_GENERAL_DISC_ATTR_REQ_A(buffer, cmd_ptr, direction, def_resp, start_attr_id, max_len, addr, dst_addr_mode, dst_ep, ep, profile_id, cluster_id, cb)
 Discover Attribute Request. More...
 
#define ZB_ZCL_GENERAL_DISC_ATTR_REQ_MANUF(buffer, cmd_ptr, direction, def_resp, manuf_code, start_attr_id, max_len, addr, dst_addr_mode, dst_ep, ep, profile_id, cluster_id, cb)
 Discover Attribute Request. More...
 

Typedefs

typedef struct zb_zcl_disc_attr_req_s zb_zcl_disc_attr_req_t
 ZCL Discover Attribute Command frame. More...
 
typedef struct zb_zcl_disc_attr_info_s zb_zcl_disc_attr_info_t
 ZCL Description for Discover Attribute Response frame. More...
 
typedef struct zb_zcl_disc_attr_res_s zb_zcl_disc_attr_res_t
 ZCL Discover Attribute Response frame. More...
 
typedef zb_uint8_t zb_zcl_disc_complete_t
 Type for possible values of ZCL Discover Attribute Response. More...
 

ZCL Discover Attribute Response - complete field

See also
ZCL spec, clause 2.4.14
#define ZB_ZCL_DISC_NON_COMPLETE   0x00U
 
#define ZB_ZCL_DISC_COMPLETE   0x01U
 

Detailed Description

Discover attributes command described in ZCL spec, subclauses 2.4.13 and 2.4.14.

Read attributes request command can be formed and sent as in following snippet:

ZB_ZCL_GENERAL_DISC_ATTR_REQ(zcl_cmd_buf, cmd_ptr, ZB_ZCL_ENABLE_DEFAULT_RESPONSE,
DUT_ADDR, DUT_ADDR_MODE, DUT_ENDPOINT,

Discover attributes response can be parsed as:

until allocated buffer space exceeds.

Discover attributes request parsing and response filling and sending is implemented in ZCL library internal functions.

Macro Definition Documentation

§ ZB_ZCL_DISC_COMPLETE

§ ZB_ZCL_DISC_NON_COMPLETE

#define ZB_ZCL_DISC_NON_COMPLETE   0x00U

§ ZB_ZCL_GENERAL_DISC_ATTR_REQ_A

#define ZB_ZCL_GENERAL_DISC_ATTR_REQ_A (   buffer,
  cmd_ptr,
  direction,
  def_resp,
  start_attr_id,
  max_len,
  addr,
  dst_addr_mode,
  dst_ep,
  ep,
  profile_id,
  cluster_id,
  cb 
)

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_commands.h>

Value:
{ \
zb_uint8_t *cmd_ptr = ZB_ZCL_START_PACKET(buffer); \
ZB_ZCL_CONSTRUCT_GENERAL_COMMAND_REQ_FRAME_CONTROL_A(cmd_ptr, direction, \
ZB_ZCL_CONSTRUCT_COMMAND_HEADER(cmd_ptr, ZB_ZCL_GET_SEQ_NUM(), ZB_ZCL_CMD_DISC_ATTRIB); \
ZB_ZCL_PACKET_PUT_DATA16_VAL(cmd_ptr, (start_attr_id)); \
ZB_ZCL_PACKET_PUT_DATA8(cmd_ptr, (max_len)); \
ZB_ZCL_FINISH_PACKET(buffer, cmd_ptr) \
ZB_ZCL_SEND_COMMAND_SHORT(buffer, addr, dst_addr_mode, dst_ep, ep, profile_id, cluster_id, cb); \
}
#define ZB_ZCL_GET_SEQ_NUM()
Return next sequence number for ZCL frame.
Definition: zb_zcl_common.h:1470
#define ZB_ZCL_START_PACKET(zbbuf)
Initializes zb_buf_t buffer and returns pointer to the beginning of array.
Definition: zb_zcl_common.h:1550
#define ZB_ZCL_NOT_MANUFACTURER_SPECIFIC
Definition: zb_zcl_common.h:1017
#define ZB_ZCL_CMD_DISC_ATTRIB
Definition: zb_zcl_commands.h:73

Discover Attribute Request.

Parameters
buffer- reference to buffer to put packet into
cmd_ptr- pointer to command (not used)
direction- direction of command (see zcl_frame_direction)
def_resp- enable/disable default response
start_attr_id- start attribute ID
max_len- max count
addr- address to send packet to
dst_addr_mode- addressing mode
dst_ep- destination endpoint
ep- sending endpoint
profile_id- profile identifier
cluster_id- cluster identifier
cb- callback for getting command send status

§ ZB_ZCL_GENERAL_DISC_ATTR_REQ_MANUF

#define ZB_ZCL_GENERAL_DISC_ATTR_REQ_MANUF (   buffer,
  cmd_ptr,
  direction,
  def_resp,
  manuf_code,
  start_attr_id,
  max_len,
  addr,
  dst_addr_mode,
  dst_ep,
  ep,
  profile_id,
  cluster_id,
  cb 
)

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_commands.h>

Value:
{ \
zb_uint8_t *cmd_ptr = ZB_ZCL_START_PACKET(buffer); \
ZB_ZCL_CONSTRUCT_GENERAL_COMMAND_REQ_FRAME_CONTROL_A(cmd_ptr, direction, \
ZB_ZCL_CONSTRUCT_COMMAND_HEADER_EXT( \
cmd_ptr, ZB_ZCL_GET_SEQ_NUM(), \
ZB_ZCL_PACKET_PUT_DATA16_VAL(cmd_ptr, (start_attr_id)); \
ZB_ZCL_PACKET_PUT_DATA8(cmd_ptr, (max_len)); \
ZB_ZCL_FINISH_PACKET(buffer, cmd_ptr) \
ZB_ZCL_SEND_COMMAND_SHORT(buffer, addr, dst_addr_mode, dst_ep, ep, profile_id, cluster_id, cb); \
}
#define ZB_ZCL_GET_SEQ_NUM()
Return next sequence number for ZCL frame.
Definition: zb_zcl_common.h:1470
#define ZB_ZCL_START_PACKET(zbbuf)
Initializes zb_buf_t buffer and returns pointer to the beginning of array.
Definition: zb_zcl_common.h:1550
#define ZB_ZCL_MANUFACTURER_SPECIFIC
Definition: zb_zcl_common.h:1020
#define ZB_ZCL_CMD_DISC_ATTRIB
Definition: zb_zcl_commands.h:73

Discover Attribute Request.

Parameters
buffer- reference to buffer to put packet into
cmd_ptr- pointer to command (not used)
direction- direction of command (see zcl_frame_direction)
def_resp- enable/disable default response
manuf_code- manufacturer specific code
start_attr_id- start attribute ID
max_len- max count
addr- address to send packet to
dst_addr_mode- addressing mode
dst_ep- destination endpoint
ep- sending endpoint
profile_id- profile identifier
cluster_id- cluster identifier
cb- callback for getting command send status

§ ZB_ZCL_GENERAL_DISC_READ_ATTR_REQ

#define ZB_ZCL_GENERAL_DISC_READ_ATTR_REQ (   buffer,
  def_resp,
  start_attr_id,
  max_len,
  addr,
  dst_addr_mode,
  dst_ep,
  ep,
  profile_id,
  cluster_id,
  cb 
)

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_commands.h>

Value:
{ \
zb_uint8_t *cmd_ptr = ZB_ZCL_START_PACKET(buffer); \
ZB_ZCL_CONSTRUCT_GENERAL_COMMAND_REQ_FRAME_CONTROL(cmd_ptr, def_resp); \
ZB_ZCL_CONSTRUCT_COMMAND_HEADER(cmd_ptr, ZB_ZCL_GET_SEQ_NUM(), ZB_ZCL_CMD_DISC_ATTRIB); \
ZB_ZCL_PACKET_PUT_DATA16_VAL(cmd_ptr, (start_attr_id)); \
ZB_ZCL_PACKET_PUT_DATA8(cmd_ptr, (max_len)); \
ZB_ZCL_FINISH_PACKET(buffer, cmd_ptr) \
ZB_ZCL_SEND_COMMAND_SHORT(buffer, addr, dst_addr_mode, dst_ep, ep, profile_id, cluster_id, cb); \
}
#define ZB_ZCL_GET_SEQ_NUM()
Return next sequence number for ZCL frame.
Definition: zb_zcl_common.h:1470
#define ZB_ZCL_START_PACKET(zbbuf)
Initializes zb_buf_t buffer and returns pointer to the beginning of array.
Definition: zb_zcl_common.h:1550
#define ZB_ZCL_CMD_DISC_ATTRIB
Definition: zb_zcl_commands.h:73

Discover attribute command.

Parameters
buffer- reference to buffer to put packet into
def_resp- enable/disable default response
start_attr_id- start attribute ID
max_len- max count
addr- address to send packet to
dst_addr_mode- addressing mode
dst_ep- destination endpoint
ep- sending endpoint
profile_id- profile identifier
cluster_id- cluster identifier
cb- callback for getting command send status

§ ZB_ZCL_GENERAL_GET_COMPLETE_DISC_RES

#define ZB_ZCL_GENERAL_GET_COMPLETE_DISC_RES (   data_buf,
  complete 
)

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_commands.h>

Value:
{ \
if (zb_buf_len(data_buf) > 0) \
{ \
complete = *(zb_uint8_t*)zb_buf_begin(data_buf); \
(void)zb_buf_cut_left((data_buf), sizeof(zb_uint8_t)); \
} \
else \
{ \
(complete) = 0; \
} \
}
#define zb_buf_cut_left(buf, size)
Definition: zboss_api_buf.h:474
#define zb_buf_begin(buf)
Definition: zboss_api_buf.h:354
unsigned char zb_uint8_t
Project-local 1-byte unsigned int type.
Definition: zb_types.h:147
#define zb_buf_len(buf)
Definition: zboss_api_buf.h:372

Parses Discovery attribute response and returns next Read attribute status record or NULL if there is no more data.

If response contains invalid data, 0 is returned.

Parameters
data_buf- ID zb_bufid_t of a buffer containing discover attribute response data
complete- variable to store Complete field
Note
data_buf buffer should contain Discover attribute response payload, without ZCL header.

§ ZB_ZCL_GENERAL_GET_NEXT_DISC_ATTR_RES

#define ZB_ZCL_GENERAL_GET_NEXT_DISC_ATTR_RES (   data_buf,
  disc_attr_info 
)

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_commands.h>

Value:
{ \
(disc_attr_info) = zb_buf_len(data_buf) >= ZB_ZCL_DISC_ATTR_RESP_SIZE ? \
\
if (disc_attr_info) \
{ \
ZB_ZCL_HTOLE16_INPLACE(&(disc_attr_info)->attr_id); \
\
(void)zb_buf_cut_left((data_buf), ZB_ZCL_DISC_ATTR_RESP_SIZE); \
} \
}
#define zb_buf_cut_left(buf, size)
Definition: zboss_api_buf.h:474
#define zb_buf_begin(buf)
Definition: zboss_api_buf.h:354
ZCL Description for Discover Attribute Response frame.
Definition: zb_zcl_commands.h:1182
#define zb_buf_len(buf)
Definition: zboss_api_buf.h:372

Discovery attribute response and returns next Discovery attribute status record or NULL if there is no more data.

If response contains invalid data, NULL is returned.

Parameters
data_buf- ID zb_bufid_t of a buffer containing part of Discover attribute response data
disc_attr_info- out pointer to zb_zcl_disc_attr_info_t, containing Discover attribute status record
Note
data_buf buffer should contain Discover attribute response payload, without ZCL header. Each parsed Discover attribute status record is extracted from initial data_buf buffer

Typedef Documentation

§ zb_zcl_disc_attr_info_t

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_commands.h>

ZCL Description for Discover Attribute Response frame.

See also
ZCL spec, zb_zcl_read_attr 2.4.14 Discover Attribute Response

§ zb_zcl_disc_attr_req_t

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_commands.h>

ZCL Discover Attribute Command frame.

See also
ZCL spec, zb_zcl_disc_attr 2.4.13 Discover Attributes Command

§ zb_zcl_disc_attr_res_t

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_commands.h>

ZCL Discover Attribute Response frame.

See also
ZCL spec, zb_zcl_read_attr 2.4.15 Discover Attribute Response
Note
Command frame contains variable number of parameters

§ zb_zcl_disc_complete_t

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_commands.h>

Type for possible values of ZCL Discover Attribute Response.

Deprecated:
holds one of zcl_disc_complete. Kept only for backward compatibility as zcl_disc_complete were declared previously as enum. Can be removed in future releases.