Data Structures | |
| union | zb_addr_u_t |
| union | zb_addr_u |
| Union to address either long or short address. More... | |
Macros | |
| #define | ZB_STDC_90 |
| #define | ZB_32BIT_WORD |
| #define | ZB_XDATA |
| #define | ZB_CODE |
| #define | ZB_IAR_CODE |
| #define | ZB_REGISTER register |
| #define | ZB_VOID_ARGLIST void |
| #define | ZB_CONST const |
| #define | ZB_INLINE |
| #define | ZB_BITFIELD_CAST(x) (x) |
| #define | ZB_CPP_STR2(x) #x |
| #define | ZB_CPP_STR(x) ZB_CPP_STR2(x) |
| #define | ZB_FALSE 0U |
| #define | ZB_TRUE 1U |
| #define | ZB_FALSE_U ZB_FALSE |
| #define | ZB_TRUE_U ZB_TRUE |
| #define | ZB_B2U(b) (((b) != ZB_FALSE) ? (1U) : (0U)) |
| #define | ZB_U2B(u) (((u) != 0U) ? (ZB_TRUE) : (ZB_FALSE)) |
| #define | ZB_INT8_MIN (-127 - 1) |
| #define | ZB_INT8_MAX 127 |
| #define | ZB_UINT8_MIN 0U |
| #define | ZB_UINT8_MAX 255U |
| #define | ZB_INT16_MIN (-32767 - 1) |
| #define | ZB_INT16_MAX 32767 |
| #define | ZB_UINT16_MIN 0U |
| #define | ZB_UINT16_MAX 65535U |
| #define | ZB_INT32_MIN (-2147483647L - 1) |
| #define | ZB_INT32_MAX 2147483647L |
| #define | ZB_UINT32_MIN 0UL |
| #define | ZB_UINT32_MAX 4294967295UL |
| #define | ZB_UINT_MIN 0UL |
| #define | ZB_SHORT_MIN ZB_INT32_MIN |
| #define | ZB_SHORT_MAX ZB_INT32_MAX |
| #define | ZB_USHORT_MAX ZB_UINT32_MAX |
| #define | ZB_INT_MIN ZB_INT32_MIN |
| #define | ZB_INT_MAX ZB_INT32_MAX |
| #define | ZB_UINT_MAX ZB_UINT32_MAX |
| #define | ZB_INT_MASK 0x7fffffffU |
| #define | ZB_PACKED_STRUCT |
| #define | ZB_PACKED_PRE |
| #define | ZB_WEAK_PRE |
| #define | ZB_WEAK |
| #define | ZB_ALIGNED_PRE |
| #define | ZB_DEPRECATED |
| #define | ZB_NORETURN |
| #define | ZB_IS_64BIT_ADDR_UNKNOWN(addr) (ZB_MEMCMP((addr), (void const*)g_unknown_ieee_addr, 8) == 0) |
| #define | ZB_64BIT_ADDR_UNKNOWN(addr) ZB_MEMSET((addr), -1, 8) |
| #define | ZB_EXTPANID_IS_ZERO ZB_IS_64BIT_ADDR_ZERO |
| #define | ZB_EXTPANID_ZERO ZB_64BIT_ADDR_ZERO |
| #define | ZB_EXTPANID_COPY ZB_64BIT_ADDR_COPY |
| #define | ZB_EXTPANID_CMP ZB_64BIT_ADDR_CMP |
| #define | ZB_IEEE_ADDR_IS_ZERO ZB_IS_64BIT_ADDR_ZERO |
| #define | ZB_IEEE_ADDR_IS_UNKNOWN ZB_IS_64BIT_ADDR_UNKNOWN |
| #define | ZB_IEEE_ADDR_ZERO ZB_64BIT_ADDR_ZERO |
| #define | ZB_IEEE_ADDR_UNKNOWN ZB_64BIT_ADDR_UNKNOWN |
| #define | ZB_IEEE_ADDR_COPY ZB_64BIT_ADDR_COPY |
| #define | ZB_IEEE_ADDR_CMP ZB_64BIT_ADDR_CMP |
| #define | ZB_CCM_KEY_IS_ZERO(k) (ZB_IS_64BIT_ADDR_ZERO((zb_uint8_t*)(k)) && ZB_IS_64BIT_ADDR_ZERO(((zb_uint8_t*)(k)) + 8U)) |
| #define | ZB_IEEE_ADDR_IS_VALID(addr) !(ZB_IEEE_ADDR_IS_ZERO(addr)||ZB_IEEE_ADDR_IS_UNKNOWN(addr)) |
| #define | ZB_ADDR_CMP(addr_mode, addr1, addr2) |
| #define | ZB_ADDR_U_CAST(addr) ((const zb_addr_u *)(const void *)(&(addr))) |
| #define | ZB_INT8_C(c) c |
| #define | ZB_UINT8_C(c) c ## U |
| #define | ZB_INT16_C(c) c |
| #define | ZB_UINT16_C(c) c ## U |
| #define | ZB_INT32_C(c) c ## L |
| #define | ZB_UINT32_C(c) c ## UL |
| #define | ZB_OFFSETOF(t, f) ((zb_size_t)(&((t *)NULL)->f)) |
| #define | ZB_OFFSETOF_VAR(s, f) (zb_size_t)(((zb_int8_t *)(&(s)->f)) - ((zb_int8_t *)(s))) |
| #define | ZB_SIZEOF_FIELD(type, field) (sizeof(((type*)0)->field)) |
| #define | ZB_ARRAY_SIZE(arr) (sizeof((arr))/sizeof((arr)[0])) |
| #define | ZB_SIGNED_SHIFT(v, s) ((zb_int_t)(v) >> (s)) |
| #define | ZB_ASSERT_IF_NOT_ALIGNED(data_type, length) ZB_ASSERT_COMPILE_DECL(((sizeof(data_type) % (length)) == 0U)) |
| #define | ZB_ASSERT_IF_NOT_ALIGNED_TO_4(data_type) ZB_ASSERT_IF_NOT_ALIGNED(data_type,4U) |
| #define | ZB_ASSERT_VALUE_ALIGNED(const_expr, length) ZB_ASSERT_COMPILE_DECL((((const_expr) % (length)) == 0U)) |
| #define | ZB_ASSERT_VALUE_ALIGNED_TO_4(const_expr) ZB_ASSERT_VALUE_ALIGNED(const_expr, 4U) |
| #define | ZB_GET_LOW_BYTE(val) (zb_uint8_t)((val) & 0xFFU) |
| #define | ZB_GET_HI_BYTE(val) (zb_uint8_t)(((val) >> 8U) & 0xFFU) |
| #define | ZB_SET_LOW_BYTE(res, val) (res) = ((((zb_uint16_t)(res)) & 0xFF00U) | (((zb_uint16_t)(val)) & 0xFFU)) |
| #define | ZB_SET_HI_BYTE(res, val) (res) = (((((zb_uint16_t)(val)) << 8U) & 0xFF00U) | (((zb_uint16_t)(res)) & 0xFFU)) |
| #define | ZB_PKT_16B_ZERO_BYTE 0U |
| #define | ZB_PKT_16B_FIRST_BYTE 1U |
| #define | ZB_ASSIGN_UINT16(ptr, vp) *((zb_uint16_t*)(ptr)) = *(zb_uint16_t*)(vp) |
| #define | ZB_ASSIGN_INT16(ptr, vp) *((zb_int16_t*)(ptr)) = *(zb_int16_t*)(vp) |
| #define | ZB_COPY_UINT24(ptr, vp) *((zb_uint24_t*)(ptr)) = *(zb_uint24_t*)(vp) |
| #define | ZB_COPY_INT24(ptr, vp) *((zb_int24_t*)(ptr)) = *(zb_int24_t*)(vp) |
| #define | ZB_ASSIGN_UINT32(ptr, vp) *((zb_uint32_t*)(ptr)) = *(zb_uint32_t*)(vp) |
| #define | ZB_ASSIGN_INT32(ptr, vp) *((zb_int32_t*)(ptr)) = *(zb_int32_t*)(vp) |
| #define | ZB_REVERSE16(ptr, val) |
| #define | ZB_REVERSE64(ptr, val) |
| #define | ZB_ARRAY_IDX_BY_ELEM(ar, el) ((el) - (ar)) |
| #define | ZB_ARRAY_IDX_BY_STRUCT_ELEM(ar, el, el_size) ( ((zb_size_t)(el) - (zb_size_t)(ar)) / (el_size) ) |
| #define | MIN_SIGNED_24BIT_VAL (-8388607LL) /* (0xFF800001LL) */ |
| #define | MAX_SIGNED_24BIT_VAL (0x7FFFFF) |
| #define | MAX_UNSIGNED_24BIT_VAL (0xFFFFFFU) |
| #define | MIN_SIGNED_48BIT_VAL (-140737488355327LL) /* (0xFFFF800000000001LL) */ |
| #define | MAX_SIGNED_48BIT_VAL (0x7FFFFFFFFFFF) |
| #define | MAX_UNSIGNED_48BIT_VAL (0xFFFFFFFFFFFFU) |
| #define | ZB_S64_FROM_S48(x) ((x & 0xFFFFFFFFFFFF) | ((x & 0x800000000000) ? 0xFFFF000000000000 : 0x0)) |
| #define | ZB_S64_TO_S48(x) ((zb_int64_t)(x & 0xFFFFFFFFFFFF)) |
| #define | ZB_S32_FROM_S24(x) ((x & 0xFFFFFF) | ((x & 0x800000) ? 0xFF000000 : 0x0)) |
| #define | ZB_S32_TO_S24(x) ((zb_int32_t)(x & 0xFFFFFF)) |
Typedefs | |
| typedef zb_uint32_t | zb_lbitfield_t |
| typedef long long | zb_int64_t |
| typedef unsigned long long | zb_uint64_t |
| typedef zb_ushort_t | zb_uindex_t |
| typedef zb_uint8_t | zb_64bit_data_t[8] |
| typedef union zb_addr_u_t | zb_addr_u |
| typedef zb_int32_t | zb_ret_t |
| Return type for ZB functions returning execution status. More... | |
Enumerations | |
| enum | zb_param_e { ZB_UNUSED_PARAM = 0 } |
| General purpose parameter type. More... | |
Variables | |
| const zb_64bit_addr_t | g_zero_addr |
| const zb_64bit_addr_t | g_unknown_ieee_addr |
Endian change API. | |
Macros to change words endian and access words at potentially non-aligned pointers. Zigbee uses little endian, see ZB spec, subclause 1.2.1.3. | |
| void | zb_htole16 (zb_uint8_t *ptr, zb_uint8_t *val) |
| void | zb_htole32 (zb_uint8_t *ptr, zb_uint8_t *val) |
| void * | zb_put_next_htole16 (zb_uint8_t *dst, zb_uint16_t val) |
| void * | zb_put_next_htole32 (zb_uint8_t *dst, zb_uint32_t val1) |
| void | zb_get_next_letoh16 (zb_uint16_t *dst, const zb_uint8_t **src) |
| void * | zb_put_next_2_htole16 (zb_uint8_t *dst, zb_uint16_t val1, zb_uint16_t val2) |
| void * | zb_put_next_2_htole32 (zb_uint8_t *dst, zb_uint32_t val1, zb_uint32_t val2) |
| void * | zb_put_next_ieee (zb_uint8_t *dst, zb_ieee_addr_t src) |
| #define | ZB_8BIT_SIZE 1U |
| #define | ZB_16BIT_SIZE 2U |
| #define | ZB_24BIT_SIZE 3U |
| #define | ZB_32BIT_SIZE 4U |
| #define | ZB_48BIT_SIZE 6U |
| #define | ZB_64BIT_SIZE 8U |
| #define | ZB_HTOLE16(ptr, val) zb_htole16((zb_uint8_t*)(ptr), (zb_uint8_t*)(val)) |
| #define | ZB_HTOLE16_ONPLACE(val) |
| #define | ZB_HTOLE32_ONPLACE(val) { zb_uint32_t _v = (val); ZB_HTOLE32(&(val), &_v); } |
| #define | ZB_HTOLE32(ptr, val) zb_htole32((zb_uint8_t*)(ptr), (zb_uint8_t*)(val)) |
| #define | ZB_HTOBE32(ptr, val) ZB_MEMCPY(ptr, val, 4U) |
| #define | ZB_HTOBE16(ptr, val) (*(zb_uint16_t *)(ptr)) = *((zb_uint16_t *)(val)) |
| #define | ZB_HTOBE16_VAL(ptr, val) ((zb_uint16_t *)(ptr))[0] = (val) |
| #define | ZB_HTOLE64(ptr, val) zb_memcpy8(ptr, val) |
| #define | ZB_HTOLE32_VAL(ptr, val) |
| #define | ZB_HTOLE16_VAL(ptr, val) |
| #define | ZB_PUT_NEXT_HTOLE16(ptr, val) |
| #define | ZB_PUT_NEXT_HTOLE32(ptr, val) (ptr) = zb_put_next_htole32((ptr), (val)) |
| #define | ZB_LETOH64(dst, src) zb_memcpy8((zb_uint8_t*)dst, (zb_uint8_t*)src) |
| #define | ZB_PUT_NEXT_IEEE(dst, src) (dst) = zb_put_next_ieee((dst), (src)); |
| #define | ZB_LETOH16 ZB_HTOLE16 |
| #define | ZB_LETOH24 ZB_HTOLE24 |
| #define | ZB_LETOH48 ZB_HTOLE48 |
| #define | ZB_LETOH32 ZB_HTOLE32 |
| #define | ZB_BETOH16 ZB_HTOBE16 |
| #define | ZB_BETOH32 ZB_HTOBE32 |
| #define | ZB_LETOH16_ONPLACE ZB_HTOLE16_ONPLACE |
| #define | ZB_LETOH32_ONPLACE ZB_HTOLE32_ONPLACE |
Base types. | |
| typedef char | zb_char_t |
| Project-local char type. More... | |
| typedef unsigned char | zb_uchar_t |
| Project-local unsigned char type. More... | |
| typedef unsigned char | zb_uint8_t |
| Project-local 1-byte unsigned int type. More... | |
| typedef signed char | zb_int8_t |
| Project-local 1-byte signed int type. More... | |
| typedef unsigned short | zb_uint16_t |
| Project-local 2-byte unsigned int type. More... | |
| typedef signed short | zb_int16_t |
| Project-local 2-byte signed int type. More... | |
| typedef unsigned int | zb_uint32_t |
| Project-local 4-byte unsigned int type. More... | |
| typedef signed int | zb_int32_t |
| Project-local 4-byte signed int type. More... | |
| typedef zb_uint32_t | zb_bitfield_t |
| Type to be used for unsigned bit fields inside structure. More... | |
| typedef zb_int32_t | zb_sbitfield_t |
| Type to be used for signed bit fields inside structure. More... | |
| typedef zb_uint32_t | zb_size_t |
| Project-local size_t type. More... | |
| typedef int | zb_short_t |
| Short int (can fit into single CPU register). More... | |
| typedef unsigned int | zb_ushort_t |
| Short unsigned int (can fit into single CPU register). More... | |
| typedef int | zb_int_t |
| Int (at least 2 bytes). More... | |
| typedef unsigned int | zb_uint_t |
| Unsigned int (at least 2 bytes). More... | |
| typedef zb_int_t | zb_long_t |
| Long int (at least 4 bytes). More... | |
| typedef zb_uint_t | zb_ulong_t |
| Unsigned long int (at least 4 bytes). More... | |
| typedef zb_uint8_t | zb_bool_t |
| General purpose boolean type. For C90, 'zb_bool_t' is an alias of 'zb_uint8_t'. For C99, the availability of the 'stdbool.h' standard header is expected and 'zb_bool_t' is an alias of 'bool'. ZB_FALSE and ZB_TRUE are defined as macros for both standards. More... | |
| typedef zb_bitfield_t | zb_bitbool_t |
| Type to be used for boolean bit fields inside structure. More... | |
| typedef float | zb_single_t |
| Project-local single precision float type. More... | |
Address types and API. | |
| typedef zb_uint8_t | zb_64bit_addr_t[8] |
| 8-bytes address (xpanid or long device address) base type. More... | |
| typedef zb_64bit_addr_t | zb_ieee_addr_t |
| Long (64-bit) device address. More... | |
| typedef zb_64bit_addr_t | zb_ext_pan_id_t |
| Long (64-bit) extended Pan ID. More... | |
| #define | ZB_IS_64BIT_ADDR_ZERO(addr) (ZB_MEMCMP((addr), (void const*)g_zero_addr, 8) == 0) |
| Checks that long address is a zero one. More... | |
| #define | ZB_64BIT_ADDR_ZERO(addr) ZB_MEMSET((addr), 0, 8) |
| Clears long address. More... | |
| #define | ZB_64BIT_ADDR_COPY(dst, src) ZB_MEMCPY(dst, src, sizeof(zb_64bit_addr_t)) |
| Copy long address. More... | |
| #define | ZB_64BIT_ADDR_CMP(one, two) (ZB_MEMCMP((one), (two), 8) == 0) |
| Check two long addresses are equal. More... | |
| #define MAX_SIGNED_24BIT_VAL (0x7FFFFF) |
| #define MAX_SIGNED_48BIT_VAL (0x7FFFFFFFFFFF) |
| #define MAX_UNSIGNED_24BIT_VAL (0xFFFFFFU) |
| #define MAX_UNSIGNED_48BIT_VAL (0xFFFFFFFFFFFFU) |
| #define MIN_SIGNED_24BIT_VAL (-8388607LL) /* (0xFF800001LL) */ |
| #define MIN_SIGNED_48BIT_VAL (-140737488355327LL) /* (0xFFFF800000000001LL) */ |
| #define ZB_16BIT_SIZE 2U |
| #define ZB_24BIT_SIZE 3U |
| #define ZB_32BIT_SIZE 4U |
| #define ZB_32BIT_WORD |
| #define ZB_48BIT_SIZE 6U |
| #define ZB_64BIT_ADDR_CMP | ( | one, | |
| two | |||
| ) | (ZB_MEMCMP((one), (two), 8) == 0) |
Check two long addresses are equal.
| one | address to compare. |
| two | address to compare to. |
| #define ZB_64BIT_ADDR_COPY | ( | dst, | |
| src | |||
| ) | ZB_MEMCPY(dst, src, sizeof(zb_64bit_addr_t)) |
Copy long address.
| dst | where to copy the address. |
| src | address to copy. |
| #define ZB_64BIT_ADDR_UNKNOWN | ( | addr | ) | ZB_MEMSET((addr), -1, 8) |
| #define ZB_64BIT_ADDR_ZERO | ( | addr | ) | ZB_MEMSET((addr), 0, 8) |
Clears long address.
| addr | address to clear. |
| #define ZB_64BIT_SIZE 8U |
| #define ZB_8BIT_SIZE 1U |
| #define ZB_ADDR_CMP | ( | addr_mode, | |
| addr1, | |||
| addr2 | |||
| ) |
| #define ZB_ADDR_U_CAST | ( | addr | ) | ((const zb_addr_u *)(const void *)(&(addr))) |
| #define ZB_ALIGNED_PRE |
| #define ZB_ARRAY_IDX_BY_ELEM | ( | ar, | |
| el | |||
| ) | ((el) - (ar)) |
| #define ZB_ARRAY_SIZE | ( | arr | ) | (sizeof((arr))/sizeof((arr)[0])) |
| #define ZB_ASSERT_IF_NOT_ALIGNED | ( | data_type, | |
| length | |||
| ) | ZB_ASSERT_COMPILE_DECL(((sizeof(data_type) % (length)) == 0U)) |
| #define ZB_ASSERT_IF_NOT_ALIGNED_TO_4 | ( | data_type | ) | ZB_ASSERT_IF_NOT_ALIGNED(data_type,4U) |
| #define ZB_ASSERT_VALUE_ALIGNED | ( | const_expr, | |
| length | |||
| ) | ZB_ASSERT_COMPILE_DECL((((const_expr) % (length)) == 0U)) |
| #define ZB_ASSERT_VALUE_ALIGNED_TO_4 | ( | const_expr | ) | ZB_ASSERT_VALUE_ALIGNED(const_expr, 4U) |
| #define ZB_ASSIGN_INT16 | ( | ptr, | |
| vp | |||
| ) | *((zb_int16_t*)(ptr)) = *(zb_int16_t*)(vp) |
| #define ZB_ASSIGN_INT32 | ( | ptr, | |
| vp | |||
| ) | *((zb_int32_t*)(ptr)) = *(zb_int32_t*)(vp) |
| #define ZB_ASSIGN_UINT16 | ( | ptr, | |
| vp | |||
| ) | *((zb_uint16_t*)(ptr)) = *(zb_uint16_t*)(vp) |
| #define ZB_ASSIGN_UINT32 | ( | ptr, | |
| vp | |||
| ) | *((zb_uint32_t*)(ptr)) = *(zb_uint32_t*)(vp) |
| #define ZB_B2U | ( | b | ) | (((b) != ZB_FALSE) ? (1U) : (0U)) |
| #define ZB_BETOH16 ZB_HTOBE16 |
| #define ZB_BETOH32 ZB_HTOBE32 |
| #define ZB_BITFIELD_CAST | ( | x | ) | (x) |
| #define ZB_CCM_KEY_IS_ZERO | ( | k | ) | (ZB_IS_64BIT_ADDR_ZERO((zb_uint8_t*)(k)) && ZB_IS_64BIT_ADDR_ZERO(((zb_uint8_t*)(k)) + 8U)) |
| #define ZB_CODE |
| #define ZB_CONST const |
| #define ZB_COPY_INT24 | ( | ptr, | |
| vp | |||
| ) | *((zb_int24_t*)(ptr)) = *(zb_int24_t*)(vp) |
| #define ZB_COPY_UINT24 | ( | ptr, | |
| vp | |||
| ) | *((zb_uint24_t*)(ptr)) = *(zb_uint24_t*)(vp) |
| #define ZB_CPP_STR | ( | x | ) | ZB_CPP_STR2(x) |
Create a string at compile time, like 0 - "0"
| #define ZB_CPP_STR2 | ( | x | ) | #x |
| #define ZB_DEPRECATED |
| #define ZB_EXTPANID_CMP ZB_64BIT_ADDR_CMP |
| #define ZB_EXTPANID_COPY ZB_64BIT_ADDR_COPY |
| #define ZB_EXTPANID_IS_ZERO ZB_IS_64BIT_ADDR_ZERO |
| #define ZB_EXTPANID_ZERO ZB_64BIT_ADDR_ZERO |
| #define ZB_FALSE 0U |
False value literal.
| #define ZB_FALSE_U ZB_FALSE |
| #define ZB_GET_HI_BYTE | ( | val | ) | (zb_uint8_t)(((val) >> 8U) & 0xFFU) |
| #define ZB_GET_LOW_BYTE | ( | val | ) | (zb_uint8_t)((val) & 0xFFU) |
| #define ZB_HTOBE16 | ( | ptr, | |
| val | |||
| ) | (*(zb_uint16_t *)(ptr)) = *((zb_uint16_t *)(val)) |
| #define ZB_HTOBE16_VAL | ( | ptr, | |
| val | |||
| ) | ((zb_uint16_t *)(ptr))[0] = (val) |
| #define ZB_HTOBE32 | ( | ptr, | |
| val | |||
| ) | ZB_MEMCPY(ptr, val, 4U) |
| #define ZB_HTOLE16 | ( | ptr, | |
| val | |||
| ) | zb_htole16((zb_uint8_t*)(ptr), (zb_uint8_t*)(val)) |
| #define ZB_HTOLE16_ONPLACE | ( | val | ) |
| #define ZB_HTOLE16_VAL | ( | ptr, | |
| val | |||
| ) |
| #define ZB_HTOLE32 | ( | ptr, | |
| val | |||
| ) | zb_htole32((zb_uint8_t*)(ptr), (zb_uint8_t*)(val)) |
| #define ZB_HTOLE32_ONPLACE | ( | val | ) | { zb_uint32_t _v = (val); ZB_HTOLE32(&(val), &_v); } |
| #define ZB_HTOLE32_VAL | ( | ptr, | |
| val | |||
| ) |
| #define ZB_HTOLE64 | ( | ptr, | |
| val | |||
| ) | zb_memcpy8(ptr, val) |
| #define ZB_IAR_CODE |
| #define ZB_IEEE_ADDR_CMP ZB_64BIT_ADDR_CMP |
| #define ZB_IEEE_ADDR_COPY ZB_64BIT_ADDR_COPY |
| #define ZB_IEEE_ADDR_IS_UNKNOWN ZB_IS_64BIT_ADDR_UNKNOWN |
| #define ZB_IEEE_ADDR_IS_VALID | ( | addr | ) | !(ZB_IEEE_ADDR_IS_ZERO(addr)||ZB_IEEE_ADDR_IS_UNKNOWN(addr)) |
| #define ZB_IEEE_ADDR_IS_ZERO ZB_IS_64BIT_ADDR_ZERO |
| #define ZB_IEEE_ADDR_UNKNOWN ZB_64BIT_ADDR_UNKNOWN |
| #define ZB_IEEE_ADDR_ZERO ZB_64BIT_ADDR_ZERO |
| #define ZB_INLINE |
| #define ZB_INT16_C | ( | c | ) | c |
| #define ZB_INT16_MAX 32767 |
| #define ZB_INT16_MIN (-32767 - 1) |
| #define ZB_INT32_C | ( | c | ) | c ## L |
| #define ZB_INT32_MAX 2147483647L |
| #define ZB_INT32_MIN (-2147483647L - 1) |
| #define ZB_INT8_C | ( | c | ) | c |
| #define ZB_INT8_MAX 127 |
| #define ZB_INT8_MIN (-127 - 1) |
| #define ZB_INT_MASK 0x7fffffffU |
| #define ZB_INT_MAX ZB_INT32_MAX |
| #define ZB_INT_MIN ZB_INT32_MIN |
| #define ZB_IS_64BIT_ADDR_UNKNOWN | ( | addr | ) | (ZB_MEMCMP((addr), (void const*)g_unknown_ieee_addr, 8) == 0) |
| #define ZB_IS_64BIT_ADDR_ZERO | ( | addr | ) | (ZB_MEMCMP((addr), (void const*)g_zero_addr, 8) == 0) |
Checks that long address is a zero one.
| addr | address to check. |
| #define ZB_LETOH16 ZB_HTOLE16 |
Convert 16-bits integer from the little endian to the host endian
| ptr | - destination pointer. It is ok if it not aligned to 2. |
| val | - source pointer. It is ok if it not aligned to 2. |
| #define ZB_LETOH16_ONPLACE ZB_HTOLE16_ONPLACE |
| #define ZB_LETOH24 ZB_HTOLE24 |
| #define ZB_LETOH32 ZB_HTOLE32 |
| #define ZB_LETOH32_ONPLACE ZB_HTOLE32_ONPLACE |
| #define ZB_LETOH48 ZB_HTOLE48 |
| #define ZB_LETOH64 | ( | dst, | |
| src | |||
| ) | zb_memcpy8((zb_uint8_t*)dst, (zb_uint8_t*)src) |
| #define ZB_NORETURN |
| #define ZB_OFFSETOF | ( | t, | |
| f | |||
| ) | ((zb_size_t)(&((t *)NULL)->f)) |
| #define ZB_PACKED_PRE |
| #define ZB_PACKED_STRUCT |
| #define ZB_PKT_16B_FIRST_BYTE 1U |
| #define ZB_PKT_16B_ZERO_BYTE 0U |
| #define ZB_PUT_NEXT_HTOLE16 | ( | ptr, | |
| val | |||
| ) |
| #define ZB_PUT_NEXT_HTOLE32 | ( | ptr, | |
| val | |||
| ) | (ptr) = zb_put_next_htole32((ptr), (val)) |
| #define ZB_PUT_NEXT_IEEE | ( | dst, | |
| src | |||
| ) | (dst) = zb_put_next_ieee((dst), (src)); |
| #define ZB_REGISTER register |
| #define ZB_REVERSE16 | ( | ptr, | |
| val | |||
| ) |
| #define ZB_REVERSE64 | ( | ptr, | |
| val | |||
| ) |
| #define ZB_S32_FROM_S24 | ( | x | ) | ((x & 0xFFFFFF) | ((x & 0x800000) ? 0xFF000000 : 0x0)) |
| #define ZB_S32_TO_S24 | ( | x | ) | ((zb_int32_t)(x & 0xFFFFFF)) |
| #define ZB_S64_FROM_S48 | ( | x | ) | ((x & 0xFFFFFFFFFFFF) | ((x & 0x800000000000) ? 0xFFFF000000000000 : 0x0)) |
| #define ZB_S64_TO_S48 | ( | x | ) | ((zb_int64_t)(x & 0xFFFFFFFFFFFF)) |
| #define ZB_SET_HI_BYTE | ( | res, | |
| val | |||
| ) | (res) = (((((zb_uint16_t)(val)) << 8U) & 0xFF00U) | (((zb_uint16_t)(res)) & 0xFFU)) |
| #define ZB_SET_LOW_BYTE | ( | res, | |
| val | |||
| ) | (res) = ((((zb_uint16_t)(res)) & 0xFF00U) | (((zb_uint16_t)(val)) & 0xFFU)) |
| #define ZB_SHORT_MAX ZB_INT32_MAX |
| #define ZB_SHORT_MIN ZB_INT32_MIN |
| #define ZB_SIGNED_SHIFT | ( | v, | |
| s | |||
| ) | ((zb_int_t)(v) >> (s)) |
| #define ZB_SIZEOF_FIELD | ( | type, | |
| field | |||
| ) | (sizeof(((type*)0)->field)) |
| #define ZB_STDC_90 |
| #define ZB_TRUE 1U |
True value literal.
| #define ZB_TRUE_U ZB_TRUE |
| #define ZB_U2B | ( | u | ) | (((u) != 0U) ? (ZB_TRUE) : (ZB_FALSE)) |
| #define ZB_UINT16_C | ( | c | ) | c ## U |
| #define ZB_UINT16_MAX 65535U |
| #define ZB_UINT16_MIN 0U |
| #define ZB_UINT32_C | ( | c | ) | c ## UL |
| #define ZB_UINT32_MAX 4294967295UL |
| #define ZB_UINT32_MIN 0UL |
| #define ZB_UINT8_C | ( | c | ) | c ## U |
| #define ZB_UINT8_MAX 255U |
| #define ZB_UINT8_MIN 0U |
| #define ZB_UINT_MAX ZB_UINT32_MAX |
| #define ZB_UINT_MIN 0UL |
| #define ZB_USHORT_MAX ZB_UINT32_MAX |
| #define ZB_VOID_ARGLIST void |
| #define ZB_WEAK |
| #define ZB_WEAK_PRE |
| #define ZB_XDATA |
| zb_64bit_addr_t |
8-bytes address (xpanid or long device address) base type.
| typedef zb_uint8_t zb_64bit_data_t[8] |
| typedef union zb_addr_u_t zb_addr_u |
Type to be used for boolean bit fields inside structure.
Type to be used for unsigned bit fields inside structure.
General purpose boolean type. For C90, 'zb_bool_t' is an alias of 'zb_uint8_t'. For C99, the availability of the 'stdbool.h' standard header is expected and 'zb_bool_t' is an alias of 'bool'. ZB_FALSE and ZB_TRUE are defined as macros for both standards.
Boolean type can be ZB_TRUE or ZB_FALSE.
To ensure that zb_bool_t always has the same size of one byte, static compile time assertions were added. See 'zb_common.h'.
Project-local char type.
Long (64-bit) extended Pan ID.
Long (64-bit) device address.
Project-local 2-byte signed int type.
Project-local 4-byte signed int type.
| typedef long long zb_int64_t |
Project-local 1-byte signed int type.
Int (at least 2 bytes).
| typedef zb_uint32_t zb_lbitfield_t |
Long int (at least 4 bytes).
| typedef zb_int32_t zb_ret_t |
Return type for ZB functions returning execution status.
Type to be used for signed bit fields inside structure.
Short int (can fit into single CPU register).
Project-local single precision float type.
Project-local size_t type.
Project-local unsigned char type.
| typedef zb_ushort_t zb_uindex_t |
Project-local 2-byte unsigned int type.
Project-local 4-byte unsigned int type.
| typedef unsigned long long zb_uint64_t |
Project-local 1-byte unsigned int type.
Unsigned int (at least 2 bytes).
Unsigned long int (at least 4 bytes).
Short unsigned int (can fit into single CPU register).
| enum zb_param_e |
| void zb_get_next_letoh16 | ( | zb_uint16_t * | dst, |
| const zb_uint8_t ** | src | ||
| ) |
| void zb_htole16 | ( | zb_uint8_t * | ptr, |
| zb_uint8_t * | val | ||
| ) |
| void zb_htole32 | ( | zb_uint8_t * | ptr, |
| zb_uint8_t * | val | ||
| ) |
| void* zb_put_next_2_htole16 | ( | zb_uint8_t * | dst, |
| zb_uint16_t | val1, | ||
| zb_uint16_t | val2 | ||
| ) |
| void* zb_put_next_2_htole32 | ( | zb_uint8_t * | dst, |
| zb_uint32_t | val1, | ||
| zb_uint32_t | val2 | ||
| ) |
| void* zb_put_next_htole16 | ( | zb_uint8_t * | dst, |
| zb_uint16_t | val | ||
| ) |
Put next 2-bite value into buffer, move pointer
To be used for headers compose.
| dst | - (in/out) address of the buffer pointer As a side effect it will be incremented by 2. |
| val | - value |
| void* zb_put_next_htole32 | ( | zb_uint8_t * | dst, |
| zb_uint32_t | val1 | ||
| ) |
| void* zb_put_next_ieee | ( | zb_uint8_t * | dst, |
| zb_ieee_addr_t | src | ||
| ) |
| const zb_64bit_addr_t g_unknown_ieee_addr |