Data Structures | |
| struct | zb_apsme_binding_req_s |
| APSME binding structure. More... | |
| struct | zb_aps_check_binding_req_s |
| struct | zb_aps_check_binding_resp_s |
| struct | zb_apsme_add_group_req_s |
| APSME-ADD-GROUP.request primitive parameters, should be passed to zb_zdo_add_group_req() More... | |
| struct | zb_apsme_add_group_conf_s |
| APSME-ADD-GROUP.confirm primitive parameters. More... | |
| struct | zb_apsme_remove_all_groups_req_s |
| APSME-REMOVE-ALL-GROUPS.request primitive parameters, should be passed to zb_zdo_remove_all_groups_req(). More... | |
| struct | zb_apsme_remove_all_groups_conf_s |
| APSME-REMOVE-ALL-GROUPS.confirm primitive parameters. More... | |
Functions | |
| zb_bool_t | zb_aps_is_endpoint_in_group (zb_uint16_t group_id, zb_uint8_t endpoint) |
| void | zb_apsme_bind_request (zb_uint8_t param) |
| APSME-BIND.request primitive. More... | |
| void | zb_apsme_unbind_request (zb_uint8_t param) |
| APSME-UNBIND.request primitive. More... | |
| void | zb_apsme_unbind_all (zb_uint8_t param) |
| Perform unbind all entries. This custom function and it is not described in Zigbee specification. More... | |
| void | zb_aps_check_binding_request (zb_bufid_t param) |
| Checks if the binding with specified parameters exists. More... | |
| void | zb_apsme_add_group_request (zb_uint8_t param) |
| APSME-ADD-GROUP.request primitive. More... | |
| void | zb_apsme_remove_group_request (zb_uint8_t param) |
| APSME-REMOVE-GROUP.request primitive. More... | |
| void | zb_apsme_remove_all_groups_request (zb_uint8_t param) |
| APSME-REMOVE-ALL-GROUPS.request primitive. More... | |
| typedef struct zb_aps_check_binding_req_s zb_aps_check_binding_req_t |
This data structure passed to zb_zdo_check_binding_request().
| typedef struct zb_aps_check_binding_resp_s zb_aps_check_binding_resp_t |
This data structure passed to callback passed to zb_zdo_check_binding_request().
| typedef struct zb_apsme_add_group_conf_s zb_apsme_add_group_conf_t |
APSME-ADD-GROUP.confirm primitive parameters.
| typedef struct zb_apsme_add_group_req_s zb_apsme_add_group_req_t |
APSME-ADD-GROUP.request primitive parameters, should be passed to zb_zdo_add_group_req()
| typedef struct zb_apsme_binding_req_s zb_apsme_binding_req_t |
APSME binding structure.
This data structure passed to zb_apsme_bind_request() and to zb_apsme_unbind_request().
APSME-REMOVE-ALL-GROUPS.confirm primitive parameters.
| typedef struct zb_apsme_remove_all_groups_req_s zb_apsme_remove_all_groups_req_t |
APSME-REMOVE-ALL-GROUPS.request primitive parameters, should be passed to zb_zdo_remove_all_groups_req().
| typedef struct zb_apsme_add_group_conf_s zb_apsme_remove_group_conf_t |
APSME-REMOVE-GROUP.confirm primitive parameters.
| typedef struct zb_apsme_add_group_req_s zb_apsme_remove_group_req_t |
APSME-REMOVE-GROUP.request primitive parameters, should be passed to zb_zdo_add_group_req()
| void zb_aps_check_binding_request | ( | zb_bufid_t | param | ) |
Checks if the binding with specified parameters exists.
| zb_bool_t zb_aps_is_endpoint_in_group | ( | zb_uint16_t | group_id, |
| zb_uint8_t | endpoint | ||
| ) |
| void zb_apsme_add_group_request | ( | zb_uint8_t | param | ) |
APSME-ADD-GROUP.request primitive.
| param | - index of buffer with parameter. See zb_apsme_add_group_req_t. |
| void zb_apsme_bind_request | ( | zb_uint8_t | param | ) |
APSME-BIND.request primitive.
| param | - index of buffer containing request data (see zb_apsme_binding_req_t). |
| void zb_apsme_remove_all_groups_request | ( | zb_uint8_t | param | ) |
APSME-REMOVE-ALL-GROUPS.request primitive.
| param | - index of buffer with parameter. See zb_apsme_remove_all_groups_req_t. |
| void zb_apsme_remove_group_request | ( | zb_uint8_t | param | ) |
APSME-REMOVE-GROUP.request primitive.
| param | - index of buffer with parameter. See zb_apsme_remove_group_req_t. |
| void zb_apsme_unbind_all | ( | zb_uint8_t | param | ) |
Perform unbind all entries. This custom function and it is not described in Zigbee specification.
| param | - not used. |
| void zb_apsme_unbind_request | ( | zb_uint8_t | param | ) |
APSME-UNBIND.request primitive.
| param | - index of buffer containing request data (see zb_apsme_binding_req_t). |