Logo
Developing with ZBOSS for Zigbee

Enumerations

enum  zb_zcl_price_set_received_block_threshold_e {
  ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK1_THRESHOLD = ZB_ZCL_ATTR_SET_WITH_ATTR_ID(ZB_ZCL_PRICE_SET_RECEIVED_BLOCK_THRESHOLD, 0x00), ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK2_THRESHOLD, ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK3_THRESHOLD, ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK4_THRESHOLD,
  ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK5_THRESHOLD, ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK6_THRESHOLD, ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK7_THRESHOLD, ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK8_THRESHOLD,
  ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK9_THRESHOLD, ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK10_THRESHOLD, ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK11_THRESHOLD, ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK12_THRESHOLD,
  ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK13_THRESHOLD, ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK14_THRESHOLD, ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK15_THRESHOLD
}
 Received Block Threshold Attributes Set. More...
 

Detailed Description

This set of attributes provides remote access to the Price server ReceivedBlockThresholds. The number of block thresholds is indicated by the NumberOfBlockThresholds field in the associated PublishTariffInformation command. The number of blocks is one greater than the number of thresholds.

Enumeration Type Documentation

§ zb_zcl_price_set_received_block_threshold_e

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_price.h>

Received Block Threshold Attributes Set.

See also
SE spec, D.4.2.2.11
Enumerator
ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK1_THRESHOLD 

The format of these attributes is the same as for the 'Delivered' Block Thresholds

ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK2_THRESHOLD 
ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK3_THRESHOLD 
ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK4_THRESHOLD 
ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK5_THRESHOLD 
ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK6_THRESHOLD 
ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK7_THRESHOLD 
ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK8_THRESHOLD 
ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK9_THRESHOLD 
ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK10_THRESHOLD 
ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK11_THRESHOLD 
ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK12_THRESHOLD 
ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK13_THRESHOLD 
ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK14_THRESHOLD 
ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK15_THRESHOLD