| #define ZB_ZCL_CLUSTER_ID_METERING_CLIENT_ROLE_GENERATED_CMD_LIST |
| #define ZB_ZCL_CLUSTER_ID_METERING_CLIENT_ROLE_RECEIVED_CMD_LIST ZB_ZCL_CLUSTER_ID_METERING_SERVER_ROLE_GENERATED_CMD_LIST |
| #define ZB_ZCL_CLUSTER_ID_METERING_SERVER_ROLE_GENERATED_CMD_LIST |
| #define ZB_ZCL_CLUSTER_ID_METERING_SERVER_ROLE_RECEIVED_CMD_LIST ZB_ZCL_CLUSTER_ID_METERING_CLIENT_ROLE_GENERATED_CMD_LIST |
| #define ZB_ZCL_METERING_GET_PROFILE_PAYLOAD_SIZE_IS_VALID | ( | current_size | ) | ((current_size >= sizeof(zb_zcl_metering_get_profile_payload_t) ? ZB_TRUE : ZB_FALSE)) |
| #define ZB_ZCL_METERING_SEND_CMD_GET_PROFILE | ( | _param, | |
| _dst_addr, | |||
| _addr_mode, | |||
| _dst_ep, | |||
| _src_ep, | |||
| _payload, | |||
| cb | |||
| ) |
Macro for call zb_zcl_metering_send_cmd_get_profile function
| #define ZB_ZCL_METERING_SEND_CMD_GET_PROFILE_RESPONSE | ( | _param, | |
| _dst_addr, | |||
| _addr_mode, | |||
| _dst_ep, | |||
| _src_ep, | |||
| _payload, | |||
| _pl_size, | |||
| cb | |||
| ) |
Macro for call zb_zcl_metering_send_cmd_get_profile_response function
| #define ZB_ZCL_METERING_SEND_CMD_GET_SAMPLED_DATA | ( | _param, | |
| _dst_addr, | |||
| _addr_mode, | |||
| _dst_ep, | |||
| _src_ep, | |||
| _payload, | |||
| cb | |||
| ) |
Macro for call zb_zcl_metering_send_cmd_get_sampled_data function
| #define ZB_ZCL_METERING_SEND_CMD_GET_SAMPLED_DATA_RESPONSE | ( | _param, | |
| _dst_addr, | |||
| _addr_mode, | |||
| _dst_ep, | |||
| _src_ep, | |||
| _payload, | |||
| _pl_size, | |||
| cb | |||
| ) |
Macro for call zb_zcl_metering_send_cmd_get_sampled_data_response function
| #define ZB_ZCL_METERING_SEND_CMD_GET_SNAPSHOT | ( | _param, | |
| _dst_addr, | |||
| _addr_mode, | |||
| _dst_ep, | |||
| _src_ep, | |||
| _payload, | |||
| cb | |||
| ) |
Macro for call zb_zcl_metering_send_cmd_get_snapshot function
| #define ZB_ZCL_METERING_SEND_CMD_PUBLISH_SNAPSHOT | ( | _param, | |
| _dst_addr, | |||
| _addr_mode, | |||
| _dst_ep, | |||
| _src_ep, | |||
| _payload, | |||
| cb | |||
| ) |
Macro for call zb_zcl_metering_send_cmd_publish_snapshot function
| #define ZB_ZCL_METERING_SEND_CMD_REQUEST_FAST_POLL_MODE | ( | _param, | |
| _dst_addr, | |||
| _addr_mode, | |||
| _dst_ep, | |||
| _src_ep, | |||
| _payload, | |||
| cb | |||
| ) |
Macro for call zb_zcl_metering_send_cmd_request_fast_poll_mode function
| #define ZB_ZCL_METERING_SEND_CMD_REQUEST_FAST_POLL_MODE_RESPONSE | ( | _param, | |
| _dst_addr, | |||
| _addr_mode, | |||
| _dst_ep, | |||
| _src_ep, | |||
| _payload, | |||
| cb | |||
| ) |
Macro for call zb_zcl_metering_send_cmd_request_fast_poll_mode_response function
SnapshotPayloadType 2 = Block Information Delivered Set
SnapshotPayloadType 3 = Block Information Received Set
| typedef struct zb_zcl_metering_block_tier_delivered_no_billing_payload_s zb_zcl_metering_block_tier_delivered_no_billing_payload_t |
SnapshotPayloadType 6 = Block Tier Information Set Delivered (No Billing)
| typedef struct zb_zcl_metering_block_tier_received_no_billing_payload_s zb_zcl_metering_block_tier_received_no_billing_payload_t |
SnapshotPayloadType 7 = Block Tier Information Set Received (No Billing)
| typedef enum zb_zcl_metering_cli_cmd_e zb_zcl_metering_cli_cmd_t |
Metering cluster client command identifiers.
GetProfile command payload
| typedef struct zb_zcl_metering_get_profile_response_payload_s zb_zcl_metering_get_profile_response_payload_t |
GetProfileResponse command payload
| typedef struct zb_zcl_metering_get_sampled_data_payload_s zb_zcl_metering_get_sampled_data_payload_t |
GetSampledData command payload
| typedef struct zb_zcl_metering_get_sampled_data_response_payload_s zb_zcl_metering_get_sampled_data_response_payload_t |
GetSampledDataResponse command payload
GetSnapshot command payload
| typedef struct zb_zcl_metering_publish_snapshot_payload_s zb_zcl_metering_publish_snapshot_payload_t |
PublishSnapshot command payload
| typedef struct zb_zcl_metering_request_fast_poll_mode_payload_s zb_zcl_metering_request_fast_poll_mode_payload_t |
RequestFastPollMode command payload
| typedef struct zb_zcl_metering_request_fast_poll_mode_response_payload_s zb_zcl_metering_request_fast_poll_mode_response_payload_t |
RequestFastPollModeResponse command payload
The format of the Snapshot Sub-Payload differs depending on the SnapshotPayloadType
| typedef enum zb_zcl_metering_srv_cmd_e zb_zcl_metering_srv_cmd_t |
Metering cluster server command identifiers.
| typedef struct zb_zcl_metering_tou_delivered_no_billing_payload_s zb_zcl_metering_tou_delivered_no_billing_payload_t |
SnapshotPayloadType 4 = TOU Information Set Delivered (No Billing)
SnapshotPayloadType 0 = TOU Information Delivered Set
| typedef struct zb_zcl_metering_tou_received_no_billing_payload_s zb_zcl_metering_tou_received_no_billing_payload_t |
SnapshotPayloadType 5 = TOU Information Set Received (No Billing)
SnapshotPayloadType 1 = TOU Information Received Set
Metering cluster client command identifiers.
Profile Interval Period
Sample Type Enumerations
Snapshot Cause BitMap
Snapshot Payload Type
Metering cluster server command identifiers.
Status Field Values
| void zb_zcl_metering_send_cmd_get_profile | ( | zb_uint8_t | param, |
| zb_addr_u * | dst_addr, | ||
| zb_aps_addr_mode_t | dst_addr_mode, | ||
| zb_uint8_t | dst_ep, | ||
| zb_uint8_t | src_ep, | ||
| zb_zcl_metering_get_profile_payload_t * | payload, | ||
| zb_callback_t | cb | ||
| ) |
Function for send GetProfile command. On receiver's side callback ZCL device callback ZB_ZCL_REGISTER_DEVICE_CB will be called with ZB_ZCL_METERING_GET_PROFILE_CB_ID
| param | - Reference to buffer. |
| dst_addr | - Address of the device to send command to. |
| dst_addr_mode | - Address mode for dst_addr. |
| dst_ep | - Destination endpoint. |
| src_ep | - Current endpoint. |
| payload | - Packet payload (ref to zb_zcl_metering_get_profile_payload_t). |
| cb | - Callback which should be called when the ZCL stack receives APS ack. |
| void zb_zcl_metering_send_cmd_get_profile_response | ( | zb_uint8_t | param, |
| const zb_addr_u * | dst_addr, | ||
| zb_aps_addr_mode_t | dst_addr_mode, | ||
| zb_uint8_t | dst_ep, | ||
| zb_uint8_t | src_ep, | ||
| const zb_zcl_metering_get_profile_response_payload_t * | pl, | ||
| zb_uint8_t | pl_size, | ||
| zb_uint8_t | tsn, | ||
| zb_callback_t | cb | ||
| ) |
Function for send GetProfileResponse command. On receiver's side callback ZCL device callback ZB_ZCL_REGISTER_DEVICE_CB will be called with ZB_ZCL_METERING_GET_PROFILE_RESPONSE_CB_ID
| param | - Reference to buffer. |
| dst_addr | - Address of the device to send command to. |
| dst_addr_mode | - Address mode for dst_addr. |
| dst_ep | - Destination endpoint. |
| src_ep | - Current endpoint. |
| pl | - Packet payload (ref to zb_zcl_metering_get_profile_response_payload_t). |
| pl_size | - size in bytes of input payload. Stack can calculate actual payload size. Set pl_size to 0 for it. |
| tsn | - transaction sequence number of response |
| cb | - Callback which should be called when the ZCL stack receives APS ack. |
| void zb_zcl_metering_send_cmd_get_sampled_data | ( | zb_uint8_t | param, |
| zb_addr_u * | dst_addr, | ||
| zb_aps_addr_mode_t | dst_addr_mode, | ||
| zb_uint8_t | dst_ep, | ||
| zb_uint8_t | src_ep, | ||
| zb_zcl_metering_get_sampled_data_payload_t * | payload, | ||
| zb_callback_t | cb | ||
| ) |
Function for send GetSampledData command. On receiver's side callback ZCL device callback ZB_ZCL_REGISTER_DEVICE_CB will be called with ZB_ZCL_METERING_GET_SAMPLED_DATA_CB_ID
| param | - Reference to buffer. |
| dst_addr | - Address of the device to send command to. |
| dst_addr_mode | - Address mode for dst_addr. |
| dst_ep | - Destination endpoint. |
| src_ep | - Current endpoint. |
| payload | - Packet payload (ref to zb_zcl_metering_get_sampled_data_payload_t). |
| cb | - Callback which should be called when the ZCL stack receives APS ack. |
| void zb_zcl_metering_send_cmd_get_sampled_data_response | ( | zb_uint8_t | param, |
| const zb_addr_u * | dst_addr, | ||
| zb_aps_addr_mode_t | dst_addr_mode, | ||
| zb_uint8_t | dst_ep, | ||
| zb_uint8_t | src_ep, | ||
| const zb_zcl_metering_get_sampled_data_response_payload_t * | pl, | ||
| zb_uint8_t | pl_size, | ||
| zb_uint8_t | tsn, | ||
| zb_callback_t | cb | ||
| ) |
Function for send GetSampledDataResponse command. On receiver's side callback ZCL device callback ZB_ZCL_REGISTER_DEVICE_CB will be called with ZB_ZCL_METERING_GET_SAMPLED_DATA_RESPONSE_CB_ID
| param | - Reference to buffer. |
| dst_addr | - Address of the device to send command to. |
| dst_addr_mode | - Address mode for dst_addr. |
| dst_ep | - Destination endpoint. |
| src_ep | - Current endpoint. |
| pl | - Packet payload (ref to zb_zcl_metering_get_sampled_data_response_payload_t). |
| pl_size | - size in bytes of input payload. Stack can calculate actual payload size. Set pl_size to 0 for it. |
| tsn | - transaction sequence number of response |
| cb | - Callback which should be called when the ZCL stack receives APS ack. |
| void zb_zcl_metering_send_cmd_get_snapshot | ( | zb_uint8_t | param, |
| zb_addr_u * | dst_addr, | ||
| zb_aps_addr_mode_t | dst_addr_mode, | ||
| zb_uint8_t | dst_ep, | ||
| zb_uint8_t | src_ep, | ||
| zb_zcl_metering_get_snapshot_payload_t * | payload, | ||
| zb_callback_t | cb | ||
| ) |
Function for send GetSnapshot command. On receiver's side callback ZCL device callback ZB_ZCL_REGISTER_DEVICE_CB will be called with ZB_ZCL_METERING_GET_SNAPSHOT_CB_ID
| param | - Reference to buffer. |
| dst_addr | - Address of the device to send command to. |
| dst_addr_mode | - Address mode for dst_addr. |
| dst_ep | - Destination endpoint. |
| src_ep | - Current endpoint. |
| payload | - Packet payload (ref to zb_zcl_metering_get_snapshot_payload_t). |
| cb | - Callback which should be called when the ZCL stack receives APS ack. |
| void zb_zcl_metering_send_cmd_publish_snapshot | ( | zb_uint8_t | param, |
| const zb_addr_u * | dst_addr, | ||
| zb_aps_addr_mode_t | dst_addr_mode, | ||
| zb_uint8_t | dst_ep, | ||
| zb_uint8_t | src_ep, | ||
| const zb_zcl_metering_publish_snapshot_payload_t * | pl, | ||
| zb_callback_t | cb | ||
| ) |
Function for send PublishSnapshot command. On receiver's side callback ZCL device callback ZB_ZCL_REGISTER_DEVICE_CB will be called with ZB_ZCL_METERING_PUBLISH_SNAPSHOT_CB_ID
| param | - Reference to buffer. |
| dst_addr | - Address of the device to send command to. |
| dst_addr_mode | - Address mode for dst_addr. |
| dst_ep | - Destination endpoint. |
| src_ep | - Current endpoint. |
| pl | - Packet payload (ref to zb_zcl_metering_publish_snapshot_payload_t). |
| cb | - Callback which should be called when the ZCL stack receives APS ack. |
| void zb_zcl_metering_send_cmd_request_fast_poll_mode | ( | zb_uint8_t | param, |
| zb_addr_u * | dst_addr, | ||
| zb_aps_addr_mode_t | dst_addr_mode, | ||
| zb_uint8_t | dst_ep, | ||
| zb_uint8_t | src_ep, | ||
| zb_zcl_metering_request_fast_poll_mode_payload_t * | payload, | ||
| zb_callback_t | cb | ||
| ) |
Function for send RequestFastPollMode command. On receiver's side callback ZCL device callback ZB_ZCL_REGISTER_DEVICE_CB will be called with ZB_ZCL_METERING_REQUEST_FAST_POLL_MODE_CB_ID
| param | - Reference to buffer. |
| dst_addr | - Address of the device to send command to. |
| dst_addr_mode | - Address mode for dst_addr. |
| dst_ep | - Destination endpoint. |
| src_ep | - Current endpoint. |
| payload | - Packet payload (ref to zb_zcl_metering_request_fast_poll_mode_payload_t). |
| cb | - Callback which should be called when the ZCL stack receives APS ack. |
| void zb_zcl_metering_send_cmd_request_fast_poll_mode_response | ( | zb_uint8_t | param, |
| const zb_addr_u * | dst_addr, | ||
| zb_aps_addr_mode_t | dst_addr_mode, | ||
| zb_uint8_t | dst_ep, | ||
| zb_uint8_t | src_ep, | ||
| const zb_zcl_metering_request_fast_poll_mode_response_payload_t * | pl, | ||
| zb_uint8_t | pl_size, | ||
| zb_uint8_t | tsn, | ||
| zb_callback_t | cb | ||
| ) |
Function for send RequestFastPollMode command. On receiver's side callback ZCL device callback ZB_ZCL_REGISTER_DEVICE_CB will be called with ZB_ZCL_METERING_REQUEST_FAST_POLL_MODE_CB_ID
| param | - Reference to buffer. |
| dst_addr | - Address of the device to send command to. |
| dst_addr_mode | - Address mode for dst_addr. |
| dst_ep | - Destination endpoint. |
| src_ep | - Current endpoint. |
| pl | - Packet payload (ref to zb_zcl_metering_request_fast_poll_mode_response_payload_t). |
| pl_size | - size in bytes of input payload. Stack can calculate actual payload size. Set pl_size to 0 for it. |
| tsn | - transaction sequence number of response |
| cb | - Callback which should be called when the ZCL stack receives APS ack. |