Data Structures | |
| struct | zb_zcl_identify_effect_req_s |
| Structured representation of Trigger effect command payload. More... | |
| struct | zb_zcl_identify_effect_value_param_s |
| Declare change Identify attribute for User Application. More... | |
| struct | zb_zcl_identify_effect_user_app_schedule_e |
| struct | zb_zcl_identify_req_s |
| Structured representation of Identify command payload. More... | |
| struct | zb_zcl_identify_query_res_s |
| Structured representation of Identify Query Response command payload. More... | |
Macros | |
| #define | ZB_ZCL_IDENTIFY_SEND_IDENTIFY_REQ( buffer, time, addr, dst_addr_mode, dst_ep, ep, prfl_id, def_resp, cb) |
| Send Identify command. More... | |
| #define | ZB_ZCL_IDENTIFY_SEND_IDENTIFY_QUERY_REQ( buffer, addr, dst_addr_mode, dst_ep, ep, prfl_id, def_resp, cb) |
| Send Identify Query command. More... | |
| #define | ZB_ZCL_IDENTIFY_SEND_IDENTIFY_QUERY_RES( buffer, time, addr, dst_addr_mode, dst_ep, ep, prfl_id, seq_num, aps_secured) |
| Send Identify Query Response command. More... | |
| #define | ZB_ZCL_IDENTIFY_GET_IDENTIFY_REQ(data_ptr, buffer, status) |
| Identify cluster Identify command payload structured read. More... | |
| #define | ZB_ZCL_IDENTIFY_GET_IDENTIFY_QUERY_RES(data_ptr, buffer, status) |
| Identify cluster Identify Query Response command payload structured read. More... | |
Typedefs | |
| typedef struct zb_zcl_identify_req_s | zb_zcl_identify_req_t |
| Structured representation of Identify command payload. More... | |
| typedef struct zb_zcl_identify_query_res_s | zb_zcl_identify_query_res_t |
| Structured representation of Identify Query Response command payload. More... | |
Functions | |
| zb_uint8_t | zb_zcl_start_identifying (zb_uint8_t endpoint, zb_uint16_t timeout) |
| Start identify process on given endpoint. More... | |
| void | zb_zcl_stop_identifying (zb_uint8_t endpoint) |
| Stop identify process on given endpoint Complimentary function to zb_zcl_start_identifying. Used to force identify termination before timeout provided to zb_zcl_start_identifying is elapsed. More... | |
| zb_uint8_t | zb_zcl_is_identifying (zb_uint8_t endpoint) |
| Indicates that endpoint supports Identify cluster and is identifying. More... | |
Identify cluster attributes | |
| enum | zb_zcl_identify_attr_e { ZB_ZCL_ATTR_IDENTIFY_IDENTIFY_TIME_ID = 0x0000 } |
| Identify cluster attribute identifier. More... | |
| #define | ZB_ZCL_IDENTIFY_CLUSTER_REVISION_DEFAULT ((zb_uint16_t)0x0002u) |
| Default value for Identify cluster revision global attribute. More... | |
| #define | ZB_ZCL_IDENTIFY_IDENTIFY_TIME_DEFAULT_VALUE 0x0000 |
| Default value for Identify attribute. More... | |
Inform User App about ZCL Identify cluster command and change attributes. | |
Internal structures and define-procedure for inform User App about ZCL Identify cluster command and change attributes. | |
| typedef struct zb_zcl_identify_effect_value_param_s | zb_zcl_identify_effect_value_param_t |
| Declare change Identify attribute for User Application. More... | |
| typedef struct zb_zcl_identify_effect_user_app_schedule_e | zb_zcl_identify_effect_user_app_schedule_t |
| #define | ZB_ZCL_IDENTIFY_EFFECT_SCHEDULE_USER_APP(buffer, pcmd_info, effectId, effectVar) |
Identify cluster implementation supports Identify command and Identify Query request-response command pair. All these commands have simple payload. Both Identify and Identify Query request are being processed, and Identify Query response is being generated in ZCL internals.
| #define ZB_ZCL_IDENTIFY_CLUSTER_REVISION_DEFAULT ((zb_uint16_t)0x0002u) |
Default value for Identify cluster revision global attribute.
| #define ZB_ZCL_IDENTIFY_EFFECT_SCHEDULE_USER_APP | ( | buffer, | |
| pcmd_info, | |||
| effectId, | |||
| effectVar | |||
| ) |
| #define ZB_ZCL_IDENTIFY_GET_IDENTIFY_QUERY_RES | ( | data_ptr, | |
| buffer, | |||
| status | |||
| ) |
Identify cluster Identify Query Response command payload structured read.
| data_ptr | - pointer to a variable of type zb_zcl_identify_query_res_t |
| buffer | containing the packet (by pointer). |
| status | - variable to put parse status to (see zb_zcl_parse_status_t). |
| #define ZB_ZCL_IDENTIFY_GET_IDENTIFY_REQ | ( | data_ptr, | |
| buffer, | |||
| status | |||
| ) |
Identify cluster Identify command payload structured read.
| data_ptr | - pointer to a variable of type zb_zcl_identify_req_t |
| buffer | containing the packet (by pointer). |
| status | - variable to put parse status to (see zb_zcl_parse_status_t). |
| #define ZB_ZCL_IDENTIFY_GET_TRIGGER_VARIANT_REQ | ( | data_ptr, | |
| buffer, | |||
| status | |||
| ) |
Parses Trigger effect command.
| data_ptr | - pointer to a variable of type zb_zcl_identify_effect_req_s. |
| buffer | containing the packet (by pointer). |
| status | - variable to put parse status to (see zb_zcl_parse_status_t). |
| #define ZB_ZCL_IDENTIFY_IDENTIFY_TIME_DEFAULT_VALUE 0x0000 |
Default value for Identify attribute.
| #define ZB_ZCL_IDENTIFY_SEND_IDENTIFY_QUERY_REQ | ( | buffer, | |
| addr, | |||
| dst_addr_mode, | |||
| dst_ep, | |||
| ep, | |||
| prfl_id, | |||
| def_resp, | |||
| cb | |||
| ) |
Send Identify Query command.
| buffer | to put packet to |
| addr | - address to send packet to |
| dst_addr_mode | - addressing mode |
| dst_ep | - destination endpoint |
| ep | - sending endpoint |
| prfl_id | - profile identifier |
| def_resp | - flag "Default response required" |
| cb | - callback for getting command send status |
| #define ZB_ZCL_IDENTIFY_SEND_IDENTIFY_QUERY_RES | ( | buffer, | |
| time, | |||
| addr, | |||
| dst_addr_mode, | |||
| dst_ep, | |||
| ep, | |||
| prfl_id, | |||
| seq_num, | |||
| aps_secured | |||
| ) |
Send Identify Query Response command.
| buffer | to put packet to |
| time | the device will be identifying |
| addr | - address to send packet to |
| dst_addr_mode | - addressing mode |
| dst_ep | - destination endpoint |
| ep | - sending endpoint |
| prfl_id | - profile identifier |
| seq_num | - sequence number |
| aps_secured | - APS security mode |
| #define ZB_ZCL_IDENTIFY_SEND_IDENTIFY_REQ | ( | buffer, | |
| time, | |||
| addr, | |||
| dst_addr_mode, | |||
| dst_ep, | |||
| ep, | |||
| prfl_id, | |||
| def_resp, | |||
| cb | |||
| ) |
Send Identify command.
| buffer | to put packet to |
| time | the device will be identifying |
| addr | - address to send packet to |
| dst_addr_mode | - addressing mode |
| dst_ep | - destination endpoint |
| ep | - sending endpoint |
| prfl_id | - profile identifier |
| def_resp | - flag "Default response required" |
| cb | - callback for getting command send status |
| #define ZB_ZCL_IDENTIFY_SEND_TRIGGER_VARIANT_REQ | ( | buffer, | |
| addr, | |||
| dst_addr_mode, | |||
| dst_ep, | |||
| ep, | |||
| prof_id, | |||
| def_resp, | |||
| cb, | |||
| effect_id, | |||
| effect_var | |||
| ) |
Send Trigger effect command.
| buffer | to put packet to |
| addr | - address to send packet to |
| dst_addr_mode | - addressing mode |
| dst_ep | - destination endpoint |
| ep | - sending endpoint |
| prof_id | - profile identifier |
| def_resp | - flag "Default response required" |
| cb | - callback for getting command send status |
| effect_id | - effect identify, see zb_zcl_identify_trigger_effect_e |
| effect_var | - effect variant, see zb_zcl_identify_trigger_variant_e |
| typedef struct zb_zcl_identify_effect_req_s zb_zcl_identify_effect_req_t |
Structured representation of Trigger effect command payload.
| typedef struct zb_zcl_identify_effect_user_app_schedule_e zb_zcl_identify_effect_user_app_schedule_t |
Struct for invoke User App & continue after
Declare change Identify attribute for User Application.
| typedef struct zb_zcl_identify_query_res_s zb_zcl_identify_query_res_t |
Structured representation of Identify Query Response command payload.
| typedef struct zb_zcl_identify_req_s zb_zcl_identify_req_t |
Structured representation of Identify command payload.
Command identifiers for "Identify" cluster.
Effect identifier enum
| zb_uint8_t zb_zcl_is_identifying | ( | zb_uint8_t | endpoint | ) |
Indicates that endpoint supports Identify cluster and is identifying.
| endpoint | number to analyze |
| zb_uint8_t zb_zcl_start_identifying | ( | zb_uint8_t | endpoint, |
| zb_uint16_t | timeout | ||
| ) |
Start identify process on given endpoint.
| endpoint | - endpoint to start identifying on |
| timeout | - time (in seconds) after which identifying will stop |
| void zb_zcl_stop_identifying | ( | zb_uint8_t | endpoint | ) |
Stop identify process on given endpoint Complimentary function to zb_zcl_start_identifying. Used to force identify termination before timeout provided to zb_zcl_start_identifying is elapsed.
| endpoint | Endpoint |