Logo
Developing with ZBOSS for Zigbee
ZCL IAS Zone cluster

Data Structures

struct  zb_zcl_ias_zone_init_test_mode_ha_s
 Structure representsation of Initiate Test Mode - Errata to 05-3520-29 Spec, 1.1.23.2.2.1. More...
 
struct  zb_zcl_ias_zone_status_change_not_s
 Structure representsation of Zone Status Change Notification see ZCL spec 8.2.2.4.1.1. More...
 
struct  zb_zcl_ias_zone_enroll_request_s
 Structure representsation of "Zone Enroll Request" command see ZCL spec 8.2.2.4.1.2. More...
 
struct  zb_zcl_ias_zone_enroll_res_s
 Structure representsation of Enroll response command payload see ZCL spec 8.2.2.3.1.1. More...
 
struct  zb_zcl_ias_zone_status_param_s
 Declare Set/Clear Zone Status bits. More...
 
struct  zb_zcl_ias_zone_notification_param_s
 Structure is used to pass parameters for ZoneStatus notification command. More...
 
struct  zb_zcl_ias_zone_int_ctx_s
 
struct  zb_zcl_ias_zone_enroll_response_value_param_s
 Declare run Enroll Response command for User Application. More...
 
struct  zb_zcl_ias_zone_enroll_response_user_app_schedule_e
 

Macros

#define ZB_ZCL_IAS_ZONE_SET_BITS(buffer, ep, set_bits)
 Set Zone Status bits custom server command. More...
 
#define ZB_ZCL_IAS_ZONE_CLEAR_BITS(buffer, ep, set_bits)
 Clear Zone Status bits custom server command. More...
 
#define ZB_ZCL_IAS_ZONE_ENROLL_RESPONSE_SCHEDULE_USER_APP(buffer, pcmd_info, enroll_response_, zone_id_)
 

Typedefs

typedef struct zb_zcl_ias_zone_status_param_s zb_zcl_ias_zone_status_param_t
 Declare Set/Clear Zone Status bits. More...
 
typedef struct zb_zcl_ias_zone_notification_param_s zb_zcl_ias_zone_notification_param_t
 Structure is used to pass parameters for ZoneStatus notification command. More...
 
typedef zb_ret_t(* zb_ias_zone_app_callback_t) (zb_uint8_t param, zb_uint16_t general_val)
 
typedef struct zb_zcl_ias_zone_int_ctx_s zb_zcl_ias_zone_int_ctx_t
 
typedef struct zb_zcl_ias_zone_enroll_response_value_param_s zb_zcl_ias_zone_enroll_response_value_param_t
 Declare run Enroll Response command for User Application. More...
 
typedef struct zb_zcl_ias_zone_enroll_response_user_app_schedule_e zb_zcl_ias_zone_enroll_response_user_app_schedule_t
 

Enumerations

enum  zb_zcl_general_cb_params_e { ZB_ZCL_VALID_CIE_ADDR_SET = 1, ZB_ZCL_CURR_ZONE_SENSITIVITY_LEVEL_SET = 2, ZB_ZCL_INIT_TEST_MODE = 3, ZB_ZCL_INIT_NORMAL_MODE = 4 }
 

Functions

void zb_zcl_ias_zone_change_status (zb_uint8_t param)
 
zb_bool_t zb_zcl_ias_zone_set_status (zb_uint8_t ep, zb_uint16_t new_val, zb_uint16_t delay, zb_uint8_t buf_param)
 Use this function to change IAS Zone status. This function will set new value of ZoneStatus and will send Zone status change notification. More...
 
void zb_zcl_ias_zone_register_cb (zb_uint8_t endpoint, zb_callback_t process_result_cb, zb_ias_zone_app_callback_t general_cb)
 Registry callbacks to get status of Zone Status Change Notification command. More...
 
zb_bool_t zb_zcl_ias_zone_check_attr_notify (zb_uint8_t buf_param)
 checks, if Zone Status change notification should be sent and schedules command if it is needed More...
 
void zb_zcl_ias_zone_send_status_change_not (zb_uint8_t param)
 fills in notification command and sends it More...
 
void zb_zcl_ias_zone_check_cie_addr_on_zcl_initialization (zb_uint8_t ep_id)
 checks cie address on zcl initialization More...
 
zb_ret_t zb_zcl_ias_zone_put_cie_address_to_binding_whitelist (zb_uint8_t endpoint)
 puts cie command to binding whitelist table More...
 
void zb_zcl_ias_set_attr_val_post_process (zb_zcl_parsed_hdr_t *cmd_info, zb_uint16_t attr_id, zb_uint8_t *value)
 IAS Zone specific set attribute value postprocessing. More...
 

IAS Zone cluster attributes

enum  zb_zcl_ias_zone_attr_e {
  ZB_ZCL_ATTR_IAS_ZONE_ZONESTATE_ID = 0x0000, ZB_ZCL_ATTR_IAS_ZONE_ZONETYPE_ID = 0x0001, ZB_ZCL_ATTR_IAS_ZONE_ZONESTATUS_ID = 0x0002, ZB_ZCL_ATTR_IAS_ZONE_IAS_CIE_ADDRESS_ID = 0x0010,
  ZB_ZCL_ATTR_IAS_ZONE_ZONEID_ID = 0x0011, ZB_ZCL_ATTR_IAS_ZONE_NUMBER_OF_ZONE_SENSITIVITY_LEVELS_SUPPORTED_ID = 0x0012, ZB_ZCL_ATTR_IAS_ZONE_CURRENT_ZONE_SENSITIVITY_LEVEL_ID = 0x0013, ZB_ZCL_ATTR_CUSTOM_ZGP_CALIBRATION = 0x8000,
  ZB_ZCL_ATTR_CUSTOM_ZGP_CLOUD_ACK = 0x8003, ZB_ZCL_ATTR_CUSTOM_CIE_ADDR_IS_SET = 0xE000, ZB_ZCL_ATTR_CUSTOM_CIE_EP = 0xE001, ZB_ZCL_ATTR_CUSTOM_CIE_SHORT_ADDR = 0xE002,
  ZB_ZCL_ATTR_IAS_ZONE_INT_CTX_ID = 0xeffe
}
 IAS Zone cluster attribute identifiers. More...
 
enum  zb_zcl_ias_zone_zonestate_e { ZB_ZCL_IAS_ZONE_ZONESTATE_NOT_ENROLLED = 0, ZB_ZCL_IAS_ZONE_ZONESTATE_ENROLLED = 1 }
 IAS Zone ZoneState value. More...
 
enum  zb_zcl_ias_zone_zonetype_e {
  ZB_ZCL_IAS_ZONE_ZONETYPE_STANDARD_CIE = 0x0000, ZB_ZCL_IAS_ZONE_ZONETYPE_MOTION = 0x000d, ZB_ZCL_IAS_ZONE_ZONETYPE_CONTACT_SWITCH = 0x0015, ZB_ZCL_IAS_ZONE_ZONETYPE_FIRE_SENSOR = 0x0028,
  ZB_ZCL_IAS_ZONE_ZONETYPE_WATER_SENSOR = 0x002a, ZB_ZCL_IAS_ZONE_ZONETYPE_GAS_SENSOR = 0x002b, ZB_ZCL_IAS_ZONE_ZONETYPE_PERSONAL_EMERGENCY = 0x002c, ZB_ZCL_IAS_ZONE_ZONETYPE_VIBRATION_MOVEMENT = 0x002d,
  ZB_ZCL_IAS_ZONE_ZONETYPE_REMOTE_CONTROL = 0x010f, ZB_ZCL_IAS_ZONE_ZONETYPE_KEY_FOB = 0x0115, ZB_ZCL_IAS_ZONE_ZONETYPE_KEYPAD = 0x021d, ZB_ZCL_IAS_ZONE_ZONETYPE_STANDARD_WARNING = 0x0225,
  ZB_ZCL_IAS_ZONE_ZONETYPE_MANUF_SPEC = 0x8000, ZB_ZCL_IAS_ZONE_ZONETYPE_INVALID = 0xffff
}
 IAS Zone ZoneType value. More...
 
enum  zb_zcl_ias_zone_zonestatus_e {
  ZB_ZCL_IAS_ZONE_ZONE_STATUS_ALARM1 = 1 << 0, ZB_ZCL_IAS_ZONE_ZONE_STATUS_ALARM2 = 1 << 1, ZB_ZCL_IAS_ZONE_ZONE_STATUS_TAMPER = 1 << 2, ZB_ZCL_IAS_ZONE_ZONE_STATUS_BATTERY = 1 << 3,
  ZB_ZCL_IAS_ZONE_ZONE_STATUS_SUPERVISION = 1 << 4, ZB_ZCL_IAS_ZONE_ZONE_STATUS_RESTORE = 1 << 5, ZB_ZCL_IAS_ZONE_ZONE_STATUS_TROUBLE = 1 << 6, ZB_ZCL_IAS_ZONE_ZONE_STATUS_AC_MAINS = 1 << 7,
  ZB_ZCL_IAS_ZONE_ZONE_STATUS_TEST = 1 << 8, ZB_ZCL_IAS_ZONE_ZONE_STATUS_BATTERY_DEFECT = 1 << 9
}
 IAS Zone ZoneStatus attribute flags. More...
 
#define ZB_ZCL_IAS_ZONE_ZONESTATE_DEF_VALUE   ZB_ZCL_IAS_ZONE_ZONESTATE_NOT_ENROLLED
 IAS Zone ZoneState attribute default value. More...
 
#define ZB_ZCL_IAS_ZONE_CLUSTER_REVISION_DEFAULT   ((zb_uint16_t)0x0002u)
 Default value for IAS Zone cluster revision global attribute. More...
 
#define ZB_ZCL_IAS_ZONE_ZONE_STATUS_DEF_VALUE   0
 IAS Zone ZoneStatus attribute default value. More...
 
#define ZB_ZCL_IAS_ZONE_NUMBER_OF_ZONE_SENSITIVITY_LEVELS_SUPPORTED_MIN_VALUE   ((zb_uint8_t)0x02)
 Min value for NumberOfZoneSensitivityLevelsSupported attribute. More...
 
#define ZB_ZCL_IAS_ZONE_NUMBER_OF_ZONE_SENSITIVITY_LEVELS_SUPPORTED_DEFAULT_VALUE   ZB_ZCL_IAS_ZONE_NUMBER_OF_ZONE_SENSITIVITY_LEVELS_SUPPORTED_MIN_VALUE
 Default value for NumberOfZoneSensitivityLevelsSupported attribute. More...
 
#define ZB_ZCL_IAS_ZONE_CURRENT_ZONE_SENSITIVITY_LEVEL_DEFAULT_VALUE   ((zb_uint8_t)0x00)
 Default value for CurrentZoneSensitivityLevel attribute. More...
 
#define ZB_ZCL_IAS_ZONEID_ID_DEF_VALUE   0xff
 IAS Zone ZoneID attribute default value. More...
 
#define ZB_ZCL_DECLARE_IAS_ZONE_ATTRIB_LIST( attr_list, zone_state, zone_type, zone_status, ias_cie_address, cie_short_addr, cie_ep)
 Declare attribute list for IAS Zone cluster - server side. More...
 
#define ZB_ZCL_DECLARE_IAS_ZONE_ATTRIB_LIST_EXT( attr_list, zone_state, zone_type, zone_status, number_of_zone_sens_levels_supported, current_zone_sens_level, ias_cie_address, zone_id, cie_short_addr, cie_ep)
 Declare attribute list for IAS Zone cluster - server side (extended attribute set) More...
 

IAS Zone cluster commands

enum  zb_zcl_ias_zone_cmd_e { ZB_ZCL_CMD_IAS_ZONE_ZONE_ENROLL_RESPONSE_ID = 0x00, ZB_ZCL_CMD_IAS_ZONE_INITIATE_NORMAL_OPERATION_MODE_ID = 0x01, ZB_ZCL_CMD_IAS_ZONE_INITIATE_TEST_MODE_ID = 0x02 }
 IAS Zone cluster command identifiers. More...
 
enum  zb_zcl_ias_zone_resp_cmd_e { ZB_ZCL_CMD_IAS_ZONE_ZONE_STATUS_CHANGE_NOT_ID = 0x00, ZB_ZCL_CMD_IAS_ZONE_ZONE_ENROLL_REQUEST_ID = 0x01 }
 IAS Zone cluster response command identifiers. More...
 
enum  zb_zcl_ias_zone_enroll_responce_code_e { ZB_ZCL_IAS_ZONE_ENROLL_RESPONCE_CODE_SUCCESS = 0x00, ZB_ZCL_IAS_ZONE_ENROLL_RESPONCE_CODE_NOT_SUPPORTED = 0x01, ZB_ZCL_IAS_ZONE_ENROLL_RESPONCE_CODE_NO_ENROLL = 0x02, ZB_ZCL_IAS_ZONE_ENROLL_RESPONCE_CODE_TOO_MANY_ZONES = 0x03 }
 Values of the Enroll Response Code see ZCL spec 8.2.2.3.1.1. More...
 
typedef struct zb_zcl_ias_zone_init_test_mode_ha_s zb_zcl_ias_zone_init_test_mode_t
 Structure representsation of Initiate Test Mode - Errata to 05-3520-29 Spec, 1.1.23.2.2.1. More...
 
typedef struct zb_zcl_ias_zone_status_change_not_s zb_zcl_ias_zone_status_change_not_t
 Structure representsation of Zone Status Change Notification see ZCL spec 8.2.2.4.1.1. More...
 
typedef struct zb_zcl_ias_zone_enroll_request_s zb_zcl_ias_zone_enroll_request_t
 Structure representsation of "Zone Enroll Request" command see ZCL spec 8.2.2.4.1.2. More...
 
typedef struct zb_zcl_ias_zone_enroll_res_s zb_zcl_ias_zone_enroll_res_t
 Structure representsation of Enroll response command payload see ZCL spec 8.2.2.3.1.1. More...
 
#define ZB_ZCL_IAS_ZONE_GET_INITIATE_TEST_MODE_REQ(data_ptr, buffer, status)
 Macro for getting "Initiate Test Mode" command. More...
 
#define ZB_ZCL_IAS_ZONE_SEND_INITIATE_TEST_MODE_REQ( buffer, addr, dst_addr_mode, dst_ep, ep, prfl_id, cb, test_mode_duration, current_zone_sens_level)
 Initiate Test Mode command. More...
 
#define ZB_ZCL_IAS_ZONE_SEND_INITIATE_NORMAL_OPERATION_MODE_REQ( buffer, addr, dst_addr_mode, dst_ep, ep, prfl_id, cb)
 Initiate Normal Operation Mode command. More...
 
#define ZB_ZCL_IAS_ZONE_SEND_STATUS_CHANGE_NOTIFICATION_REQ( buffer, addr, dst_addr_mode, dst_ep, ep, prfl_id, cb, zone_status, extended_status, zone_id, delay)
 Zone Status Change Notification command. More...
 
#define ZB_ZCL_IAS_ZONE_GET_STATUS_CHANGE_NOTIFICATION_REQ(data_ptr, buffer, status)
 Macro for getting Zone Status Change Notification command. More...
 
#define ZB_ZCL_IAS_ZONE_SEND_ZONE_ENROLL_REQUEST_REQ( buffer, addr, dst_addr_mode, dst_ep, ep, prfl_id, cb, zone_type, manufacturer_code)
 Zone "Zone Enroll Request" command, see ZCL spec 8.2.2.4.2. More...
 
#define ZB_ZCL_IAS_ZONE_GET_ZONE_ENROLL_REQUEST_REQ(data_ptr, buffer, status)
 Macro for getting Zone Status Change Notification command, see ZCL spec 8.2.2.4.1. More...
 
#define ZB_ZCL_IAS_ZONE_SEND_ZONE_ENROLL_RES( buffer, addr, dst_addr_mode, dst_ep, ep, prfl_id, def_resp, cb, code, zone_id)
 Send "Zone Enroll response" command, see ZCL spec 8.2.2.3.1. More...
 
#define ZB_ZCL_IAS_ZONE_SEND_ZONE_ENROLL_RES_EXT( buffer, addr, dst_addr_mode, dst_ep, ep, prfl_id, def_resp, cb, code, zone_id, seq)
 Send "Zone Enroll response with add parameters - sequency" command, see ZCL spec 8.2.2.3.1. More...
 
#define ZB_ZCL_IAS_ZONE_GET_ZONE_ENROLL_RES(data_ptr, buffer, status)
 Macro for getting "Zone Enroll response" command. More...
 

Detailed Description

IAS Zone cluster definitions

Macro Definition Documentation

§ ZB_ZCL_DECLARE_IAS_ZONE_ATTRIB_LIST

#define ZB_ZCL_DECLARE_IAS_ZONE_ATTRIB_LIST (   attr_list,
  zone_state,
  zone_type,
  zone_status,
  ias_cie_address,
  cie_short_addr,
  cie_ep 
)

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_ias_zone.h>

Value:
zb_uint8_t cie_addr_is_set_##attr_list; \
ZB_ZCL_START_DECLARE_ATTRIB_LIST(attr_list) \
ZB_ZCL_SET_ATTR_DESC(ZB_ZCL_ATTR_IAS_ZONE_ZONESTATE_ID, (zone_state)) \
ZB_ZCL_SET_ATTR_DESC(ZB_ZCL_ATTR_IAS_ZONE_ZONETYPE_ID, (zone_type)) \
ZB_ZCL_SET_ATTR_DESC(ZB_ZCL_ATTR_IAS_ZONE_ZONESTATUS_ID, (zone_status)) \
ZB_ZCL_SET_ATTR_DESC(ZB_ZCL_ATTR_IAS_ZONE_IAS_CIE_ADDRESS_ID, (ias_cie_address)) \
ZB_ZCL_SET_ATTR_DESC(ZB_ZCL_ATTR_CUSTOM_CIE_SHORT_ADDR, (cie_short_addr)) \
ZB_ZCL_SET_ATTR_DESC(ZB_ZCL_ATTR_CUSTOM_CIE_EP, (cie_ep)) \
ZB_ZCL_SET_ATTR_DESC(ZB_ZCL_ATTR_CUSTOM_CIE_ADDR_IS_SET, &(cie_addr_is_set_##attr_list)) \
ZB_ZCL_FINISH_DECLARE_ATTRIB_LIST
ZoneStatus attribute, ZCL spec 8.2.2.2.1.3.
Definition: zb_zcl_ias_zone.h:62
ZoneState attribute, ZCL spec 8.2.2.2.1.1.
Definition: zb_zcl_ias_zone.h:58
Definition: zb_zcl_ias_zone.h:75
unsigned char zb_uint8_t
Project-local 1-byte unsigned int type.
Definition: zb_types.h:147
ZoneType attribute, ZCL spec 8.2.2.2.1.2.
Definition: zb_zcl_ias_zone.h:60
Definition: zb_zcl_ias_zone.h:76
IAS_CIE_Address attribute, ZCL spec 8.2.2.2.2.1.
Definition: zb_zcl_ias_zone.h:64
Definition: zb_zcl_ias_zone.h:77

Declare attribute list for IAS Zone cluster - server side.

Parameters
attr_list- attribute list name
zone_state- pointer to variable to store ZoneState attribute
zone_type- pointer to variable to store ZoneType attribute
zone_status- pointer to variable to store ZoneStatus attribute
ias_cie_address- pointer to variable to store IAS-CIE address attribute
cie_short_addr- custom attribute to store CIE short address
cie_ep- custom attribute to store CIE Endpoint number

§ ZB_ZCL_DECLARE_IAS_ZONE_ATTRIB_LIST_EXT

#define ZB_ZCL_DECLARE_IAS_ZONE_ATTRIB_LIST_EXT (   attr_list,
  zone_state,
  zone_type,
  zone_status,
  number_of_zone_sens_levels_supported,
  current_zone_sens_level,
  ias_cie_address,
  zone_id,
  cie_short_addr,
  cie_ep 
)

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_ias_zone.h>

Value:
zb_uint8_t cie_addr_is_set_##attr_list; \
zb_uint16_t last_change_##attr_list; \
zb_zcl_ias_zone_int_ctx_t int_ctx_##attr_list; \
ZB_ZCL_START_DECLARE_ATTRIB_LIST_CLUSTER_REVISION(attr_list, ZB_ZCL_IAS_ZONE) \
ZB_ZCL_SET_ATTR_DESC(ZB_ZCL_ATTR_IAS_ZONE_ZONESTATE_ID, (zone_state)) \
ZB_ZCL_SET_ATTR_DESC(ZB_ZCL_ATTR_IAS_ZONE_ZONETYPE_ID, (zone_type)) \
ZB_ZCL_SET_ATTR_DESC(ZB_ZCL_ATTR_IAS_ZONE_ZONESTATUS_ID, (zone_status)) \
ZB_ZCL_SET_ATTR_DESC(ZB_ZCL_ATTR_IAS_ZONE_IAS_CIE_ADDRESS_ID, (ias_cie_address)) \
ZB_ZCL_SET_ATTR_DESC(ZB_ZCL_ATTR_IAS_ZONE_ZONEID_ID, (zone_id)) \
(number_of_zone_sens_levels_supported)) \
(current_zone_sens_level)) \
ZB_ZCL_SET_ATTR_DESC(ZB_ZCL_ATTR_IAS_ZONE_INT_CTX_ID, &(int_ctx_##attr_list)) \
ZB_ZCL_SET_ATTR_DESC(ZB_ZCL_ATTR_CUSTOM_CIE_SHORT_ADDR, (cie_short_addr)) \
ZB_ZCL_SET_ATTR_DESC(ZB_ZCL_ATTR_CUSTOM_CIE_EP, (cie_ep)) \
ZB_ZCL_SET_ATTR_DESC(ZB_ZCL_ATTR_CUSTOM_CIE_ADDR_IS_SET, &(cie_addr_is_set_##attr_list)) \
ZB_ZCL_FINISH_DECLARE_ATTRIB_LIST
ZoneStatus attribute, ZCL spec 8.2.2.2.1.3.
Definition: zb_zcl_ias_zone.h:62
ZoneState attribute, ZCL spec 8.2.2.2.1.1.
Definition: zb_zcl_ias_zone.h:58
Definition: zb_zcl_ias_zone.h:75
NumberOfZoneSensitivityLevelsSupported attribute, ZCL spec 8.2.2.1.2.3.
Definition: zb_zcl_ias_zone.h:68
CurrentZoneSensitivityLevel attribute, ZCL spec 8.2.2.1.2.4.
Definition: zb_zcl_ias_zone.h:70
unsigned char zb_uint8_t
Project-local 1-byte unsigned int type.
Definition: zb_types.h:147
Struct with pointers on User App callbacks.
Definition: zb_zcl_ias_zone.h:80
ZoneType attribute, ZCL spec 8.2.2.2.1.2.
Definition: zb_zcl_ias_zone.h:60
Definition: zb_zcl_ias_zone.h:76
ZoneID attribute, ZCL spec 8.2.2.1.2.2.
Definition: zb_zcl_ias_zone.h:66
IAS_CIE_Address attribute, ZCL spec 8.2.2.2.2.1.
Definition: zb_zcl_ias_zone.h:64
Definition: zb_zcl_ias_zone.h:77

Declare attribute list for IAS Zone cluster - server side (extended attribute set)

Parameters
attr_list- attribute list name
zone_state- pointer to variable to store ZoneState attribute
zone_type- pointer to variable to store ZoneType attribute
zone_status- pointer to variable to store ZoneStatus attribute
ias_cie_address- pointer to variable to store IAS-CIE address attribute
zone_id- pointer to variable to store Zone ID attribute
number_of_zone_sens_levels_supported- pointer to variable to store NumberOfZoneSensitivityLevelsSupported attribute
current_zone_sens_level- pointer to variable to store CurrentZoneSensitivityLevel attribute
cie_short_addr- custom attribute to store CIE short address
cie_ep- custom attribute to store CIE Endpoint number

§ ZB_ZCL_IAS_ZONE_CLEAR_BITS

#define ZB_ZCL_IAS_ZONE_CLEAR_BITS (   buffer,
  ep,
  set_bits 
)

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_ias_zone.h>

Value:
{ \
zb_zcl_ias_zone_status_param_t* cmd_data = \
ZB_BUF_GET_PARAM((buffer), zb_zcl_ias_zone_status_param_t); \
cmd_data->endpoint = (ep); \
cmd_data->bits = (set_bits); \
cmd_data->is_set = ZB_FALSE; \
ZB_SCHEDULE_CALLBACK(zb_zcl_ias_zone_change_status, ((buffer))); \
}
#define ZB_FALSE
Definition: zb_types.h:349
Declare Set/Clear Zone Status bits.
Definition: zb_zcl_ias_zone.h:747
void zb_zcl_ias_zone_change_status(zb_uint8_t param)

Clear Zone Status bits custom server command.

Parameters
buffer- to put packet to
ep- sending endpoint
set_bits- flag set of Zone Status, see zb_zcl_ias_zone_zonestatus_e

§ ZB_ZCL_IAS_ZONE_CLUSTER_REVISION_DEFAULT

#define ZB_ZCL_IAS_ZONE_CLUSTER_REVISION_DEFAULT   ((zb_uint16_t)0x0002u)

§ ZB_ZCL_IAS_ZONE_CURRENT_ZONE_SENSITIVITY_LEVEL_DEFAULT_VALUE

#define ZB_ZCL_IAS_ZONE_CURRENT_ZONE_SENSITIVITY_LEVEL_DEFAULT_VALUE   ((zb_uint8_t)0x00)

§ ZB_ZCL_IAS_ZONE_ENROLL_RESPONSE_SCHEDULE_USER_APP

#define ZB_ZCL_IAS_ZONE_ENROLL_RESPONSE_SCHEDULE_USER_APP (   buffer,
  pcmd_info,
  enroll_response_,
  zone_id_ 
)

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_ias_zone.h>

Value:
{ \
zb_zcl_ias_zone_enroll_response_user_app_schedule_t* user_data = \
ZB_MEMMOVE(&(user_data->cmd_info), (pcmd_info), sizeof(zb_zcl_parsed_hdr_t)); \
user_data->param.enroll_response = (enroll_response_); \
user_data->param.zone_id = (zone_id_); \
ZB_SCHEDULE_CALLBACK(zb_zcl_ias_zone_enroll_response_invoke_user_app, ((buffer))); \
}
Definition: zb_zcl_common.h:1158

§ ZB_ZCL_IAS_ZONE_GET_INITIATE_TEST_MODE_REQ

#define ZB_ZCL_IAS_ZONE_GET_INITIATE_TEST_MODE_REQ (   data_ptr,
  buffer,
  status 
)

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_ias_zone.h>

Value:
{ \
if (zb_buf_len((buffer)) < sizeof(zb_zcl_ias_zone_init_test_mode_t)) \
{ \
} \
else \
{ \
zb_zcl_ias_zone_init_test_mode_t *src_ptr = \
(data_ptr)->test_mode_duration = src_ptr->test_mode_duration; \
(data_ptr)->current_zone_sens_level = src_ptr->current_zone_sens_level; \
} \
}
Definition: zb_zcl_common.h:339
Definition: zb_zcl_common.h:338
#define zb_buf_begin(buf)
Definition: zboss_api_buf.h:354
Structure representsation of Initiate Test Mode - Errata to 05-3520-29 Spec, 1.1.23.2.2.1.
Definition: zb_zcl_ias_zone.h:415
#define zb_buf_len(buf)
Definition: zboss_api_buf.h:372

Macro for getting "Initiate Test Mode" command.

Attention
Assumes that ZCL header already cut.
Parameters
data_ptr- pointer to a variable of type zb_zcl_ias_zone_init_test_mode_t.
buffercontaining the packet (by pointer).
status- variable to put parse status to (see zb_zcl_parse_status_t).

§ ZB_ZCL_IAS_ZONE_GET_STATUS_CHANGE_NOTIFICATION_REQ

#define ZB_ZCL_IAS_ZONE_GET_STATUS_CHANGE_NOTIFICATION_REQ (   data_ptr,
  buffer,
  status 
)

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_ias_zone.h>

Value:
{ \
{ \
} \
else \
{ \
zb_zcl_ias_zone_status_change_not_t *src_ptr = \
ZB_HTOLE16(&((data_ptr)->zone_status), &(src_ptr->zone_status)); \
(data_ptr)->extended_status = src_ptr->extended_status; \
(data_ptr)->zone_id = src_ptr->zone_id; \
ZB_HTOLE16(&((data_ptr)->delay), &(src_ptr->delay)); \
} \
}
Definition: zb_zcl_common.h:339
Definition: zb_zcl_common.h:338
#define zb_buf_begin(buf)
Definition: zboss_api_buf.h:354
#define zb_buf_len(buf)
Definition: zboss_api_buf.h:372
Structure representsation of Zone Status Change Notification see ZCL spec 8.2.2.4.1.1.
Definition: zb_zcl_ias_zone.h:499

Macro for getting Zone Status Change Notification command.

Attention
Assumes that ZCL header already cut.
Parameters
data_ptr- pointer to a variable of type zb_zcl_ias_zone_status_change_not_s.
buffercontaining the packet (by pointer).
status- variable to put parse status to (see zb_zcl_parse_status_t).

§ ZB_ZCL_IAS_ZONE_GET_ZONE_ENROLL_REQUEST_REQ

#define ZB_ZCL_IAS_ZONE_GET_ZONE_ENROLL_REQUEST_REQ (   data_ptr,
  buffer,
  status 
)

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_ias_zone.h>

Value:
{ \
if (zb_buf_len((buffer)) < sizeof(zb_zcl_ias_zone_enroll_request_t)) \
{ \
} \
else \
{ \
zb_zcl_ias_zone_enroll_request_t *src_ptr = \
ZB_HTOLE16(&((data_ptr)->zone_type), &(src_ptr->zone_type)); \
ZB_HTOLE16(&((data_ptr)->manufacturer_code), &(src_ptr->manufacturer_code)); \
} \
}
Structure representsation of "Zone Enroll Request" command see ZCL spec 8.2.2.4.1.2.
Definition: zb_zcl_ias_zone.h:572
Definition: zb_zcl_common.h:339
Definition: zb_zcl_common.h:338
#define zb_buf_begin(buf)
Definition: zboss_api_buf.h:354
#define zb_buf_len(buf)
Definition: zboss_api_buf.h:372

Macro for getting Zone Status Change Notification command, see ZCL spec 8.2.2.4.1.

Attention
Assumes that ZCL header already cut.
Parameters
data_ptr- pointer to a variable of type zb_zcl_ias_zone_enroll_request_s.
buffercontaining the packet (by pointer).
status- variable to put parse status to (see zb_zcl_parse_status_t).

§ ZB_ZCL_IAS_ZONE_GET_ZONE_ENROLL_RES

#define ZB_ZCL_IAS_ZONE_GET_ZONE_ENROLL_RES (   data_ptr,
  buffer,
  status 
)

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_ias_zone.h>

Value:
{ \
if (zb_buf_len((buffer)) < sizeof(zb_zcl_ias_zone_enroll_res_t)) \
{ \
} \
else \
{ \
zb_zcl_ias_zone_enroll_res_t *src_ptr = \
(data_ptr)->code = src_ptr->code; \
(data_ptr)->zone_id = src_ptr->zone_id; \
} \
}
Structure representsation of Enroll response command payload see ZCL spec 8.2.2.3.1.1.
Definition: zb_zcl_ias_zone.h:649
Definition: zb_zcl_common.h:339
Definition: zb_zcl_common.h:338
#define zb_buf_begin(buf)
Definition: zboss_api_buf.h:354
#define zb_buf_len(buf)
Definition: zboss_api_buf.h:372

Macro for getting "Zone Enroll response" command.

Attention
Assumes that ZCL header already cut.
Parameters
data_ptr- pointer to a variable of type zb_zcl_ias_zone_enroll_res_s.
buffercontaining the packet (by pointer).
status- variable to put parse status to (see zb_zcl_parse_status_t).

§ ZB_ZCL_IAS_ZONE_NUMBER_OF_ZONE_SENSITIVITY_LEVELS_SUPPORTED_DEFAULT_VALUE

#define ZB_ZCL_IAS_ZONE_NUMBER_OF_ZONE_SENSITIVITY_LEVELS_SUPPORTED_DEFAULT_VALUE   ZB_ZCL_IAS_ZONE_NUMBER_OF_ZONE_SENSITIVITY_LEVELS_SUPPORTED_MIN_VALUE

§ ZB_ZCL_IAS_ZONE_NUMBER_OF_ZONE_SENSITIVITY_LEVELS_SUPPORTED_MIN_VALUE

#define ZB_ZCL_IAS_ZONE_NUMBER_OF_ZONE_SENSITIVITY_LEVELS_SUPPORTED_MIN_VALUE   ((zb_uint8_t)0x02)

§ ZB_ZCL_IAS_ZONE_SEND_INITIATE_NORMAL_OPERATION_MODE_REQ

#define ZB_ZCL_IAS_ZONE_SEND_INITIATE_NORMAL_OPERATION_MODE_REQ (   buffer,
  addr,
  dst_addr_mode,
  dst_ep,
  ep,
  prfl_id,
  cb 
)

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_ias_zone.h>

Value:
{ \
zb_uint8_t* ptr = ZB_ZCL_START_PACKET_REQ(buffer) \
ZB_ZCL_CONSTRUCT_SPECIFIC_COMMAND_REQ_FRAME_CONTROL(ptr, ZB_ZCL_ENABLE_DEFAULT_RESPONSE) \
ZB_ZCL_CONSTRUCT_COMMAND_HEADER_REQ(ptr, ZB_ZCL_GET_SEQ_NUM(), \
ZB_ZCL_FINISH_PACKET((buffer), ptr) \
ZB_ZCL_SEND_COMMAND_SHORT( \
buffer, addr, dst_addr_mode, dst_ep, ep, prfl_id, \
}
#define ZB_ZCL_GET_SEQ_NUM()
Return next sequence number for ZCL frame.
Definition: zb_zcl_common.h:1470
#define ZB_ZCL_ENABLE_DEFAULT_RESPONSE
Definition: zb_zcl_common.h:1043
#define ZB_ZCL_CLUSTER_ID_IAS_ZONE
Definition: zb_zcl_common.h:265

Initiate Normal Operation Mode command.

Parameters
buffer- to put packet to
addr- address to send packet to
dst_addr_mode- addressing mode
dst_ep- destination endpoint
ep- sending endpoint
prfl_id- profile identifier
cb- callback for getting command send status

§ ZB_ZCL_IAS_ZONE_SEND_INITIATE_TEST_MODE_REQ

#define ZB_ZCL_IAS_ZONE_SEND_INITIATE_TEST_MODE_REQ (   buffer,
  addr,
  dst_addr_mode,
  dst_ep,
  ep,
  prfl_id,
  cb,
  test_mode_duration,
  current_zone_sens_level 
)

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_ias_zone.h>

Value:
{ \
zb_uint8_t* ptr = ZB_ZCL_START_PACKET_REQ(buffer) \
ZB_ZCL_CONSTRUCT_SPECIFIC_COMMAND_REQ_FRAME_CONTROL(ptr, ZB_ZCL_ENABLE_DEFAULT_RESPONSE) \
ZB_ZCL_CONSTRUCT_COMMAND_HEADER_REQ(ptr, ZB_ZCL_GET_SEQ_NUM(), \
ZB_ZCL_PACKET_PUT_DATA8(ptr, (test_mode_duration)); \
ZB_ZCL_PACKET_PUT_DATA8(ptr, (current_zone_sens_level)); \
ZB_ZCL_FINISH_PACKET((buffer), ptr) \
ZB_ZCL_SEND_COMMAND_SHORT( \
buffer, addr, dst_addr_mode, dst_ep, ep, prfl_id, \
}
#define ZB_ZCL_GET_SEQ_NUM()
Return next sequence number for ZCL frame.
Definition: zb_zcl_common.h:1470
Definition: zb_zcl_ias_zone.h:382
#define ZB_ZCL_ENABLE_DEFAULT_RESPONSE
Definition: zb_zcl_common.h:1043
#define ZB_ZCL_CLUSTER_ID_IAS_ZONE
Definition: zb_zcl_common.h:265

Initiate Test Mode command.

Parameters
buffer- to put packet to
addr- address to send packet to
dst_addr_mode- addressing mode
dst_ep- destination endpoint
ep- sending endpoint
prfl_id- profile identifier
cb- callback for getting command send status
test_mode_duration- Test Mode duration
current_zone_sens_level- CurrentZoneSensitivityLevel

§ ZB_ZCL_IAS_ZONE_SEND_STATUS_CHANGE_NOTIFICATION_REQ

#define ZB_ZCL_IAS_ZONE_SEND_STATUS_CHANGE_NOTIFICATION_REQ (   buffer,
  addr,
  dst_addr_mode,
  dst_ep,
  ep,
  prfl_id,
  cb,
  zone_status,
  extended_status,
  zone_id,
  delay 
)

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_ias_zone.h>

Value:
{ \
zb_uint8_t* ptr = ZB_ZCL_START_PACKET(buffer); \
ZB_ZCL_CONSTRUCT_SPECIFIC_COMMAND_RES_FRAME_CONTROL(ptr); \
ZB_ZCL_CONSTRUCT_COMMAND_HEADER(ptr, ZB_ZCL_GET_SEQ_NUM(), \
ZB_ZCL_PACKET_PUT_DATA16_VAL(ptr, (zone_status)); \
ZB_ZCL_PACKET_PUT_DATA8(ptr, (extended_status)); \
ZB_ZCL_PACKET_PUT_DATA8(ptr, (zone_id)); \
ZB_ZCL_PACKET_PUT_DATA16_VAL(ptr, (delay)); \
ZB_ZCL_FINISH_PACKET((buffer), ptr) \
ZB_ZCL_SEND_COMMAND_SHORT( \
buffer, addr, dst_addr_mode, dst_ep, ep, prfl_id, \
}
#define ZB_ZCL_GET_SEQ_NUM()
Return next sequence number for ZCL frame.
Definition: zb_zcl_common.h:1470
#define ZB_ZCL_START_PACKET(zbbuf)
Initializes zb_buf_t buffer and returns pointer to the beginning of array.
Definition: zb_zcl_common.h:1550
Definition: zb_zcl_ias_zone.h:391
#define ZB_ZCL_CLUSTER_ID_IAS_ZONE
Definition: zb_zcl_common.h:265

Zone Status Change Notification command.

Parameters
buffer- to put packet to
addr- address to send packet to
dst_addr_mode- addressing mode
dst_ep- destination endpoint
ep- sending endpoint
prfl_id- profile identifier
cb- callback for getting command send status
zone_status- Zone Status, see zb_zcl_ias_zone_zonestatus_e
extended_status- Extended Status
zone_id- Zone ID
delay- Delay

§ ZB_ZCL_IAS_ZONE_SEND_ZONE_ENROLL_REQUEST_REQ

#define ZB_ZCL_IAS_ZONE_SEND_ZONE_ENROLL_REQUEST_REQ (   buffer,
  addr,
  dst_addr_mode,
  dst_ep,
  ep,
  prfl_id,
  cb,
  zone_type,
  manufacturer_code 
)

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_ias_zone.h>

Value:
{ \
zb_uint8_t* ptr = ZB_ZCL_START_PACKET(buffer); \
ZB_ZCL_CONSTRUCT_SPECIFIC_COMMAND_RES_FRAME_CONTROL(ptr); \
ZB_ZCL_CONSTRUCT_COMMAND_HEADER(ptr, ZB_ZCL_GET_SEQ_NUM(), \
ZB_ZCL_PACKET_PUT_DATA16_VAL(ptr, (zone_type)); \
ZB_ZCL_PACKET_PUT_DATA16_VAL(ptr, (manufacturer_code)); \
ZB_ZCL_FINISH_PACKET((buffer), ptr) \
ZB_ZCL_SEND_COMMAND_SHORT( \
buffer, addr, dst_addr_mode, dst_ep, ep, prfl_id, \
}
Definition: zb_zcl_ias_zone.h:393
#define ZB_ZCL_GET_SEQ_NUM()
Return next sequence number for ZCL frame.
Definition: zb_zcl_common.h:1470
#define ZB_ZCL_START_PACKET(zbbuf)
Initializes zb_buf_t buffer and returns pointer to the beginning of array.
Definition: zb_zcl_common.h:1550
#define ZB_ZCL_CLUSTER_ID_IAS_ZONE
Definition: zb_zcl_common.h:265

Zone "Zone Enroll Request" command, see ZCL spec 8.2.2.4.2.

Parameters
buffer- to put packet to
addr- address to send packet to
dst_addr_mode- addressing mode
dst_ep- destination endpoint
ep- sending endpoint
prfl_id- profile identifier
cb- callback for getting command send status
zone_type- Zone Type, see zb_zcl_ias_zone_zonetype_e
manufacturer_code- Manufacture code

§ ZB_ZCL_IAS_ZONE_SEND_ZONE_ENROLL_RES

#define ZB_ZCL_IAS_ZONE_SEND_ZONE_ENROLL_RES (   buffer,
  addr,
  dst_addr_mode,
  dst_ep,
  ep,
  prfl_id,
  def_resp,
  cb,
  code,
  zone_id 
)

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_ias_zone.h>

Value:
{ \
zb_uint8_t* ptr = ZB_ZCL_START_PACKET_REQ(buffer) \
ZB_ZCL_CONSTRUCT_SPECIFIC_COMMAND_REQ_FRAME_CONTROL(ptr, (def_resp)) \
ZB_ZCL_CONSTRUCT_COMMAND_HEADER_REQ(ptr, ZB_ZCL_GET_SEQ_NUM(), \
ZB_ZCL_PACKET_PUT_DATA8(ptr, (code)); \
ZB_ZCL_PACKET_PUT_DATA8(ptr, (zone_id)); \
ZB_ZCL_FINISH_PACKET((buffer), ptr) \
ZB_ZCL_SEND_COMMAND_SHORT( \
buffer, addr, dst_addr_mode, dst_ep, ep, prfl_id, \
}
#define ZB_ZCL_GET_SEQ_NUM()
Return next sequence number for ZCL frame.
Definition: zb_zcl_common.h:1470
Definition: zb_zcl_ias_zone.h:377
#define ZB_ZCL_CLUSTER_ID_IAS_ZONE
Definition: zb_zcl_common.h:265

Send "Zone Enroll response" command, see ZCL spec 8.2.2.3.1.

Parameters
bufferto put packet to
addr- address to send packet to
dst_addr_mode- addressing mode
dst_ep- destination endpoint
ep- sending endpoint
prfl_id- profile identifier
def_resp- enable/disable default response
cb- callback
code- Enroll response code, see zb_zcl_ias_zone_enroll_responce_code_e
zone_id- Zone ID

§ ZB_ZCL_IAS_ZONE_SEND_ZONE_ENROLL_RES_EXT

#define ZB_ZCL_IAS_ZONE_SEND_ZONE_ENROLL_RES_EXT (   buffer,
  addr,
  dst_addr_mode,
  dst_ep,
  ep,
  prfl_id,
  def_resp,
  cb,
  code,
  zone_id,
  seq 
)

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_ias_zone.h>

Value:
{ \
zb_uint8_t* ptr = ZB_ZCL_START_PACKET_REQ(buffer) \
ZB_ZCL_CONSTRUCT_SPECIFIC_COMMAND_REQ_FRAME_CONTROL(ptr, (def_resp)) \
ZB_ZCL_CONSTRUCT_COMMAND_HEADER_REQ(ptr, (seq), \
ZB_ZCL_PACKET_PUT_DATA8(ptr, (code)); \
ZB_ZCL_PACKET_PUT_DATA8(ptr, (zone_id)); \
ZB_ZCL_FINISH_PACKET((buffer), ptr) \
ZB_ZCL_SEND_COMMAND_SHORT( \
buffer, addr, dst_addr_mode, dst_ep, ep, prfl_id, \
}
Definition: zb_zcl_ias_zone.h:377
#define ZB_ZCL_CLUSTER_ID_IAS_ZONE
Definition: zb_zcl_common.h:265

Send "Zone Enroll response with add parameters - sequency" command, see ZCL spec 8.2.2.3.1.

Parameters
bufferto put packet to
addr- address to send packet to
dst_addr_mode- addressing mode
dst_ep- destination endpoint
ep- sending endpoint
prfl_id- profile identifier
def_resp- enable/disable default response
cb- callback
code- Enroll response code, see zb_zcl_ias_zone_enroll_responce_code_e
zone_id- Zone ID
seq- known sequency

§ ZB_ZCL_IAS_ZONE_SET_BITS

#define ZB_ZCL_IAS_ZONE_SET_BITS (   buffer,
  ep,
  set_bits 
)

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_ias_zone.h>

Value:
{ \
zb_zcl_ias_zone_status_param_t* cmd_data = \
ZB_BUF_GET_PARAM((buffer), zb_zcl_ias_zone_status_param_t); \
cmd_data->endpoint = (ep); \
cmd_data->bits = (set_bits); \
cmd_data->is_set = ZB_TRUE; \
ZB_SCHEDULE_CALLBACK(zb_zcl_ias_zone_change_status, ((buffer))); \
}
Declare Set/Clear Zone Status bits.
Definition: zb_zcl_ias_zone.h:747
void zb_zcl_ias_zone_change_status(zb_uint8_t param)
#define ZB_TRUE
Definition: zb_types.h:350

Set Zone Status bits custom server command.

Parameters
buffer- to put packet to
ep- endpoint
set_bits- flag set of Zone Status, see zb_zcl_ias_zone_zonestatus_e

§ ZB_ZCL_IAS_ZONE_ZONE_STATUS_DEF_VALUE

#define ZB_ZCL_IAS_ZONE_ZONE_STATUS_DEF_VALUE   0

§ ZB_ZCL_IAS_ZONE_ZONESTATE_DEF_VALUE

§ ZB_ZCL_IAS_ZONEID_ID_DEF_VALUE

#define ZB_ZCL_IAS_ZONEID_ID_DEF_VALUE   0xff

Typedef Documentation

§ zb_ias_zone_app_callback_t

§ zb_zcl_ias_zone_enroll_request_t

§ zb_zcl_ias_zone_enroll_res_t

§ zb_zcl_ias_zone_enroll_response_user_app_schedule_t

§ zb_zcl_ias_zone_enroll_response_value_param_t

§ zb_zcl_ias_zone_init_test_mode_t

§ zb_zcl_ias_zone_int_ctx_t

§ zb_zcl_ias_zone_notification_param_t

§ zb_zcl_ias_zone_status_change_not_t

§ zb_zcl_ias_zone_status_param_t

Enumeration Type Documentation

§ zb_zcl_general_cb_params_e

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_ias_zone.h>

Enumerator
ZB_ZCL_VALID_CIE_ADDR_SET 
ZB_ZCL_CURR_ZONE_SENSITIVITY_LEVEL_SET 
ZB_ZCL_INIT_TEST_MODE 
ZB_ZCL_INIT_NORMAL_MODE 

§ zb_zcl_ias_zone_attr_e

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_ias_zone.h>

IAS Zone cluster attribute identifiers.

See also
ZCL spec, IAS Zone Cluster 8.2.2.2
Enumerator
ZB_ZCL_ATTR_IAS_ZONE_ZONESTATE_ID 

ZoneState attribute, ZCL spec 8.2.2.2.1.1.

ZB_ZCL_ATTR_IAS_ZONE_ZONETYPE_ID 

ZoneType attribute, ZCL spec 8.2.2.2.1.2.

ZB_ZCL_ATTR_IAS_ZONE_ZONESTATUS_ID 

ZoneStatus attribute, ZCL spec 8.2.2.2.1.3.

ZB_ZCL_ATTR_IAS_ZONE_IAS_CIE_ADDRESS_ID 

IAS_CIE_Address attribute, ZCL spec 8.2.2.2.2.1.

ZB_ZCL_ATTR_IAS_ZONE_ZONEID_ID 

ZoneID attribute, ZCL spec 8.2.2.1.2.2.

ZB_ZCL_ATTR_IAS_ZONE_NUMBER_OF_ZONE_SENSITIVITY_LEVELS_SUPPORTED_ID 

NumberOfZoneSensitivityLevelsSupported attribute, ZCL spec 8.2.2.1.2.3.

ZB_ZCL_ATTR_IAS_ZONE_CURRENT_ZONE_SENSITIVITY_LEVEL_ID 

CurrentZoneSensitivityLevel attribute, ZCL spec 8.2.2.1.2.4.

ZB_ZCL_ATTR_CUSTOM_ZGP_CALIBRATION 
ZB_ZCL_ATTR_CUSTOM_ZGP_CLOUD_ACK 
ZB_ZCL_ATTR_CUSTOM_CIE_ADDR_IS_SET 
ZB_ZCL_ATTR_CUSTOM_CIE_EP 
ZB_ZCL_ATTR_CUSTOM_CIE_SHORT_ADDR 
ZB_ZCL_ATTR_IAS_ZONE_INT_CTX_ID 

Struct with pointers on User App callbacks.

§ zb_zcl_ias_zone_cmd_e

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_ias_zone.h>

IAS Zone cluster command identifiers.

See also
ZCL spec, IAS Zone Cluster, 8.2.2.3
Enumerator
ZB_ZCL_CMD_IAS_ZONE_ZONE_ENROLL_RESPONSE_ID 

"Zone Enroll Response" command, ZCL spec 8.2.2.3.1 "Initiate Normal Operation Mode" command, ZCL spec 8.2.2.2.1

ZB_ZCL_CMD_IAS_ZONE_INITIATE_NORMAL_OPERATION_MODE_ID 

"Initiate Test Mode" command, ZCL spec 8.2.2.2.2.3

ZB_ZCL_CMD_IAS_ZONE_INITIATE_TEST_MODE_ID 

§ zb_zcl_ias_zone_enroll_responce_code_e

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_ias_zone.h>

Values of the Enroll Response Code see ZCL spec 8.2.2.3.1.1.

Enumerator
ZB_ZCL_IAS_ZONE_ENROLL_RESPONCE_CODE_SUCCESS 

Success

ZB_ZCL_IAS_ZONE_ENROLL_RESPONCE_CODE_NOT_SUPPORTED 

Not supported

ZB_ZCL_IAS_ZONE_ENROLL_RESPONCE_CODE_NO_ENROLL 

No enroll permit

ZB_ZCL_IAS_ZONE_ENROLL_RESPONCE_CODE_TOO_MANY_ZONES 

Too many zones

§ zb_zcl_ias_zone_resp_cmd_e

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_ias_zone.h>

IAS Zone cluster response command identifiers.

See also
ZCL spec, IAS Zone Cluster, 8.2.2.4
Enumerator
ZB_ZCL_CMD_IAS_ZONE_ZONE_STATUS_CHANGE_NOT_ID 

"Zone Status Change Notification" command. ZCL spec 8.2.2.4.1

ZB_ZCL_CMD_IAS_ZONE_ZONE_ENROLL_REQUEST_ID 

"Zone Enroll Request" command. ZCL spec 8.2.2.4.2

§ zb_zcl_ias_zone_zonestate_e

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_ias_zone.h>

IAS Zone ZoneState value.

Enumerator
ZB_ZCL_IAS_ZONE_ZONESTATE_NOT_ENROLLED 

ZoneState not enrolled value.

ZB_ZCL_IAS_ZONE_ZONESTATE_ENROLLED 

ZoneState enrolled value.

§ zb_zcl_ias_zone_zonestatus_e

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_ias_zone.h>

IAS Zone ZoneStatus attribute flags.

See also
ZCL spec 8.2.2.2.1.3
Enumerator
ZB_ZCL_IAS_ZONE_ZONE_STATUS_ALARM1 

Alarm 1

ZB_ZCL_IAS_ZONE_ZONE_STATUS_ALARM2 

Alarm 2

ZB_ZCL_IAS_ZONE_ZONE_STATUS_TAMPER 

Tamper

ZB_ZCL_IAS_ZONE_ZONE_STATUS_BATTERY 

Battery

ZB_ZCL_IAS_ZONE_ZONE_STATUS_SUPERVISION 

Supervision reports

ZB_ZCL_IAS_ZONE_ZONE_STATUS_RESTORE 

Restore reports

ZB_ZCL_IAS_ZONE_ZONE_STATUS_TROUBLE 

Trouble

ZB_ZCL_IAS_ZONE_ZONE_STATUS_AC_MAINS 

AC (mains)

ZB_ZCL_IAS_ZONE_ZONE_STATUS_TEST 

Test

ZB_ZCL_IAS_ZONE_ZONE_STATUS_BATTERY_DEFECT 

Battery Defect

§ zb_zcl_ias_zone_zonetype_e

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_ias_zone.h>

IAS Zone ZoneType value.

Enumerator
ZB_ZCL_IAS_ZONE_ZONETYPE_STANDARD_CIE 

ZoneType Standard CIE System Alarm value.

ZB_ZCL_IAS_ZONE_ZONETYPE_MOTION 

ZoneType Motion value.

ZB_ZCL_IAS_ZONE_ZONETYPE_CONTACT_SWITCH 

ZoneType Contact switch value.

ZB_ZCL_IAS_ZONE_ZONETYPE_FIRE_SENSOR 

ZoneType Fire sensor value.

ZB_ZCL_IAS_ZONE_ZONETYPE_WATER_SENSOR 

ZoneType Water sensor value.

ZB_ZCL_IAS_ZONE_ZONETYPE_GAS_SENSOR 

ZoneType Gas sensor value.

ZB_ZCL_IAS_ZONE_ZONETYPE_PERSONAL_EMERGENCY 

ZoneType Personal emergency value.

ZB_ZCL_IAS_ZONE_ZONETYPE_VIBRATION_MOVEMENT 

ZoneType Vibration / Movement sensor value.

ZB_ZCL_IAS_ZONE_ZONETYPE_REMOTE_CONTROL 

ZoneType Remote Control value.

ZB_ZCL_IAS_ZONE_ZONETYPE_KEY_FOB 

ZoneType Key fob value.

ZB_ZCL_IAS_ZONE_ZONETYPE_KEYPAD 

ZoneType Keypad value.

ZB_ZCL_IAS_ZONE_ZONETYPE_STANDARD_WARNING 

ZoneType Standard Warning Device value.

ZB_ZCL_IAS_ZONE_ZONETYPE_MANUF_SPEC 

Manufacturer specific ZoneType value.

ZB_ZCL_IAS_ZONE_ZONETYPE_INVALID 

ZoneType Invalid Zone Type value.

Function Documentation

§ zb_zcl_ias_set_attr_val_post_process()

void zb_zcl_ias_set_attr_val_post_process ( zb_zcl_parsed_hdr_t cmd_info,
zb_uint16_t  attr_id,
zb_uint8_t value 
)

§ zb_zcl_ias_zone_change_status()

§ zb_zcl_ias_zone_check_attr_notify()

zb_bool_t zb_zcl_ias_zone_check_attr_notify ( zb_uint8_t  buf_param)

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_ias_zone.h>

checks, if Zone Status change notification should be sent and schedules command if it is needed

Returns
ZB_TRUE if command is sent

§ zb_zcl_ias_zone_check_cie_addr_on_zcl_initialization()

void zb_zcl_ias_zone_check_cie_addr_on_zcl_initialization ( zb_uint8_t  ep_id)

§ zb_zcl_ias_zone_put_cie_address_to_binding_whitelist()

zb_ret_t zb_zcl_ias_zone_put_cie_address_to_binding_whitelist ( zb_uint8_t  endpoint)

§ zb_zcl_ias_zone_register_cb()

void zb_zcl_ias_zone_register_cb ( zb_uint8_t  endpoint,
zb_callback_t  process_result_cb,
zb_ias_zone_app_callback_t  general_cb 
)

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_ias_zone.h>

Registry callbacks to get status of Zone Status Change Notification command.

Parameters
endpoint- local endpoint number
process_result_cb- notification sent callback function
general_cb- general callback function

§ zb_zcl_ias_zone_send_status_change_not()

void zb_zcl_ias_zone_send_status_change_not ( zb_uint8_t  param)

§ zb_zcl_ias_zone_set_status()

zb_bool_t zb_zcl_ias_zone_set_status ( zb_uint8_t  ep,
zb_uint16_t  new_val,
zb_uint16_t  delay,
zb_uint8_t  buf_param 
)

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_ias_zone.h>

Use this function to change IAS Zone status. This function will set new value of ZoneStatus and will send Zone status change notification.

Note
If another API (ZB_ZCL_SET_ATTRIBUTE()) is used for modifying ZoneStatus, notification will NOT be send. This is limitation of the current implementation.
Parameters
ep- local endpoint number
new_val- new value for ZoneStatus
delay- delay in quarter seconds (actual only for HA ZCL version, is ignored for pure ZCL implementation)
buf_param- reference to a buffer that will be used for sending notification. If buffer reference is not specified, notification will NOT be sent
Returns
Returns ZB_TRUE if notification is scheduled for send, ZB_FALSE otherwise
Note
Notification send result is reported to user App using callback that is registered with zb_zcl_ias_zone_register_cb()