Data Structures | |
| struct | zb_zcl_door_lock_read_lock_door_res_payload_s |
| struct | zb_zcl_door_lock_read_unlock_door_res_payload_s |
Door Lock cluster defined in ZCL spec, clause 7.3.
The cluster contains 2 command sets:
Both requests have no payload and could be scheduled for sending with corresponding macros. Both responses have simple payload, and their sending and parsing with corresponding macros is almost trivial.
Send Door Lock command:
Send Door Unlock command:
| #define ZB_ZCL_ATTR_DOOR_LOCK_ACTUATOR_ENABLED_DEFAULT_VALUE ZB_ZCL_ATTR_DOOR_LOCK_ACTUATOR_ENABLED_ENABLED |
Default value for Actuator Enabled attribute.
| #define ZB_ZCL_ATTR_DOOR_LOCK_LOCK_STATE_DEFAULT_VALUE ZB_ZCL_ATTR_DOOR_LOCK_LOCK_STATE_UNDEFINED |
Default value for Lock State attribute.
| #define ZB_ZCL_ATTR_DOOR_LOCK_LOCK_TYPE_DEFAULT_VALUE ZB_ZCL_ATTR_DOOR_LOCK_LOCK_TYPE_UNDEFINED |
Default value for Lock Type attribute.
| #define ZB_ZCL_DECLARE_DOOR_LOCK_ATTRIB_LIST | ( | attr_list, | |
| lock_state, | |||
| lock_type, | |||
| actuator_enabled | |||
| ) |
Declare attribute list for Door Lock cluster.
| attr_list | - attribute list name |
| lock_state | |
| lock_type | |
| actuator_enabled |
| #define ZB_ZCL_DOOR_LOCK_ALARM_MASK_DEFAULT_VALUE ((zb_uint16_t)0x0000) |
Default value for AlarmMask attribute.
| #define ZB_ZCL_DOOR_LOCK_AUTO_RELOCK_TIME_DEFAULT_VALUE ((zb_uint32_t)0) |
Default value for AutoRelockTime attribute.
| #define ZB_ZCL_DOOR_LOCK_CLUSTER_REVISION_DEFAULT ((zb_uint16_t)0x0003u) |
Default value for Door Lock cluster revision global attribute.
| #define ZB_ZCL_DOOR_LOCK_DEFAULT_CONFIGURATION_REGISTER_DEFAULT_VALUE ((zb_uint16_t)0x0000) |
Default value for DefaultConfigurationRegister attribute.
| #define ZB_ZCL_DOOR_LOCK_ENABLE_INSIDE_STATUS_LED_DEFAULT_VALUE ((zb_bool_t)0) |
Default value for EnableInsideStatusLED attribute.
| #define ZB_ZCL_DOOR_LOCK_ENABLE_LOCAL_PROGRAMMING_DEFAULT_VALUE ((zb_bool_t)0x01) |
Default value for EnableLocalProgramming attribute.
| #define ZB_ZCL_DOOR_LOCK_ENABLE_LOGGING_DEFAULT_VALUE ((zb_bool_t)0) |
Default value for EnableLogging attribute.
| #define ZB_ZCL_DOOR_LOCK_ENABLE_ONE_TOUCH_LOCKING_DEFAULT_VALUE ((zb_bool_t)0) |
Default value for EnableOneTouchLocking attribute.
| #define ZB_ZCL_DOOR_LOCK_ENABLE_PRIVACY_MODE_BUTTON_DEFAULT_VALUE ((zb_bool_t)0) |
Default value for EnablePrivacyModeButton attribute.
| #define ZB_ZCL_DOOR_LOCK_KEYPAD_OPERATION_EVENT_MASK_DEFAULT_VALUE ((zb_uint16_t)0x0000) |
Default value for KeypadOperationEventMask attribute.
| #define ZB_ZCL_DOOR_LOCK_KEYPAD_PROGRAMMING_EVENT_MASK_DEFAULT_VALUE ((zb_uint16_t)0x0000) |
Default value for KeypadProgrammingEventMask attribute.
| #define ZB_ZCL_DOOR_LOCK_LANGUAGE_DEFAULT_VALUE {0} |
Default value for Language attribute.
| #define ZB_ZCL_DOOR_LOCK_LED_SETTINGS_DEFAULT_VALUE ((zb_uint8_t)0) |
Default value for LEDSettings attribute.
| #define ZB_ZCL_DOOR_LOCK_MANUAL_OPERATION_EVENT_MASK_DEFAULT_VALUE ((zb_uint16_t)0x0000) |
Default value for ManualOperationEventMask attribute.
| #define ZB_ZCL_DOOR_LOCK_MAX_PIN_LEN_DEFAULT_VALUE ((zb_uint8_t)0x08) |
Default value for MaxPINLen attribute.
| #define ZB_ZCL_DOOR_LOCK_MAX_RFID_CODE_LENGTH_DEFAULT_VALUE ((zb_uint8_t)0x14) |
Default value for MaxRFIDCodeLength attribute.
| #define ZB_ZCL_DOOR_LOCK_MIN_PIN_LEN_DEFAULT_VALUE ((zb_uint8_t)0x04) |
Default value for MinPINLen attribute.
| #define ZB_ZCL_DOOR_LOCK_MIN_RFID_CODE_LENGTH_DEFAULT_VALUE ((zb_uint8_t)0x08) |
Default value for MinRFIDCodeLength attribute.
| #define ZB_ZCL_DOOR_LOCK_NUM_HOLIDAY_SCHEDULE_DEFAULT_VALUE ((zb_uint8_t)0) |
Default value for NumHolidaySchedule attribute.
| #define ZB_ZCL_DOOR_LOCK_NUM_PIN_USERS_DEFAULT_VALUE ((zb_uint16_t)0) |
Default value for NumPINUsers attribute.
| #define ZB_ZCL_DOOR_LOCK_NUM_TOTAL_USERS_DEFAULT_VALUE ((zb_uint16_t)0) |
Default value for NumTotalUsers attribute.
| #define ZB_ZCL_DOOR_LOCK_NUM_WEEK_DAY_SCHEDULE_PER_USER_DEFAULT_VALUE ((zb_uint8_t)0) |
Default value for NumWeekDaySchedulePerUser attribute.
| #define ZB_ZCL_DOOR_LOCK_NUM_YEAR_DAY_SCHEDULE_PER_USER_DEFAULT_VALUE ((zb_uint8_t)0) |
Default value for NumYearDaySchedulePerUser attribute.
| #define ZB_ZCL_DOOR_LOCK_NUMBER_OF_LOG_RECORDS_SUPPORTED_DEFAULT_VALUE ((zb_uint16_t)0) |
Default value for NumberOfLogRecordsSupported attribute.
| #define ZB_ZCL_DOOR_LOCK_NUMBER_OF_RFID_USERS_SUPPORTED_DEFAULT_VALUE ((zb_uint16_t)0) |
Default value for NumberOfRFIDUsersSupported attribute.
| #define ZB_ZCL_DOOR_LOCK_OPERATING_MODE_DEFAULT_VALUE ((zb_uint8_t)0) |
Default value for OperatingMode attribute.
| #define ZB_ZCL_DOOR_LOCK_OPERATION_MODES_SUPPORTED_DEFAULT_VALUE ((zb_uint16_t)0x0001) |
Default value for OperationModesSupported attribute.
| #define ZB_ZCL_DOOR_LOCK_READ_LOCK_DOOR_RES | ( | buffer | ) |
Door Lock response structured reading.
| buffer | - ID of the message buffer (of type zb_bufid_t) containing payload |
| #define ZB_ZCL_DOOR_LOCK_READ_UNLOCK_DOOR_RES | ( | buffer | ) |
Door unLock response structured reading.
| buffer | - ID of the message buffer (of type zb_buf_t) containing payload |
| #define ZB_ZCL_DOOR_LOCK_REQUIRE_PIN_RF_ID_DEFAULT_VALUE ((zb_bool_t)0) |
Default value for RequirePIN_RF_ID attribute.
| #define ZB_ZCL_DOOR_LOCK_RF_OPERATION_EVENT_MASK_DEFAULT_VALUE ((zb_uint16_t)0x0000) |
Default value for RFOperationEventMask attribute.
| #define ZB_ZCL_DOOR_LOCK_RF_PROGRAMMING_EVENT_MASK_DEFAULT_VALUE ((zb_uint16_t)0x0000) |
Default value for RFProgrammingEventMask attribute.
| #define ZB_ZCL_DOOR_LOCK_RFID_OPERATION_EVENT_MASK_DEFAULT_VALUE ((zb_uint16_t)0x0000) |
Default value for RFIDOperationEventMask attribute.
| #define ZB_ZCL_DOOR_LOCK_RFID_PROGRAMMING_EVENT_MASK_DEFAULT_VALUE ((zb_uint16_t)0x0000) |
Default value for RFIDProgrammingEventMask attribute.
| #define ZB_ZCL_DOOR_LOCK_SECURITY_LEVEL_DEFAULT_VALUE ((zb_uint8_t)0) |
Default value for SecurityLevel attribute.
| #define ZB_ZCL_DOOR_LOCK_SEND_LOCK_DOOR_REQ | ( | buffer, | |
| dst_addr, | |||
| dst_addr_mode, | |||
| dst_ep, | |||
| ep, | |||
| dis_default_resp, | |||
| cb | |||
| ) |
General macro for sending a "Door Lock" cluster command.
| buffer | to put command payload and headers to |
| dst_addr | address to send to |
| dst_addr_mode | destination address mode |
| dst_ep | destination endpoint |
| ep | source endpoint |
| dis_default_resp | "Disable default response" flag |
| cb | command send status callback |
| #define ZB_ZCL_DOOR_LOCK_SEND_LOCK_DOOR_RES | ( | buffer, | |
| addr, | |||
| dst_addr_mode, | |||
| dst_ep, | |||
| ep, | |||
| prfl_id, | |||
| seq_num, | |||
| status, | |||
| aps_secured | |||
| ) |
Door Lock command send response macro.
| buffer | to put packet to |
| addr | - address to send packet to |
| dst_addr_mode | - addressing mode |
| dst_ep | - destination endpoint |
| ep | - sending endpoint |
| prfl_id | - profile identifier |
| seq_num | - sequence number |
| status | - result of command execute |
| aps_secured | - APS security mode |
| #define ZB_ZCL_DOOR_LOCK_SEND_PIN_OVER_THE_AIR_DEFAULT_VALUE ((zb_bool_t)0) |
Default value for SendPINOverTheAir attribute.
| #define ZB_ZCL_DOOR_LOCK_SEND_UNLOCK_DOOR_REQ | ( | buffer, | |
| dst_addr, | |||
| dst_addr_mode, | |||
| dst_ep, | |||
| ep, | |||
| dis_default_resp, | |||
| cb | |||
| ) |
General macro for sending a "Door Unlock" cluster command.
| buffer | to put command payload and headers to |
| dst_addr | address to send to |
| dst_addr_mode | destination address mode |
| dst_ep | destination endpoint |
| ep | source endpoint |
| dis_default_resp | "Disable default response" flag |
| cb | command send status callback |
| #define ZB_ZCL_DOOR_LOCK_SEND_UNLOCK_DOOR_RES | ( | buffer, | |
| addr, | |||
| dst_addr_mode, | |||
| dst_ep, | |||
| ep, | |||
| prfl_id, | |||
| seq_num, | |||
| status, | |||
| aps_secured | |||
| ) |
Door Unlock command send response macro.
| buffer | to put packet to |
| addr | - address to send packet to |
| dst_addr_mode | - addressing mode |
| dst_ep | - destination endpoint |
| ep | - sending endpoint |
| prfl_id | - profile identifier |
| seq_num | - sequence number |
| status | - result of command execute |
| aps_secured | - APS security mode |
| #define ZB_ZCL_DOOR_LOCK_SOUND_VOLUME_DEFAULT_VALUE ((zb_uint8_t)0) |
Default value for SoundVolume attribute.
| #define ZB_ZCL_DOOR_LOCK_USER_CODE_TEMPORARY_DISABLE_TIME_DEFAULT_VALUE ((zb_uint8_t)0) |
Default value for UserCodeTemporaryDisableTime attribute.
| #define ZB_ZCL_DOOR_LOCK_WRONG_CODE_ENTRY_LIMIT_DEFAULT_VALUE ((zb_uint8_t)0) |
Default value for WrongCodeEntryLimit attribute.
| typedef struct zb_zcl_door_lock_read_lock_door_res_payload_s zb_zcl_door_lock_read_lock_door_res_payload_t |
Door lock commands response payload structure
| typedef struct zb_zcl_door_lock_read_unlock_door_res_payload_s zb_zcl_door_lock_read_unlock_door_res_payload_t |
Door unlock commands response payload structure
Door Lock cluster attribute identifiers.
Door Lock cluster commands.
Door Lock cluster commands response.
Values for DoorState attribute.
Values for LockState attribute.
Values for LockType attribute.