The Daily Schedule cluster allows information that can be scheduled for an entire day to be transferred within the premises. The information is distributed by an ESI or similar server device.
§ ZB_ZCL_DAILY_SCHEDULE_CURRENT_AUXILLARY_LOAD_SWITCH_STATE_DEFAULT_VALUE
| #define ZB_ZCL_DAILY_SCHEDULE_CURRENT_AUXILLARY_LOAD_SWITCH_STATE_DEFAULT_VALUE 0x00 |
§ ZB_ZCL_DAILY_SCHEDULE_CURRENT_TARIFF_LABEL_DEFAULT_VALUE
| #define ZB_ZCL_DAILY_SCHEDULE_CURRENT_TARIFF_LABEL_DEFAULT_VALUE {0} |
§ ZB_ZCL_DAILY_SCHEDULE_LINKY_PEAK_PERIOD_STATUS_DEFAULT_VALUE
| #define ZB_ZCL_DAILY_SCHEDULE_LINKY_PEAK_PERIOD_STATUS_DEFAULT_VALUE 0x00 |
§ ZB_ZCL_DAILY_SCHEDULE_PEAK_END_TIME_DEFAULT_VALUE
| #define ZB_ZCL_DAILY_SCHEDULE_PEAK_END_TIME_DEFAULT_VALUE ((zb_uint32_t)0xFFFFFFFF) |
§ ZB_ZCL_DAILY_SCHEDULE_PEAK_START_TIME_DEFAULT_VALUE
| #define ZB_ZCL_DAILY_SCHEDULE_PEAK_START_TIME_DEFAULT_VALUE ((zb_uint32_t)0xFFFFFFFF) |