Macros | |
| #define | zb_address_lock(ref) zb_address_lock_func(TRACE_ADDR_CALL ref) |
| #define | zb_address_unlock(ref) zb_address_unlock_func(TRACE_ADDR_CALL ref) |
Typedefs | |
| typedef zb_uint8_t | zb_address_pan_id_ref_t |
| typedef zb_uint8_t | zb_address_ieee_ref_t |
| #define zb_address_lock | ( | ref | ) | zb_address_lock_func(TRACE_ADDR_CALL ref) |
Increase address lock counter, when it used in some table. Address must be already locked.
| ref | - IEEE/network address pair reference |
| #define zb_address_unlock | ( | ref | ) | zb_address_unlock_func(TRACE_ADDR_CALL ref) |
Unlock address counter. Decrease lock counter.
| ref | - IEEE/network address pair reference |
| typedef zb_uint8_t zb_address_ieee_ref_t |
IEEE address reference
Should be used inside protocol tables instead of 64/16-bit IEEE.
| typedef zb_uint8_t zb_address_pan_id_ref_t |
Pan ID reference
Should be used inside protocol tables instead of 64-bit Pan ID
| zb_ret_t zb_address_by_ieee | ( | const zb_ieee_addr_t | ieee, |
| zb_bool_t | create, | ||
| zb_bool_t | lock, | ||
| zb_address_ieee_ref_t * | ref_p | ||
| ) |
Get address ref by long address, optionally create if not exist, optionally lock. Update address alive time if not locked.
| ieee | - IEEE device address |
| create | - if TRUE, create address entry if it does not exist |
| lock | - if TRUE, lock address entry |
| ref_p | - (out) address reference |
Example
| void zb_address_by_ref | ( | zb_ieee_addr_t | ieee_address, |
| zb_uint16_t * | short_address_p, | ||
| zb_address_ieee_ref_t | ref | ||
| ) |
Get address with address reference.
Get existing IEEE (long) and short addresses with address reference. Update address alive time if it not locked.
| ieee_address | - (out) long address |
| short_address_p | - (out) short address |
| ref | - address reference |
Example
| zb_ret_t zb_address_by_short | ( | zb_uint16_t | short_address, |
| zb_bool_t | create, | ||
| zb_bool_t | lock, | ||
| zb_address_ieee_ref_t * | ref_p | ||
| ) |
Get address reference by short address. Create the reference if it does not exist. Optionally, lock the address. Update address alive time if not locked.
| short_address | - 16bit device address |
| create | - if TRUE, create address entry if it does not exist |
| lock | - if TRUE, lock address entry |
| ref_p | - (out) address reference |
Example
| zb_bool_t zb_address_cmp_pan_id_by_ref | ( | zb_address_pan_id_ref_t | pan_id_ref, |
| zb_ext_pan_id_t | pan_id | ||
| ) |
Compare Pan ID in the source form with Pan ID reference.
| pan_id_ref | - Pan ID ref |
| pan_id | - Pan ID (64-bit) |
Example
| zb_ret_t zb_address_delete | ( | zb_address_ieee_ref_t | ref | ) |
Delete address.
| ref | - IEEE/network address pair reference |
| void zb_address_done_ieee_disc | ( | zb_uint16_t | short_addr | ) |
| void zb_address_done_short_disc | ( | zb_address_ieee_ref_t | ref | ) |
| void zb_address_dump_redirs | ( | void | ) |
| zb_ret_t zb_address_get_by_ieee | ( | const zb_ieee_addr_t | ieee, |
| zb_address_ieee_ref_t * | ref_p | ||
| ) |
Get address ref by long address, do not lock.
This is a read-only version of zb_address_by_ieee(). Always use it if address not need to be created.
| ieee | - IEEE device address |
| ref_p | - (out) address reference |
| zb_ret_t zb_address_get_by_ieee_lk | ( | const zb_ieee_addr_t | ieee, |
| zb_address_ieee_ref_t * | ref_p | ||
| ) |
Get address ref by long address, lock the address
This is a read-only version of zb_address_by_ieee(). Always use it if address not need to be created.
| ieee | - IEEE device address |
| ref_p | - (out) address reference |
| zb_ret_t zb_address_get_by_short | ( | zb_uint16_t | short_address, |
| zb_address_ieee_ref_t * | ref_p | ||
| ) |
Get address reference by short address, do not lock.
This is a read-only version of zb_address_by_short().
| short_address | - 16bit device address |
| ref_p | - (out) address reference |
| zb_ret_t zb_address_get_by_short_lk | ( | zb_uint16_t | short_address, |
| zb_address_ieee_ref_t * | ref_p | ||
| ) |
Get address reference by short address, lock address
This is a read-only version of zb_address_by_short() adding an address lock.
| short_address | - 16bit device address |
| ref_p | - (out) address reference |
| zb_ret_t zb_address_get_pan_id_ref | ( | zb_ext_pan_id_t | pan_id, |
| zb_address_pan_id_ref_t * | ref | ||
| ) |
Get Pan ID reference with extended Pan ID.
| pan_id | - Pan ID |
| ref | - (output) reference to Pan ID |
Example
| void zb_address_get_short_pan_id | ( | zb_address_pan_id_ref_t | pan_id_ref, |
| zb_uint16_t * | pan_id_p | ||
| ) |
Get short Pan ID with reference.
| pan_id_ref | - reference to Pan ID |
| pan_id_p | - (output) Pan ID. |
Example
| void zb_address_ieee_by_ref | ( | zb_ieee_addr_t | ieee_address, |
| zb_address_ieee_ref_t | ref | ||
| ) |
Get IEEE address with address reference.
Get existing IEEE address(long address) with address reference. Update address alive time if it not locked.
| ieee_address | - (out) long address |
| ref | - address reference |
Example
| zb_ret_t zb_address_ieee_by_short | ( | zb_uint16_t | short_addr, |
| zb_ieee_addr_t | ieee_address | ||
| ) |
Get IEEE address (long) with short address.
| short_addr | - short address |
| ieee_address | - (out)long address |
Example
| zb_bool_t zb_address_is_locked | ( | zb_address_ieee_ref_t | ref | ) |
Check that address is locked (has lock counter > 0)
| ref | - IEEE/network address pair reference |
| zb_ret_t zb_address_lock_func | ( | TRACE_ADDR_PROTO zb_address_ieee_ref_t | ref | ) |
| zb_bool_t zb_address_setup_ieee_disc | ( | zb_uint16_t | short_addr | ) |
| zb_bool_t zb_address_setup_short_disc | ( | zb_address_ieee_ref_t | ref | ) |
| zb_uint16_t zb_address_short_by_ieee | ( | const zb_ieee_addr_t | ieee_address | ) |
Get short address by IEEE address (long).
| ieee_address | - long address |
| void zb_address_short_by_ref | ( | zb_uint16_t * | short_address_p, |
| zb_address_ieee_ref_t | ref | ||
| ) |
Get short address by address reference.
Get existing short address with address reference. Update address alive time if it not locked.
| short_address_p | - (out) short address |
| ref | - address reference |
Example
| void zb_address_unlock_func | ( | TRACE_ADDR_PROTO zb_address_ieee_ref_t | ref | ) |
| zb_ret_t zb_address_update | ( | zb_ieee_addr_t | ieee_address, |
| zb_uint16_t | short_address, | ||
| zb_bool_t | lock, | ||
| zb_address_ieee_ref_t * | ref_p | ||
| ) |
Update long/short address pair. Create the pair if not exist. Optionally, lock. Reaction on device announce etc. Long and short addresses are present. Must synchronize the address translation table with this information.
| ieee_address | - long address |
| short_address | - short address |
| lock | - if TRUE, lock address entry |
| ref_p | - (out) address reference |
Example
| zb_ret_t zb_address_update_if_absent | ( | zb_ieee_addr_t | ieee_address, |
| zb_uint16_t | short_address | ||
| ) |
Update address pair if one or oth of its component were unknown.
| ieee_address | - long address |
| short_address | - short address |
| void zb_long_address_update_by_ref | ( | zb_ieee_addr_t | ieee_address, |
| zb_address_ieee_ref_t | ref | ||
| ) |