Logo
DSR GreenBOSS  1.1.0
Data Fields
zb_zgpd_addr_u Union Reference

ZGPD address. More...

#include <zb_nwk.h>

Data Fields

zb_uint32_t src_id
 ZGPD SrcId. More...
 
zb_ieee_addr_t ieee_addr
 ZGPD IEEE address. More...
 

Detailed Description

ZGPD address.

ZGPD is identified in network whether by SrcId or its IEEE address.

Field Documentation

§ src_id

zb_uint32_t zb_zgpd_addr_u::src_id

ZGPD SrcId.

See also
ZGP spec, A.1.4.1.4

§ ieee_addr

zb_ieee_addr_t zb_zgpd_addr_u::ieee_addr

ZGPD IEEE address.


The documentation for this union was generated from the following file: