Parser MAC header.
More...
#include <zb_mac.h>
Parser MAC header.
Mac spec 7.2.1 General MAC frame format.
- Note
- Actually MHR is of variable length and this structure can't be used for physical data i/o, it is used only for function calls.
The documentation for this struct was generated from the following file: