Logo
DSR GreenBOSS  1.1.0
API Reference Guide
Here is a list of all modules:
[detail level 1234]
 Application GPD APIThe module describes main GPD API that should be used to make own Green Power device
 Application Initialization and Configuration
 GPD Сommissioning API
 GPD Commands API
 ON/OFF Сluster Сommands
 Scene Сluster Сommands
 Level Control Сluster Сommands
 Color Control Сluster Сommands
 Door Lock Сluster Сommands
 ZCL Attribute Reporting
 Zigbee Cluster Common Definitions
 IAS Zone Cluster Definitions
 Power Configuration Cluster Definitions
 Bidirectional in Operational APISpecifics of Bidirectional in Operational mode
 Commands to be sent by the Bidirectional in Operational application
 Helper functions for handling received commands
 Functions to provide Rx after Tx for Bidirectional in Operational application
 GreenBOSS InternalsThe module describes some internal GreenBOSS interfaces
 Basic Typedefs
 Interface to the Radio
 Interface to the Flash
 GPD Security
 MAC Level
 Network Level
 Commissioning Internals
 GreenBOSS Debug Capabilities
 Asserts
 Debug Trace
 Build Configurations