Data Fields
KeyStore_s_GetKeyMsg Struct Reference

#include <CryptoKeyKeyStore_PSA_s.h>

Data Fields

uint32_t key
 
uint8_t * data
 
size_t dataSize
 
size_t * dataLength
 
KeyStore_PSA_Algorithm alg
 
KeyStore_PSA_KeyUsage usage
 

Field Documentation

§ key

uint32_t KeyStore_s_GetKeyMsg::key

§ data

uint8_t* KeyStore_s_GetKeyMsg::data

§ dataSize

size_t KeyStore_s_GetKeyMsg::dataSize

§ dataLength

size_t* KeyStore_s_GetKeyMsg::dataLength

§ alg

KeyStore_PSA_Algorithm KeyStore_s_GetKeyMsg::alg

§ usage

KeyStore_PSA_KeyUsage KeyStore_s_GetKeyMsg::usage

The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale