ECDSALPF3SW.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2021-2023, Texas Instruments Incorporated
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * * Redistributions of source code must retain the above copyright
10  * notice, this list of conditions and the following disclaimer.
11  *
12  * * Redistributions in binary form must reproduce the above copyright
13  * notice, this list of conditions and the following disclaimer in the
14  * documentation and/or other materials provided with the distribution.
15  *
16  * * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
54 #ifndef ti_drivers_ecdsa_ECDSALPF3SW__include
55 #define ti_drivers_ecdsa_ECDSALPF3SW__include
56 
57 #include <stdint.h>
58 #include <stdbool.h>
59 
60 #include <ti/drivers/ECDSA.h>
61 
62 #include <third_party/ecc/include/lowlevelapi.h>
63 
64 #ifdef __cplusplus
65 extern "C" {
66 #endif
67 
74 typedef struct
75 {
76  uint8_t dummy;
78 
79 /*
80  * Performance of the ECC SW library is scaled via the window size parameter
81  * which defines the number of bits of the scalar that will be processed together
82  * during the execution of the scalar multiplication. A larger window size
83  * will have higher performance at the cost of increased memory consumption.
84  * A window size of 3 was selected for the best trade-off of performance and
85  * memory consumption. WorkZone size was empirically measured.
86  *
87  * ---------------------------------
88  * | | NIST P256 |
89  * | Window Size | WorkZone Size |
90  * | | (words) |
91  * |-------------|-----------------|
92  * | 2 | 227 |
93  * | 3 | 254 |
94  * | 4 | 308 |
95  * | 5 | 416 |
96  * ---------------------------------
97  */
98 #ifndef ECDSALPF3SW_ECC_WINDOW_SIZE
99  #define ECDSALPF3SW_ECC_WINDOW_SIZE 3
100 #endif
101 
102 /*
103  * ECC Workzone size is based on worst case empirical measurement of ECDH
104  * operations on supported curves with the selected window size.
105  */
106 #if (ECDSALPF3SW_ECC_WINDOW_SIZE == 2)
107  #define ECDSALPF3SW_ECC_WORKZONE_WORDS 227
108 #elif (ECDSALPF3SW_ECC_WINDOW_SIZE == 3)
109  #define ECDSALPF3SW_ECC_WORKZONE_WORDS 254
110 #elif (ECDSALPF3SW_ECC_WINDOW_SIZE == 4)
111  #define ECDSALPF3SW_ECC_WORKZONE_WORDS 308
112 #elif (ECDSALPF3SW_ECC_WINDOW_SIZE == 5)
113  #define ECDSALPF3SW_ECC_WORKZONE_WORDS 416
114 #else
115  #error "Invalid ECDSALPF3SW_ECC_WINDOW_SIZE"
116 #endif
117 
123 typedef struct
124 {
125  bool isOpen;
126  ECDSA_ReturnBehavior returnBehavior; /* Callback mode is not supported */
127  ECC_State eccState;
128  uint32_t eccWorkZone[ECDSALPF3SW_ECC_WORKZONE_WORDS];
130 
131 #ifdef __cplusplus
132 }
133 #endif
134 
135 #endif /* ti_drivers_ecdsa_ECDSALPF3SW__include */
TI Driver for Elliptic Curve Digital Signature Algorithm.
ECDSA_ReturnBehavior
The way in which ECDSA function calls return after performing an encryption + authentication or decry...
Definition: ECDSA.h:622
bool isOpen
Definition: ECDSALPF3SW.h:125
ECDSALPF3SW Object.
Definition: ECDSALPF3SW.h:123
ECC_State eccState
Definition: ECDSALPF3SW.h:127
ECDSA_ReturnBehavior returnBehavior
Definition: ECDSALPF3SW.h:126
#define ECDSALPF3SW_ECC_WORKZONE_WORDS
Definition: ECDSALPF3SW.h:109
uint8_t dummy
Definition: ECDSALPF3SW.h:76
ECDSALPF3SW Hardware Attributes.
Definition: ECDSALPF3SW.h:74
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale