ECDSA.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2017-2024, Texas Instruments Incorporated
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * * Redistributions of source code must retain the above copyright
10  * notice, this list of conditions and the following disclaimer.
11  *
12  * * Redistributions in binary form must reproduce the above copyright
13  * notice, this list of conditions and the following disclaimer in the
14  * documentation and/or other materials provided with the distribution.
15  *
16  * * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
457 #ifndef ti_drivers_ECDSA__include
458 #define ti_drivers_ECDSA__include
459 
460 #include <stdbool.h>
461 #include <stddef.h>
462 #include <stdint.h>
463 
466 
467 #ifdef __cplusplus
468 extern "C" {
469 #endif
470 
483 #define ECDSA_STATUS_RESERVED (-32)
484 
491 #define ECDSA_STATUS_SUCCESS (0)
492 
499 #define ECDSA_STATUS_ERROR (-1)
500 
510 #define ECDSA_STATUS_RESOURCE_UNAVAILABLE (-2)
511 
518 #define ECDSA_STATUS_R_LARGER_THAN_ORDER (-3)
519 
526 #define ECDSA_STATUS_S_LARGER_THAN_ORDER (-4)
527 
534 #define ECDSA_STATUS_PUBLIC_KEY_NOT_ON_CURVE (-5)
535 
543 #define ECDSA_STATUS_PUBLIC_KEY_LARGER_THAN_PRIME (-6)
544 
550 #define ECDSA_STATUS_POINT_AT_INFINITY (-7)
551 
555 #define ECDSA_STATUS_CANCELED (-8)
556 
565 #define ECDSA_STATUS_INVALID_KEY_SIZE (-10)
566 
573 #define ECDSA_STATUS_KEYSTORE_ERROR (-11)
574 
586 typedef struct
587 {
589  void *object;
590 
592  void const *hwAttrs;
593 } ECDSA_Config;
594 
599 
622 typedef enum
623 {
639 
640 #if ((DeviceFamily_PARENT == DeviceFamily_PARENT_CC27XX) || (DeviceFamily_PARENT == DeviceFamily_PARENT_CC35XX))
641 
644 typedef enum
645 {
654 
658 typedef enum
659 {
667 
671 typedef enum
672 {
678 #endif
679 
683 typedef struct
684 {
685 #if ((DeviceFamily_PARENT == DeviceFamily_PARENT_CC27XX) || (DeviceFamily_PARENT == DeviceFamily_PARENT_CC35XX))
687 #endif
692  const uint8_t *hash;
696  uint8_t *r;
702  uint8_t *s;
708 
712 typedef struct
713 {
714 #if ((DeviceFamily_PARENT == DeviceFamily_PARENT_CC27XX) || (DeviceFamily_PARENT == DeviceFamily_PARENT_CC35XX))
716 #else
717  const ECCParams_CurveParams *curve;
718 #endif
722  const uint8_t *hash;
726  const uint8_t *r;
732  const uint8_t *s;
739 
743 typedef union
744 {
748 
752 typedef enum
753 {
757 
777 typedef void (*ECDSA_CallbackFxn)(ECDSA_Handle handle,
778  int_fast16_t returnStatus,
779  ECDSA_Operation operation,
780  ECDSA_OperationType operationType);
781 
790 typedef struct
791 {
796  uint32_t timeout;
799  void *custom;
802 } ECDSA_Params;
803 
809 extern const ECDSA_Params ECDSA_defaultParams;
810 
819 void ECDSA_init(void);
820 
830 void ECDSA_close(ECDSA_Handle handle);
831 
849 ECDSA_Handle ECDSA_open(uint_least8_t index, const ECDSA_Params *params);
850 
863 void ECDSA_Params_init(ECDSA_Params *params);
864 
874 
884 
913 int_fast16_t ECDSA_sign(ECDSA_Handle handle, ECDSA_OperationSign *operation);
914 
942 int_fast16_t ECDSA_verify(ECDSA_Handle handle, ECDSA_OperationVerify *operation);
943 
957 int_fast16_t ECDSA_cancelOperation(ECDSA_Handle handle);
958 
983 ECDSA_Handle ECDSA_construct(ECDSA_Config *config, const ECDSA_Params *params);
984 
985 #ifdef __cplusplus
986 }
987 #endif
988 
989 #endif /* ti_drivers_ECDSA__include */
Definition: ECDSA.h:647
ECDSA_CurveType
Enum for the curve types supported by the driver.
Definition: ECDSA.h:644
ECDSA_ReturnBehavior
The way in which ECDSA function calls return after performing an encryption + authentication or decry...
Definition: ECDSA.h:622
Definition: ECDSA.h:650
uint8_t * s
Definition: ECDSA.h:702
The CryptoKey type is an opaque representation of a cryptographic key.
const CryptoKey * myPrivateKey
Definition: ECDSA.h:689
ECDSA_CurveType curveType
Definition: ECDSA.h:715
Definition: ECDSA.h:755
const uint8_t * hash
Definition: ECDSA.h:692
Definition: ECDSA.h:649
void ECDSA_OperationSign_init(ECDSA_OperationSign *operation)
Function to initialize an ECDSA_OperationSign struct to its defaults.
Definition: ECDSA.h:648
void const * hwAttrs
Definition: ECDSA.h:592
const CryptoKey * theirPublicKey
Definition: ECDSA.h:719
void(* ECDSA_CallbackFxn)(ECDSA_Handle handle, int_fast16_t returnStatus, ECDSA_Operation operation, ECDSA_OperationType operationType)
The definition of a callback function used by the ECDSA driver when used in ECDSA_RETURN_BEHAVIOR_CAL...
Definition: ECDSA.h:777
Definition: ECDSA.h:663
Definition: ECDSA.h:646
ECDSA_ReturnBehavior returnBehavior
Definition: ECDSA.h:792
const uint8_t * s
Definition: ECDSA.h:732
Definition: ECDSA.h:651
Definition: ECDSA.h:675
CryptoKey datastructure.
Definition: CryptoKey.h:211
ECDSA_DigestLength
Enum for the hash digest lengths in bits supported by the driver.
Definition: ECDSA.h:671
ECDSA Global configuration.
Definition: ECDSA.h:586
Definition: ECDSA.h:665
void ECDSA_close(ECDSA_Handle handle)
Function to close an ECDSA peripheral specified by the ECDSA handle.
void ECDSA_init(void)
This function initializes the ECDSA module.
Struct containing the parameters required for signing a message.
Definition: ECDSA.h:683
const ECDSA_Params ECDSA_defaultParams
Default ECDSA_Params structure.
Definition: ECDSA.h:661
Definition: ECDSA.h:674
ECDSA Parameters.
Definition: ECDSA.h:790
ECDSA_CurveLength
Enum for signature sizes in bits supported by the driver.
Definition: ECDSA.h:658
const ECCParams_CurveParams * curve
Definition: ECDSA.h:688
ECDSA_OperationType
Enum for the operation types supported by the driver.
Definition: ECDSA.h:752
Definition: ECDSA.h:664
void ECDSA_Params_init(ECDSA_Params *params)
Function to initialize the ECDSA_Params struct to its defaults.
const uint8_t * r
Definition: ECDSA.h:726
Union containing pointers to all supported operation structs.
Definition: ECDSA.h:743
Definition: ECDSA.h:660
Definition: ECDSA.h:634
int_fast16_t ECDSA_sign(ECDSA_Handle handle, ECDSA_OperationSign *operation)
Signs a hashed message.
void * custom
Definition: ECDSA.h:799
ECDSA_Config * ECDSA_Handle
A handle that is returned from an ECDSA_open() call.
Definition: ECDSA.h:598
uint8_t * r
Definition: ECDSA.h:696
int_fast16_t ECDSA_verify(ECDSA_Handle handle, ECDSA_OperationVerify *operation)
Verifies a received signature matches a hash and public key.
Struct containing the parameters required for verifying a message.
Definition: ECDSA.h:712
void * object
Definition: ECDSA.h:589
Definition: ECDSA.h:652
ECDSA_CallbackFxn callbackFxn
Definition: ECDSA.h:795
Definition: ECDSA.h:673
ECDSA_OperationVerify * verify
Definition: ECDSA.h:746
Definition: ECDSA.h:630
ECDSA_CurveType curveType
Definition: ECDSA.h:686
A structure containing the parameters of an elliptic curve.
Definition: ECCParams.h:143
Definition: ECDSA.h:624
const uint8_t * hash
Definition: ECDSA.h:722
ECDSA_Handle ECDSA_open(uint_least8_t index, const ECDSA_Params *params)
This function opens a given ECDSA peripheral.
Definition: ECDSA.h:676
Definition: ECDSA.h:754
ECDSA_OperationSign * sign
Definition: ECDSA.h:745
uint32_t timeout
Definition: ECDSA.h:796
Definition: ECDSA.h:662
ECDSA_Handle ECDSA_construct(ECDSA_Config *config, const ECDSA_Params *params)
Constructs a new ECDSA object.
void ECDSA_OperationVerify_init(ECDSA_OperationVerify *operation)
Function to initialize an ECDSA_OperationSign struct to its defaults.
int_fast16_t ECDSA_cancelOperation(ECDSA_Handle handle)
Cancels an ongoing ECDSA operation.
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale