Data Structures | Macros | Typedefs
AESECBLPF3.h File Reference

Detailed Description

AESECB driver implementation for the Low Power F3 family.

==========================================================================

Hardware Accelerator

The Low Power F3 family of devices has dedicated hardware accelerators. CC23XX devices have one dedicated accelerator whereas CC27XX devices have two (Primary and Secondary). Combined they can perform AES encryption operations with 128-bit, 192-bit and 256-bit keys. Only one operation can be carried out on the accelerator at a time. Mutual exclusion is implemented at the driver level and coordinated between all drivers relying on the accelerator. It is transparent to the application and only noted to ensure sensible access timeouts are set.

Implementation Limitations

Runtime Parameter Validation

The driver implementation does not perform runtime checks for most input parameters. Only values that are likely to have a stochastic element to them are checked (such as whether a driver is already open). Higher input parameter validation coverage is achieved by turning on assertions when compiling the driver.

#include <stdbool.h>
#include <stdint.h>
#include <ti/drivers/AESECB.h>
#include <ti/drivers/cryptoutils/aes/AESCommonLPF3.h>
#include <ti/drivers/cryptoutils/sharedresources/CryptoResourceLPF3.h>
#include <ti/drivers/cryptoutils/cryptokey/CryptoKeyKeyStore_PSA.h>
Include dependency graph for AESECBLPF3.h:

Go to the source code of this file.

Data Structures

struct  AESECBLPF3_Object
 AESECBLPF3 Object. More...
 

Macros

#define AESECBLPF3_DMA_SIZE_THRESHOLD   (1U * AES_BLOCK_SIZE)
 
#define AESECBLPF3_SINGLE_BLOCK_AUTOCFG   ((uint32_t)AES_AUTOCFG_AESSRC_BUF | (uint32_t)AES_AUTOCFG_TRGAES_WRBUF3S | (uint32_t)AES_AUTOCFG_BUSHALT_EN)
 

Typedefs

typedef AESCommonLPF3_HWAttrs AESECBLPF3_HWAttrs
 AESECBLPF3 Hardware Attributes. More...
 

Macro Definition Documentation

§ AESECBLPF3_DMA_SIZE_THRESHOLD

#define AESECBLPF3_DMA_SIZE_THRESHOLD   (1U * AES_BLOCK_SIZE)

The threshold at which blocking and callback mode transfers will utilize DMA. For data lengths below this threshold, polling CPU R/W will be used instead of DMA. With task switching and interrupt overhead, it is inefficient to utilize DMA for shorter length operations. The threshold value must be a multiple of AES_BLOCK_SIZE.

§ AESECBLPF3_SINGLE_BLOCK_AUTOCFG

#define AESECBLPF3_SINGLE_BLOCK_AUTOCFG   ((uint32_t)AES_AUTOCFG_AESSRC_BUF | (uint32_t)AES_AUTOCFG_TRGAES_WRBUF3S | (uint32_t)AES_AUTOCFG_BUSHALT_EN)

Typedef Documentation

§ AESECBLPF3_HWAttrs

AESECBLPF3 Hardware Attributes.

AESECBLPF3 hardware attributes should be included in the board file and pointed to by the AESECB_config struct.

© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale