![]() |
![]() |
AESCCM driver implementation for the Low Power F3 family.
==========================================================================
This implementation follows NIST 800-38c - https://nvlpubs.nist.gov/nistpubs/Legacy/SP/nistspecialpublication800-38c.pdf All symbols used in the implementation for identifiers and in the comments including but not limited to B0, B1 and S0 are all adopted from this NIST 800-38c.
The Low Power F3 family of devices has dedicated hardware accelerators. CC23XX devices have one dedicated accelerator whereas CC27XX devices have two (Primary and Secondary). Combined they can perform AES encryption operations with 128-bit, 192-bit and 256-bit keys. CC35XX devices have only one dedicated hardware accelerator. Only one operation can be carried out on the accelerator at a time. Mutual exclusion is implemented at the driver level and coordinated between all drivers relying on the accelerator. It is transparent to the application and only noted to ensure sensible access timeouts are set.
The following limitations apply to the AESCCMLPF3 Driver for CC27xx and CC35XX device families:
The driver implementation does not perform runtime checks for most input parameters. Only values that are likely to have a stochastic element to them are checked (such as whether a driver is already open). Higher input parameter validation coverage is achieved by turning on assertions when compiling the driver.
#include <stdbool.h>#include <stdint.h>#include <ti/drivers/AESCCM.h>#include <ti/drivers/cryptoutils/aes/AESCommonLPF3.h>#include <ti/devices/DeviceFamily.h>#include <ti/drivers/cryptoutils/cryptokey/CryptoKeyKeyStore_PSA.h>
Go to the source code of this file.
Data Structures | |
| struct | AESCCMLPF3_Object |
| AESCCMLPF3 Object. More... | |
Macros | |
| #define | AESCCMLPF3_AAD_BUFFER_SIZE 2U |
Typedefs | |
| typedef AESCommonLPF3_HWAttrs | AESCCMLPF3_HWAttrs |
| AESCCMLPF3 Hardware Attributes. More... | |
Functions | |
| int_fast16_t | AESCCMLPF3HSM_setMac (AESCCM_Handle handle, const uint8_t *mac, size_t macLength) |
| Function to set the mac for an AES CCM segmented operation. This API needs to be called only when the subsequent AESCCM_addData() operation is processing all of the remaining data in a single call. More... | |
| #define AESCCMLPF3_AAD_BUFFER_SIZE 2U |
AESCCMLPF3 Hardware Attributes.
AESCCMLPF3 hardware attributes should be included in the board file and pointed to by the AESCCM_config struct.
| int_fast16_t AESCCMLPF3HSM_setMac | ( | AESCCM_Handle | handle, |
| const uint8_t * | mac, | ||
| size_t | macLength | ||
| ) |
Function to set the mac for an AES CCM segmented operation. This API needs to be called only when the subsequent AESCCM_addData() operation is processing all of the remaining data in a single call.
| [in] | handle | A CCM handle returned from AESCCM_open() or AESCCM_construct() |
| [in] | mac | Pointer to the buffer containing the mac |
| [in] | macLength | The length of the mac in bytes |
| AESCCM_STATUS_SUCCESS | The operation succeeded. |
| AESCCM_STATUS_ERROR | The operation failed. |
| AESCCM_STATUS_FEATURE_NOT_SUPPORTED | The operation is not supported in this device. |