SimpleLink Common Components Module 9.14.00 Release Notes
Table of Contents
Introduction
The SimpleLink Common Components Module (SCCM) includes NV Interface (Non-volatile Memory Interface) and MCUboot. These release notes include bug fixes, updates, and new features for the SCCM components.
Documentation
The follow table details which SCCM components are supported by the different SimpleLink stacks
| Stack | NV | MCUboot |
|---|---|---|
| BLE | X | X |
| PropRF | X | |
| Zigbee | X | X |
What’s New
| ID | Summary |
|---|---|
| SCCM-606 | Enable NVOCMP voltage check for CC23XX and CC27XX |
| SCCM-585 | Add SCCM Examples for LP_EM_CC2755R10_BG |
Fixed Issues
| ID | Summary |
|---|---|
| SCCM-608 | Compaction bug that results in items lost |
Known Issues and Limitations
| ID | Summary |
|---|---|
| None | None |
It should be noted that multiple external NVS regions are not supported. If a user attempts to create a second external NVS region, all actions on the second region will be done on the first region.
Upgrade and Compatibility Information
Dependencies
SCCM components were built & tested with the Integrated Development Environments (IDEs) and listed in the top-level SDK release notes.