Radio Control Layer (RCL)
Channel Sounding Precalibration Handler

Introduction

Usage

Architecture

RCL Event (In) Description
RCL_EventSetup Setup has been performed
RCL_EventTimerStart Timer-based start signalled
RCL Event (Out) Description
RCL_EventCmdStarted Command handler has accepted and started executing
RCL_EventLastCmdDone The RCL is finished with the command
LRF Event Description
LRF_EventOpDone The PBE operation has finished
LRF_EventOpError Something went wrong. Cause located in the PBE ENDCAUSE register