Radio Control Layer (RCL)
Secondary Channel Advertiser Command Handler

Introduction

The secondary channel advertiser command handler is a "special" handler meant for testing purposes that can be used for starting advertising on a secondary advertising channel. Unlike the advertiser handler, this command handler only supports extended advertising PDUs which use the secondary physical channel.

PDU Type PDU Name Physical Channel LE 1M LE 2M LE Coded Currently Supported
0b0111 AUX_ADV_IND Secondary * * * *
0b0111 AUX_SCAN_RSP Secondary * * * *
0b0111 AUX_SYNC_IND Periodic * * * *
0b0111 AUX_CHAIN_IND Secondary and Periodic * * * *
0b0111 AUX_SYNC_SUBEVENT_IND Periodic * * *
0b0111 AUX_SYNC_SUBEVENT_RSP Periodic * * *
0b1000 AUX_CONNECT_RSP Secondary * * * *

Usage

How the secondary advertiser command handler is configured and used depends on the type of PDU that is supposed to be sent. Nevertheless, the following basic steps must have taken place before submitting the an advertiser command:

  1. RCL has been initialized (See RCL_init) and a handle must exist (See RCL_open).
  2. The RCL_CMD_BLE5_AUX_ADV_t command has been initialized and configured.
  3. The necessary Tx buffer(s) have been initialized and configured.
  4. If needed, the necessary Multibuffer for reception has been initialized and configured.

Once these steps have been completed, RCL_Command_submit and RCL_Command_pend are called to effectively send a packet and then wait for the command to conclude. Alternatively, callbacks can be used for post-processing and the submitting of new commands.

Command configuration and submitting is similar to the advertiser command handler, with the exception that the command handler requires the configuration of a channel to start the operation.

void runSecondaryAdvertiser(void)
{
RCL_Handle h = RCL_open(&rclClient, &LRF_configBle);
RCL_Buffer_TxBuffer *auxAdvTxBuffer = (RCL_Buffer_TxBuffer *)txBuffer;
AuxPtr auxAdvAuxPtr;
auxAdvCmd.channel = 25;
auxAdvCmd.ctx = &auxAdvCtx;
auxAdvCmd.stats = &auxAdvStats;
auxAdvCmd.common.scheduling = RCL_Schedule_Now;
auxAdvCmd.common.runtime.callback = advCallback;
auxAdvCmd.common.runtime.lrfCallbackMask.value = 0;
auxAdvCmd.common.runtime.rclCallbackMask.value = RCL_EventLastCmdDone.value |
auxAdvStats = (RCL_StatsAdvScanInit) { 0 };
auxAdvStats.config.accumulate = true;
/* AuxPtr to be used for the AUX_ADV_IND indicating that the next auxiliary packet will be sent on:
* BLE 2M PHY, channel 5, and in 1.2 [ms].
*/
auxAdvAuxPtr.auxOffset = 4;
auxAdvAuxPtr.offsetUnits = 1;
auxAdvAuxPtr.auxPhy = 1;
auxAdvAuxPtr.ca = 0;
auxAdvAuxPtr.chIndex = 5;
/* Populate Tx buffer used for the AUX_ADV_IND that will be sent on a secondary advertisement channel */
setAuxAdvBuffer(auxAdvTxBuffer, &auxAdvAuxPtr, AUX_ADV_DATA_LEN);
auxAdvTxBuffer->state = RCL_BufferStatePending;
RCL_TxBuffer_put(&auxAdvCtx.txBuffers, auxAdvTxBuffer);
RCL_Command_submit(h, &auxAdvCmd);
/* Wait for command to conclude */
RCL_Command_pend(&auxAdvCmd);
}

Notice how the AuxPtr previously defined are used to populate the Tx Buffer with the help of a C struct.

typedef struct
{
uint8_t chIndex: 6;
uint8_t ca: 1;
uint8_t offsetUnits: 1;
uint16_t auxOffset: 13;
uint16_t auxPhy: 3;
} AuxPtr;

Architecture

The life cycle of the secondary advertiser command handler depends on the type advertising and more specifically the PDU type. The PDU type will determine aspects such as the number of Tx buffers needed for the operation, or whether the operation involves both Tx and Rx, or just Tx. It is the responsibility of the caller to provide a Tx Buffer containing a valid advertising physical channel PDU.

Furthermore, unlike the advertiser command handler, this command handler does not support the possibility to do PHY switching as this is meant to be handled during the primary channel advertising.

The following activity diagram illustrates the behavior of the secondary channel advertiser command handler.

RCL Event (In) Description
RCL_EventSetup Setup has been performed
RCL_EventTimerStart Timer-based start signalled
RCL_EventGracefulStop Graceful stop has been observed
RCL_EventHardStop Hard stop has been observed
RCL_EventRxBufferUpdate RX buffer has been updated
RCL Event (Out) Description
RCL_EventLastCmdDone The RCL is finished with the command
RCL_EventCmdStarted Command handler has accepted and started executing
RCL_EventRxBufferFinished An RX multi-buffer is finished
RCL_EventRxEntryAvail An RX entry has been made available
RCL_EventTxBufferFinished An TX buffer is finished
LRF Event Description
LRF_EventOpDone The PBE operation has finished
LRF_EventOpError Something went wrong. Cause located in the PBE ENDCAUSE register
LRF_EventRxOk Packet received with CRC OK and not to be ignored by the MCU
LRF_EventRxNok Packet received with CRC error
LRF_EventRxIgnored Packet received, but may be ignored by MCU