33 #ifndef ti_drivers_RCL_Scheduler_h__include 34 #define ti_drivers_RCL_Scheduler_h__include 45 #define RCL_SCHEDULER_SYSTIM_US(x) (((uint32_t) (x)) * 4U) 49 #define RCL_SCHEDULER_SYSTIM_MS(x) (((uint32_t) (x)) * 4U * 1000U) 53 #define ABS_START_TIME_OFFSET RCL_SCHEDULER_SYSTIM_US(100U) 54 #define IMM_START_TIME_OFFSET RCL_SCHEDULER_SYSTIM_US(90U) 55 #define RCL_SCHEDULER_MARGIN_ARM RCL_SCHEDULER_SYSTIM_US(40U) 56 #define RCL_SCHEDULER_MARGIN_CONFIGURE RCL_SCHEDULER_SYSTIM_US(76U) 57 #define RCL_SCHEDULER_MARGIN_LOAD RCL_SCHEDULER_SYSTIM_US(460U) 58 #define RCL_SCHEDULER_SLEEP_CUTOFF RCL_SCHEDULER_SYSTIM_MS(5U) 59 #define RCL_SCHEDULER_TRIG_NOW_DELAY RCL_SCHEDULER_SYSTIM_US(50U) 60 #if defined(DeviceFamily_CC23X0R5) || defined(DeviceFamily_CC23X0R2) || defined(DeviceFamily_CC23X0R22) || defined(DeviceFamily_CC2340R53) 61 #define RCL_SCHEDULER_WAKEUP_MARGIN RCL_SCHEDULER_SYSTIM_US(390U) 62 #elif defined(DeviceFamily_CC27XX) 63 #define RCL_SCHEDULER_WAKEUP_MARGIN RCL_SCHEDULER_SYSTIM_US(150U) 65 #define RCL_SCHEDULER_WAKEUP_MARGIN RCL_SCHEDULER_SYSTIM_US(1000U) 81 typedef struct RCL_SchedulerStopInfo_s {
82 uint32_t cmdStopEnabled : 1;
83 uint32_t schedStopEnabled : 1;
84 uint32_t apiStopEnabled : 1;
90 typedef struct RCL_SchedulerState_s {
92 uint32_t nextWantsStop : 1;
RCL_StopType RCL_Scheduler_setStopTimes(void)
Function to apply relevant stop times.
Definition: RCL_Scheduler.c:432
RCL_Events postedRclEvents
Definition: RCL_Scheduler.h:95
RCL_SchedulerStopInfo gracefulStopInfo
Definition: RCL_Scheduler.h:98
RCL_SchedulerState rclSchedulerState
Definition: RCL_Scheduler.c:51
Definition: RCL_Scheduler.h:76
RCL_CommandStatus RCL_Scheduler_setStartStopTime(const RCL_Command *cmd)
Set start and stop time for LRF based on command.
Definition: RCL_Scheduler.c:139
RCL_CommandStatus RCL_Scheduler_setNewStartRelTime(uint32_t relStartTime)
Set new start time for LRF to given time relative to previous LRF start.
Definition: RCL_Scheduler.c:292
bool RCL_Scheduler_isLater(uint32_t refTime, uint32_t chkTime)
Find if a time instant occurs after another, allowing wrap-around.
Definition: RCL_Scheduler.c:483
static uint32_t RCL_Scheduler_getCurrentTime(void)
Get current time.
Definition: RCL_Scheduler.h:289
Definition: RCL_Scheduler.h:77
RCL_StopType
Stop types.
Definition: RCL_Command.h:145
RCL_StopType RCL_Scheduler_setSchedStopTime(RCL_SchedulerStopInfo *stopInfo, uint32_t schedStopTime)
Set scheduler stop time.
Definition: RCL_Scheduler.c:529
Definition: RCL_Scheduler.h:81
Definition: RCL_Scheduler.h:72
RCL_ScheduleType
Schedule type.
Definition: RCL_Command.h:157
RCL_StopType RCL_Scheduler_setCmdStopTime(RCL_SchedulerStopInfo *stopInfo, uint32_t cmdStopTime)
Set command stop time.
Definition: RCL_Scheduler.c:537
RCL_SchedulerStopReason
Definition: RCL_Scheduler.h:68
RCL_StopType RCL_Scheduler_cancelSchedStopTime(RCL_SchedulerStopInfo *stopInfo)
Cancel scheduler stop time.
Definition: RCL_Scheduler.c:545
RCL_SchedulerStopTimeState
Definition: RCL_Scheduler.h:75
RCL_CommandStatus RCL_Scheduler_setNewStartNow(void)
Set new start time for LRF to now, after a previous start.
Definition: RCL_Scheduler.c:275
RCL_CommandStatus RCL_Scheduler_setStartStopTimeEarliestStart(const RCL_Command *cmd, uint32_t earliestStartTime)
Set start and stop time for LRF based on command with earliest start time.
Definition: RCL_Scheduler.c:164
Definition: RCL_Scheduler.h:70
Definition: RCL_Scheduler.h:71
Definition: RCL_Scheduler.h:69
int32_t RCL_Scheduler_delta(uint32_t refTime, uint32_t chkTime)
Find the time difference between two times, allowing wrap-around.
Definition: RCL_Scheduler.c:501
void * RCL_Command_Handle
Definition: RCL_Types.h:36
uint32_t schedStopTime
Definition: RCL_Scheduler.h:87
uint32_t actualStartTime
Definition: RCL_Scheduler.h:96
uint32_t hal_get_current_time(void)
Definition: hal_cc23x0.c:188
RCL_StopType RCL_Scheduler_cancelCmdStopTime(RCL_SchedulerStopInfo *stopInfo)
Cancel command stop time.
Definition: RCL_Scheduler.c:553
RCL_Command * currCmd
Definition: RCL_Scheduler.h:91
RCL_CommandStatus RCL_Scheduler_setCmdStopTimeNoStartTrigger(const RCL_Command *cmd)
Set stop time for LRF based on command when it does not need a start trigger.
Definition: RCL_Scheduler.c:265
Definition: RCL_Scheduler.h:78
uint16_t requestedPhyFeatures
Definition: RCL_Scheduler.h:99
bool RCL_Scheduler_postEvent(RCL_Command_Handle c, RCL_Events e)
Post event to command handler.
Definition: RCL_Scheduler.c:745
Definition: RCL_Scheduler.h:90
RCL_CommandStatus RCL_Scheduler_setNewStartAbsTime(uint32_t startTime, bool allowDelay)
Set new start time for LRF to given absolute time, after a previous start.
Definition: RCL_Scheduler.c:283
uint32_t cmdStopTime
Definition: RCL_Scheduler.h:86
RCL_CommandStatus RCL_Scheduler_setCustomStartStopTimeEarliestStart(const RCL_CommandTiming *timing, RCL_ScheduleType scheduling, bool allowDelay, uint32_t earliestStartTime)
Set start and stop time for LRF with earliest start time.
Definition: RCL_Scheduler.c:227
RCL_CommandStatus
Command status.
Definition: RCL_Command.h:86
RCL_SchedulerStopInfo hardStopInfo
Definition: RCL_Scheduler.h:97
RCL_CommandStatus RCL_Scheduler_findStopStatus(RCL_StopType stopType)
Get relevant status when a command was stopped.
Definition: RCL_Scheduler.c:70
RCL_CommandStatus RCL_Scheduler_setCustomStartStopTime(const RCL_CommandTiming *timing, RCL_ScheduleType scheduling, bool allowDelay)
Set start and stop time for LRF.
Definition: RCL_Scheduler.c:202