Radio Control Layer (RCL)
RCL_Buffer.c File Reference
#include <stdint.h>
#include <stdlib.h>
#include <stdbool.h>
#include <ti/drivers/rcl/RCL_Command.h>
#include <ti/drivers/rcl/RCL_Scheduler.h>
#include <ti/drivers/rcl/RCL_Buffer.h>
#include <ti/drivers/rcl/RCL_Debug.h>
#include <ti/drivers/dpl/HwiP.h>
#include <ti/devices/DeviceFamily.h>
#include <ti/log/Log.h>
+ Include dependency graph for RCL_Buffer.c:

Functions

static bool RxEntry_isAtEnd (RCL_MultiBuffer *multiBuffer, uint16_t curIndex)
 
static void List_consumeAndStore (List_List *list, List_List *consumedBuffers)
 
void RCL_TxBuffer_put (List_List *list, RCL_Buffer_TxBuffer *elem)
 Function to atomically put an elem onto the end of a Tx Buffer list. More...
 
uint8_t * RCL_TxBuffer_init (RCL_Buffer_TxBuffer *buffer, uint32_t numPad, uint32_t hdrLen, uint32_t dataLen)
 Function to initialize a TX buffer entry for use by RCL. More...
 
void RCL_MultiBuffer_clear (RCL_MultiBuffer *buffer)
 Function to clear a multi buffer entry for re-use by RCL. More...
 
void RCL_MultiBuffer_init (RCL_MultiBuffer *buffer, size_t size)
 Function to initialize a multi buffer entry for use by RCL. More...
 
void RCL_MultiBuffer_put (List_List *list, RCL_MultiBuffer *elem)
 Function to atomically put an elem onto the end of a multi buffer list. More...
 
RCL_Buffer_DataEntry * RCL_MultiBuffer_RxEntry_get (List_List *list, List_List *consumedBuffers)
 Function to get the first entry in a MultiBuffer list. More...
 
bool RCL_MultiBuffer_RxEntry_isEmpty (List_List *list)
 Function to check if the MultiBuffer List is out of entries. More...
 
void RCL_MultiBuffer_ListInfo_init (RCL_MultiBuffer_ListInfo *listInfo, List_List *list)
 Function to initialize information for traversing a multi buffer list. More...
 
RCL_Buffer_DataEntry * RCL_MultiBuffer_RxEntry_next (RCL_MultiBuffer_ListInfo *listInfo)
 Function to return the next entry in a list of multi buffers. More...
 
bool RCL_MultiBuffer_RxEntry_isLast (RCL_MultiBuffer_ListInfo *listInfo)
 Function to check a traversed entry was the last one. More...
 
size_t RCL_Buffer_readPartialRxBuffer (RCL_Buffer_DataEntry *dataEntry, size_t entrySize)
 Read partially received packet into buffer. More...
 
RCL_MultiBuffer * RCL_MultiBuffer_findFirstWritableBuffer (RCL_MultiBuffer *head)
 Find the first writable buffer in a list of MultiBuffers. More...
 
RCL_MultiBuffer * RCL_MultiBuffer_getBuffer (RCL_MultiBuffer *curBuffer, uint32_t minLength)
 Returns a buffer with at least minLength bytes remaining capacity. More...
 
uint32_t RCL_MultiBuffer_findAvailableRxSpace (const RCL_MultiBuffer *curBuffer)
 Find the minumum number of bytes that can be stored in available MultiBuffers. More...
 

Function Documentation

§ RxEntry_isAtEnd()

static bool RxEntry_isAtEnd ( RCL_MultiBuffer *  multiBuffer,
uint16_t  curIndex 
)
static

§ List_consumeAndStore()

static void List_consumeAndStore ( List_List *  list,
List_List *  consumedBuffers 
)
static