rflib to RCL Migration Guide¶
As CC23xx or CC27xx devices do not have a separate CM0 core for RF, a Radio Control Layer (RCL) which is entirely different from the existing CC26x2 device rflib must be used.
The following sections discuss the major changes to radio commands from the
main application file between CC26x2 devices and the CC23xx or CC27xx devices,
using rfPacketTx.c as an example.
Warning
This is not a fully comprehensive list and the API documentation should be consulted when attempting to convert radio commands. File comparison software is highly recommended to compare the difference between application files’ radio commands.
Includes¶
The rflib directory was included for CC26x2 devices
/***** Includes *****/
//...
/* TI Drivers */
#include <ti/drivers/rf/RF.h>
/* Driverlib Header files */
#include DeviceFamily_constructPath(driverlib/rf_prop_mailbox.h)
/* Board Header files */
#include <ti_radio_config.h>
CC23xx or CC27xx devices will use RCL instead
/***** Includes *****/
//...
/* TI Drivers */
#include <ti/drivers/rcl/RCL.h>
#include <ti/drivers/rcl/RCL_Scheduler.h>
#include <ti/drivers/rcl/commands/generic.h>
#if defined(USE_250KBPS_MSK) || defined(USE_500KBPS_MSK)
#include <setup/generic_fsk_prop_setup.h>
#else
#include <setup/generic_1m_prop_setup.h>
#endif
Defines¶
CC23xx or CC27xx devices are bound to rely on different definitions since the commands are not similar
/***** Defines *****/
/* Packet TX Configuration */
#define MAX_LENGTH (30U) // Max packet length
#define NUM_DATA_ENTRIES (2U) // Number of data entries
#define NUM_PAD_BYTES (3U) // Number of pad bytes
/* Header length */
#if defined(USE_500KBPS_MSK) || defined(FIXED_LENGTH_SETUP) // 500KBPS is always set up for fixed length packets
#define HDR_LEN (0U)
#else
#if defined(USE_250KBPS_MSK) // 250KBPS with variable length enabled
#define HDR_LEN (1U)
#else // 1 Mbps with variable length enabled
#define HDR_LEN (2U)
#endif
#endif
#define PACKET_INTERVAL 500000 /* Set packet interval to 500000us or 500ms */
/* Indicates if FS is off */
#define FS_OFF (1U) // 0: On, 1: Off
#if defined(USE_250KBPS_MSK) || defined(USE_500KBPS_MSK)
#define FREQUENCY (2433000000U)
#else
#define FREQUENCY (2440000000U)
#endif
Variables and initialization¶
RF_* had been initialized for CC26x2 devices
static RF_Object rfObject;
static RF_Handle rfHandle;
// ...
void *mainThread(void *arg0)
{
RF_Params rfParams;
RF_Params_init(&rfParams);
/* Request access to the radio */
#if defined(DeviceFamily_CC26X0R2)
rfHandle = RF_open(&rfObject, &RF_prop, (RF_RadioSetup*)&RF_cmdPropRadioSetup, &rfParams);
#else
rfHandle = RF_open(&rfObject, &RF_prop, (RF_RadioSetup*)&RF_cmdPropRadioDivSetup, &rfParams);
#endif// DeviceFamily_CC26X0R2
/* Set the frequency */
RF_postCmd(rfHandle, (RF_Op*)&RF_cmdFs, RF_PriorityNormal, NULL, 0);
Which CC23xx or CC27xx devices replace with RCL_* variants
/* RCL Commands */
RCL_CmdGenericTx txCmd; // TX command
/* RCL Client used to open RCL */
static RCL_Client rclClient;
// ...
void *mainThread(void *arg0)
{
/* Initialize and open RCL */
RCL_init();
#if defined(USE_250KBPS_MSK)
RCL_Handle rclHandle = RCL_open(&rclClient, &rclRadioConfigGenericMsk250k);
#elif defined(USE_500KBPS_MSK)
RCL_Handle rclHandle = RCL_open(&rclClient, &rclRadioConfigGenericMsk500k);
#else
RCL_Handle rclHandle = RCL_open(&rclClient, &rclRadioConfigGenericBle);
#endif
/* Setup generic transmit command */
txCmd = RCL_CmdGenericTx_DefaultRuntime();
/* Set RF frequency */
txCmd.rfFrequency = FREQUENCY;
#if !(defined(USE_250KBPS_MSK) || defined(USE_500KBPS_MSK))
txCmd.common.phyFeatures = RCL_GENERIC_PHY_FEATURE_PHY_1MBPS;
#endif
RF commands¶
Different command parameters should be expected. Below is an example for CC26x2 devices
RF_cmdPropTx.pktLen = PAYLOAD_LENGTH;
RF_cmdPropTx.pPkt = packet;
RF_cmdPropTx.startTrigger.triggerType = TRIG_NOW;
// ...
while(1)
{
/* Create packet with incrementing sequence number and random payload */
packet[0] = (uint8_t)(seqNumber >> 8);
packet[1] = (uint8_t)(seqNumber++);
uint8_t i;
for (i = 2; i < PAYLOAD_LENGTH; i++)
{
packet[i] = rand();
}
/* Send packet */
RF_EventMask terminationReason = RF_runCmd(rfHandle, (RF_Op*)&RF_cmdPropTx,
RF_PriorityNormal, NULL, 0);
Compared to CC23xx or CC27xx devices
/* Start command as soon as possible */
txCmd.common.scheduling = RCL_Schedule_Now;
txCmd.common.status = RCL_CommandStatus_Idle;
txCmd.config.fsOff = FS_OFF; // Turn off FS
/* Callback triggers on last command done */
txCmd.common.runtime.callback = defaultCallback;
txCmd.common.runtime.rclCallbackMask.value = RCL_EventLastCmdDone.value;
/* Set RCL TX buffer packet to be packet buffer */
RCL_Buffer_TxBuffer *txPacket = (RCL_Buffer_TxBuffer *)&packet;
while(1)
{
/* Create packet with random payload */
uint8_t *txData;
txData = RCL_TxBuffer_init(txPacket, NUM_PAD_BYTES, HDR_LEN, MAX_LENGTH);
#if !(defined(USE_500KBPS_MSK) || defined(FIXED_LENGTH_SETUP))
#if defined(USE_250KBPS_MSK)
txData[0] = MAX_LENGTH;
#else
txData[0] = 0;
txData[1] = MAX_LENGTH;
#endif
#endif
for (int i = HDR_LEN; i < MAX_LENGTH; i++)
{
txData[i] = rand();
}
/* Set packet to transmit */
RCL_TxBuffer_put(&txCmd.txBuffers, txPacket);
txCmd.common.status = RCL_CommandStatus_Idle;
/* Submit command */
RCL_Command_submit(rclHandle, &txCmd);
/* Pend on command completion */
RCL_Command_pend(&txCmd);
Note
If changing the txCmd->txPower parameter it is important to note that
two additional sub-parameters, dbm and fraction, will each need to be
initialized. For example,
txCmd->txPower = (RCL_Command_TxPower){.dBm = txPower_dBm, .fraction = 0};
RF API comparison¶
Below is a table summarizing the different API functions, however it is once again advised that the rflib and Radio Control Layer (RCL) APIs be further referenced for a full understanding of differences.
Function |
rflib API |
RCL API |
|---|---|---|
Initialize the radio driver |
RF_Params_init |
RCL_init |
Open the radio instance |
RF_open |
RCL_open |
Close the radio instance |
RF_close |
RCL_close |
Submit a radio command |
RF_postCmd |
RCL_Command_submit |
Wait for the radio command to complete |
RF_pendCmd |
RCL_Command_pend |
Submit a radio command and wait for it to complete |
RF_runCmd |
RCL_Command_submit & RCL_Command_pend |
Stop a radio command |
RF_cancelCmd |
RCL_Command_stop |
Get RSSI |
RF_getRssi |
RCL_readRssi |