![]() |
![]() |
SPILPF3DMA Object. More...
#include <SPILPF3DMA.h>

Data Fields | |
| HwiP_Struct | hwi |
| Power_NotifyObj | spiPostObj |
| SwiP_Struct | swi |
| SemaphoreP_Struct | transferComplete |
| SPI_CallbackFxn | transferCallbackFxn |
| SPI_Transaction * | headPtr |
| SPI_Transaction * | tailPtr |
| SPI_Transaction * | completedTransfers |
| size_t | framesQueued |
| size_t | framesTransferred |
| size_t | priTransferSize |
| size_t | altTransferSize |
| uint32_t | activeChannel |
| uint32_t | bitRate |
| uint32_t | dataSize |
| uint32_t | transferTimeout |
| uint32_t | busyBit |
| uint32_t | dsample |
| uint16_t | rxScratchBuf |
| uint16_t | txScratchBuf |
| SPI_TransferMode | transferMode |
| SPI_Mode | mode |
| uint8_t | format |
| uint_least8_t | csnPin |
| SPILPF3DMA_ReturnPartial | returnPartial |
| bool | isOpen |
| bool | manualStart |
SPILPF3DMA Object.
The application must not access any member variables of this structure!
| HwiP_Struct SPILPF3DMA_Object::hwi |
| Power_NotifyObj SPILPF3DMA_Object::spiPostObj |
| SwiP_Struct SPILPF3DMA_Object::swi |
| SemaphoreP_Struct SPILPF3DMA_Object::transferComplete |
| SPI_CallbackFxn SPILPF3DMA_Object::transferCallbackFxn |
| SPI_Transaction* SPILPF3DMA_Object::headPtr |
| SPI_Transaction* SPILPF3DMA_Object::tailPtr |
| SPI_Transaction* SPILPF3DMA_Object::completedTransfers |
| size_t SPILPF3DMA_Object::framesQueued |
| size_t SPILPF3DMA_Object::framesTransferred |
| size_t SPILPF3DMA_Object::priTransferSize |
| size_t SPILPF3DMA_Object::altTransferSize |
| uint32_t SPILPF3DMA_Object::activeChannel |
| uint32_t SPILPF3DMA_Object::bitRate |
| uint32_t SPILPF3DMA_Object::dataSize |
| uint32_t SPILPF3DMA_Object::transferTimeout |
| uint32_t SPILPF3DMA_Object::busyBit |
| uint32_t SPILPF3DMA_Object::dsample |
| uint16_t SPILPF3DMA_Object::rxScratchBuf |
| uint16_t SPILPF3DMA_Object::txScratchBuf |
| SPI_TransferMode SPILPF3DMA_Object::transferMode |
| SPI_Mode SPILPF3DMA_Object::mode |
| uint8_t SPILPF3DMA_Object::format |
| uint_least8_t SPILPF3DMA_Object::csnPin |
| SPILPF3DMA_ReturnPartial SPILPF3DMA_Object::returnPartial |
| bool SPILPF3DMA_Object::isOpen |
| bool SPILPF3DMA_Object::manualStart |