![]() |
![]() |
LFOSC Compensation Profile structure. More...
#include <PowerCC27XX.h>
Data Fields | |
| uint32_t | systemWakeupIntervalUsec |
| The expected interval in us between system wakeups. More... | |
| PowerLPF3_LfoscCompensationPpmRequirement | ppmRequirement |
| The PPM requirements. More... | |
| uint16_t | maxAllowedJitterUsec |
| The maximum additional jitter allowed per wakeup beyond the ppm requirement in us. More... | |
| uint16_t | temperatureGradientMilliCelsiusPerSec |
| The absolute value of the worst case expected temperature gradient in mC/s. More... | |
LFOSC Compensation Profile structure.
When LFOSC Compensation is enabled, HFXT will periodically be turned on to calibrate the LFOSC. The duration of these calibrations and the interval between them are computed based on the values in this structure, and other parameters such as the current temperature.
| uint32_t PowerLPF3_LfoscCompensationProfile::systemWakeupIntervalUsec |
The expected interval in us between system wakeups.
This would for example be 1000000 (1s) for a 1s BLE connection interval.
| PowerLPF3_LfoscCompensationPpmRequirement PowerLPF3_LfoscCompensationProfile::ppmRequirement |
The PPM requirements.
| uint16_t PowerLPF3_LfoscCompensationProfile::maxAllowedJitterUsec |
The maximum additional jitter allowed per wakeup beyond the ppm requirement in us.
| uint16_t PowerLPF3_LfoscCompensationProfile::temperatureGradientMilliCelsiusPerSec |
The absolute value of the worst case expected temperature gradient in mC/s.