Data Fields
MCAN_ProtocolStatus Struct Reference

Structure for MCAN protocol status. More...

#include <MCAN.h>

Data Fields

MCAN_ErrCode lastErrCode
 
MCAN_ComState act
 
uint32_t errPassive
 
uint32_t warningStatus
 
uint32_t busOffStatus
 
MCAN_ErrCode dlec
 
uint32_t resi
 
uint32_t rbrs
 
uint32_t rfdf
 
uint32_t pxe
 
uint32_t tdcv
 

Detailed Description

Structure for MCAN protocol status.

Field Documentation

§ lastErrCode

MCAN_ErrCode MCAN_ProtocolStatus::lastErrCode

Last Error Code. Refer enum MCAN_ErrCode

§ act

MCAN_ComState MCAN_ProtocolStatus::act

Activity - Monitors the module's CAN communication state. Refer enum MCAN_ComState

§ errPassive

uint32_t MCAN_ProtocolStatus::errPassive

Error Passive
0 = The M_CAN is in the Error_Active state
1 = The M_CAN is in the Error_Passive state

§ warningStatus

uint32_t MCAN_ProtocolStatus::warningStatus

Warning Status
0 = Both error counters are below the Error_Warning limit of 96
1 = At least one of error counter has reached the Error_Warning limit of 96

§ busOffStatus

uint32_t MCAN_ProtocolStatus::busOffStatus

Bus_Off Status
0 = The M_CAN is not Bus_Off
1 = The M_CAN is in Bus_Off state

§ dlec

MCAN_ErrCode MCAN_ProtocolStatus::dlec

Data Phase Last Error Code. Refer enum MCAN_ErrCode

§ resi

uint32_t MCAN_ProtocolStatus::resi

ESI flag of last received CAN FD Message
0 = Last received CAN FD message did not have its ESI flag set
1 = Last received CAN FD message had its ESI flag set

§ rbrs

uint32_t MCAN_ProtocolStatus::rbrs

BRS flag of last received CAN FD Message
0 = Last received CAN FD message did not have its BRS flag set
1 = Last received CAN FD message had its BRS flag set

§ rfdf

uint32_t MCAN_ProtocolStatus::rfdf

Received a CAN FD Message
0 = Since this bit was reset by the CPU, no CAN FD message has been received
1 = Message in CAN FD format with FDF flag set has been received

§ pxe

uint32_t MCAN_ProtocolStatus::pxe

Protocol Exception Event
0 = No protocol exception event occurred since last read access
1 = Protocol exception event occurred

§ tdcv

uint32_t MCAN_ProtocolStatus::tdcv

Transmitter Delay Compensation Value


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale