Data Fields
LogSinkUART_Instance Struct Reference

LogSinkUART Sink parameters. More...

#include <LogSinkUART.h>

Data Fields

uint_least8_t index
 

Detailed Description

LogSinkUART Sink parameters.

The LogSinkUART_Instance structure contains a set of parameters used to characterize a LogSinkUART sink.

Field Documentation

§ index

uint_least8_t LogSinkUART_Instance::index

Index of the LogSinkUART sink instance used to index LogSinkUART_config[]


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale