Data Fields
I2CLPF3_Object Struct Reference

I2CLPF3 Object. More...

#include <I2CLPF3.h>

Collaboration diagram for I2CLPF3_Object:
Collaboration graph
[legend]

Data Fields

I2C_BASE_OBJECT SwiP_Struct swi
 
uint32_t bitRate
 
uint8_t sdaPin
 
uint8_t sclPin
 
void * i2cPostFxn
 
Power_NotifyObj i2cPostObj
 

Detailed Description

I2CLPF3 Object.

The application must not access any member variables of this structure!

Field Documentation

§ swi

I2C_BASE_OBJECT SwiP_Struct I2CLPF3_Object::swi

§ bitRate

uint32_t I2CLPF3_Object::bitRate

§ sdaPin

uint8_t I2CLPF3_Object::sdaPin

§ sclPin

uint8_t I2CLPF3_Object::sclPin

§ i2cPostFxn

void* I2CLPF3_Object::i2cPostFxn

§ i2cPostObj

Power_NotifyObj I2CLPF3_Object::i2cPostObj

The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale