Data Fields
Comparator_Params Struct Reference

Comparator parameters. More...

#include <Comparator.h>

Collaboration diagram for Comparator_Params:
Collaboration graph
[legend]

Data Fields

Comparator_CallBackFxn callbackFxn
 
Comparator_Trigger trigger
 

Detailed Description

Comparator parameters.

Comparator parameters are used by the Comparator_open() call. Default values for these parameters are set using Comparator_Params_init().

Field Documentation

§ callbackFxn

Comparator_CallBackFxn Comparator_Params::callbackFxn

Callback function called when events happen in the Comparator driver

§ trigger

Comparator_Trigger Comparator_Params::trigger

Interrupt trigger of the Comparator module


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale