Data Fields
CANCC27XXX10_Config Struct Reference

CANCC27XXX10 global configuration. More...

#include <CANCC27XX.h>

Data Fields

void * taskStack
 
uint16_t taskStackSize
 
uint8_t taskPri
 

Detailed Description

CANCC27XXX10 global configuration.

Field Documentation

§ taskStack

void* CANCC27XXX10_Config::taskStack

Pointer to interrupt handler task stack

§ taskStackSize

uint16_t CANCC27XXX10_Config::taskStackSize

Interrupt handler task stack size

§ taskPri

uint8_t CANCC27XXX10_Config::taskPri

Interrupt handler task priority


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale