![]() |
![]() |
ADCBufLPF3 Object. More...
#include <ADCBufLPF3.h>

ADCBufLPF3 Object.
The application must not access any member variables of this structure!
| SemaphoreP_Struct ADCBufLPF3_Object::conversionSemaphore |
Conversion semaphore. Used in blocking mode only.
| ADCBuf_Conversion* ADCBufLPF3_Object::currentConversion |
Pointer to the current conversion struct
| HwiP_Struct ADCBufLPF3_Object::hwi |
Hwi object
| ADCBuf_Callback ADCBufLPF3_Object::callbackFxn |
Pointer to callback function
| uint32_t* ADCBufLPF3_Object::activeSampleBuffer |
The last complete sample buffer used by the DMA
| uint32_t ADCBufLPF3_Object::semaphoreTimeout |
Timeout for read semaphore in ADCBuf_RETURN_MODE_BLOCKING
| uint32_t ADCBufLPF3_Object::samplingFrequency |
Frequency in Hz at which the ADC is triggered
| ADCBufLPF3_ConversionStatus ADCBufLPF3_Object::conversionStatus |
Is the ADC currently doing conversions
| ADCBuf_Return_Mode ADCBufLPF3_Object::returnMode |
Mode for all conversions
| ADCBuf_Recurrence_Mode ADCBufLPF3_Object::recurrenceMode |
Should we convert continuously or one-shot
| bool ADCBufLPF3_Object::isOpen |
Has the object been opened
| bool ADCBufLPF3_Object::userAcquiredAdcSemaphore |
Did the user manually acquire the ADC semaphore?