Macros
UART2_STATUS

Macros

#define UART2_STATUS_SUCCESS   (0)
 Successful status code returned by UART2 APIs. More...
 
#define UART2_STATUS_SREADTIMEOUT   (1)
 A read timeout occurred (not an error). More...
 
#define UART2_STATUS_EFRAMING   (-1)
 A framing error occurred. More...
 
#define UART2_STATUS_EPARITY   (-2)
 A parity error occurred. More...
 
#define UART2_STATUS_EBREAK   (-4)
 A break error occurred. More...
 
#define UART2_STATUS_EOVERRUN   (-8)
 A FIFO overrun occurred. More...
 
#define UART2_STATUS_EINUSE   (-9)
 The UART is currently in use. More...
 
#define UART2_STATUS_EINVALID   (-10)
 An invalid argument or UART2_Params field was passed to UART2 API. More...
 
#define UART2_STATUS_EFAIL   (-11)
 General failure status returned by UART2 API. More...
 
#define UART2_STATUS_EMEMORY   (-12)
 A memory allocation failure occurred. More...
 
#define UART2_STATUS_ETIMEOUT   (-13)
 A timeout occurred for a blocking UART2_read or UART2_write call. More...
 
#define UART2_STATUS_ECANCELLED   (-14)
 A UART2_write() or UART2_read() operation was cancelled. More...
 
#define UART2_STATUS_ENOTOPEN   (-15)
 A UART2_write() or UART2_read() called on a device not opened. More...
 
#define UART2_STATUS_EAGAIN   (-16)
 A UART2_write() or UART2_read() in UART2_Mode_NONBLOCKING would have blocked. More...
 

Detailed Description

Macro Definition Documentation

§ UART2_STATUS_SUCCESS

#define UART2_STATUS_SUCCESS   (0)

Successful status code returned by UART2 APIs.

§ UART2_STATUS_SREADTIMEOUT

#define UART2_STATUS_SREADTIMEOUT   (1)

A read timeout occurred (not an error).

§ UART2_STATUS_EFRAMING

#define UART2_STATUS_EFRAMING   (-1)

A framing error occurred.

§ UART2_STATUS_EPARITY

#define UART2_STATUS_EPARITY   (-2)

A parity error occurred.

§ UART2_STATUS_EBREAK

#define UART2_STATUS_EBREAK   (-4)

A break error occurred.

§ UART2_STATUS_EOVERRUN

#define UART2_STATUS_EOVERRUN   (-8)

A FIFO overrun occurred.

§ UART2_STATUS_EINUSE

#define UART2_STATUS_EINUSE   (-9)

The UART is currently in use.

§ UART2_STATUS_EINVALID

#define UART2_STATUS_EINVALID   (-10)

An invalid argument or UART2_Params field was passed to UART2 API.

§ UART2_STATUS_EFAIL

#define UART2_STATUS_EFAIL   (-11)

General failure status returned by UART2 API.

§ UART2_STATUS_EMEMORY

#define UART2_STATUS_EMEMORY   (-12)

A memory allocation failure occurred.

§ UART2_STATUS_ETIMEOUT

#define UART2_STATUS_ETIMEOUT   (-13)

A timeout occurred for a blocking UART2_read or UART2_write call.

§ UART2_STATUS_ECANCELLED

#define UART2_STATUS_ECANCELLED   (-14)

A UART2_write() or UART2_read() operation was cancelled.

§ UART2_STATUS_ENOTOPEN

#define UART2_STATUS_ENOTOPEN   (-15)

A UART2_write() or UART2_read() called on a device not opened.

§ UART2_STATUS_EAGAIN

#define UART2_STATUS_EAGAIN   (-16)

A UART2_write() or UART2_read() in UART2_Mode_NONBLOCKING would have blocked.

© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale