Macros
CAN Filter Element Configurations

Macros

#define CAN_FEC_DISABLE_FILTER   ((uint32_t)0U)
 
#define CAN_FEC_STORE_RXFIFO0   ((uint32_t)1U)
 
#define CAN_FEC_STORE_RXFIFO1   ((uint32_t)2U)
 
#define CAN_FEC_REJECT_ID   ((uint32_t)3U)
 
#define CAN_FEC_SET_PRIO   ((uint32_t)4U)
 
#define CAN_FEC_SET_PRIO_STORE_RXFIFO0   ((uint32_t)5U)
 
#define CAN_FEC_SET_PRIO_STORE_RXFIFO1   ((uint32_t)6U)
 
#define CAN_FEC_STORE_RXBUF   ((uint32_t)7U)
 

Detailed Description

Filter Element Configuration for use with CAN_MsgRamConfig
0 = Disable filter element
1 = Store in Rx FIFO 0 if filter matches
2 = Store in Rx FIFO 1 if filter matches
3 = Reject ID if filter matches
4 = Set priority if filter matches
5 = Set priority and store in FIFO 0 if filter matches
6 = Set priority and store in FIFO 1 if filter matches
7 = Store into Rx Buffer or as debug message, configuration of filter type is ignored.
If FEC = 4-6, a match sets high priority message status and generates an interrupt.

Macro Definition Documentation

§ CAN_FEC_DISABLE_FILTER

#define CAN_FEC_DISABLE_FILTER   ((uint32_t)0U)

§ CAN_FEC_STORE_RXFIFO0

#define CAN_FEC_STORE_RXFIFO0   ((uint32_t)1U)

§ CAN_FEC_STORE_RXFIFO1

#define CAN_FEC_STORE_RXFIFO1   ((uint32_t)2U)

§ CAN_FEC_REJECT_ID

#define CAN_FEC_REJECT_ID   ((uint32_t)3U)

§ CAN_FEC_SET_PRIO

#define CAN_FEC_SET_PRIO   ((uint32_t)4U)

§ CAN_FEC_SET_PRIO_STORE_RXFIFO0

#define CAN_FEC_SET_PRIO_STORE_RXFIFO0   ((uint32_t)5U)

§ CAN_FEC_SET_PRIO_STORE_RXFIFO1

#define CAN_FEC_SET_PRIO_STORE_RXFIFO1   ((uint32_t)6U)

§ CAN_FEC_STORE_RXBUF

#define CAN_FEC_STORE_RXBUF   ((uint32_t)7U)
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale