APU function to compute the Jacobi Eigen-Decomposition (EVD) of a triangular Hermitian Matrix. This results in a triangular, diagonal matrix of eigenvalues sorted in descending order replacing the original matrix, and a full matrix, where the eigenvectors are the columns. The eigenvector matrix can be placed anywhere in APU memory except for where the input matrix is placed. When not using scratchpad mode, the eigenvector matrix will be placed next to the eigenvector matrix.
Defined as:
(V, D) = eigen_decomposition(A), such that V' * A * V = D
in which A[NxN] is a triangular Hermitian matrix V[NxN] is a triangular, diagonal matrix of eigenvalues, D[NxN] is a full matrix of eigenvectors and V' signifies the conjugate transpose of V.
- Note
- Since A is the Hermitian matrix, eigenvalues are all real and positive numbers. In the APU, the output eigenvalues are already sorted in descending order. To save memory, the input matrix A is updated by in-place rotation, resulting in the diagonal matrix D. If not in scratchpad mode, i.e one of the provided vectors/matrices have their data outside of APU space, this function will return a Vector whose data contains the data of both the eigenvalue triangular matrix and the eigenvalue full matrix. The eigenvector data begins at an offset of (L*L + L)/2.
- Precondition
- APULPF3_init() has to be called first.
- Parameters
-
| [in] | mat | the input matrix |
| [in] | maxIter | the maximum number of iterations for the Jacobi algorithm (typically 3) |
| [in] | stopThreshold | threshold for stopping early. Triggers if summation of the off-digonal values is smaller than this threshold. |
| [in] | epsTol | threshold for off-diagonal elements to be considered small enough |
| [out] | result | a pointer to a vector where the output will be placed. If not in scratchpad mode, this vector will contain both the eigenvalues and the eigenvectors. Otherwise it will contain only the eigenvectors. |
- Note
- See ti_drivers_APU_DataManagement for directions on efficient APU memory management.
- Returns
- A status code indicating whether the APU operation was a success.
- Return values
-